Hi,
I am currently measuring the output impedance on a CC1352P1F3 radio circuit using a VNA (Vector Network Analyzer) on the Rx circuit and on the Tx. For the Rx circuit, there is no problem, I use the "Packet Rx" function of smart rf studio and I can measure the chip input impedance without any problem. For measuring the Tx circuit, I need to activate the power amplifier 20dBm ON but I must not send any data toward the antenna.
How is it possible ?
With smart RF studio I can activate the RF switch on the front end to the Tx path but the PA 20dBm stays OFF. The only way to activate the PA 20dBm is to send unmodulated or modulated data but those data perturbates my measurements. That's why I shall not send any data towards antenna while putting ON the PA 20dBm
Is it possible to put the power amplifier 20dBm ON without sending any signal (neither modulated nor CW) ?
The application circuit I use is a component CC1352P1F3RGZR with balun 0900PC15A0036E on the Rx line and balun 1720BL15B0200E on the TX 20dBm line.
Thanks for your help.
Laurent.