Hello,
Are the following limitations for avoiding the integer boundary problem fixed in new hardware revisions?
Table 4.14 of the CC1200’s Data Sheet
“It is expected that there will be degraded sensitivity at multiples of XOSC/2 in RX, and an increase in spurious emissions when the RF Crystal frequency 38.4 40 MHz channel is close to multiples of XOSC in TX. We recommend that the RF channel is kept RX_BW/2 away from XOSC/2 in RX, and that the level of spurious emissions be evaluated if the RF channel is closer than 1 MHz to multiples of XOSC in TX.”
What could you recommend to avoid this problem when CC1200 is used?
Thanks,
Alex