The end device can't join the network ; and the joinpermit is opened.
How do I debug next?
Note:
SDK version:simplelink_cc13x0_sdk_4_10_02_04.
examples:clloctor,sensor.
Kent
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The end device can't join the network ; and the joinpermit is opened.
How do I debug next?
Note:
SDK version:simplelink_cc13x0_sdk_4_10_02_04.
examples:clloctor,sensor.
Kent
Hi Marie,
log:
collector:
TI Collector
Restarted
Channel: 0
PermitJoin-ON
sensor:
TI Sensor
State Changed: 1
Starting...
It can be seen that the equipment is in normal operation.
The PANID and Channel is default config,I don't modify them.
Thanks a log.
kent