Hi,
I have custom board with CC1310. I have similar error as in below topic.
https://e2e.ti.com/support/microcontrollers/other/f/908/t/697937?RTOS-EK-TM4C1294XL-Type-xdc-cfg-Program-The-package-ti-sysbios-knl-is-not-compatible-with-XDCtools-used-in-this-build-Please-either-use-XDCtools-compatible-with-that-package-or-update-the-product-containing-that-package-or-rebuild-the-packa
In project I use below products but I can't use newer RTOS Object Viewer. I want to use new ROV. How can I do ? If not possible, I can't see my tasks while debugging the project in classical ROV. I see there is always written "Target Running". When I pause debug I see everything but while working I can't see anything except this "Target Running" text. Waiting for help.