This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello guys,
One of my customers is going to use CC1121 for their next products.
Also they are considering using one of following LDOs for CC1121.
TLV700 SOT-23-THIN
https://www.ti.com/product/TLV700
LP5907 SOT-23-THIN
https://www.ti.com/lit/ds/symlink/lp5907.pdf
TPS782 SOT-23-THIN
https://www.ti.com/product/TPS782
LP5900 WSON
https://www.ti.com/product/LP5900
Could you please tell me the LDO if any of these LDOs are not suitable for CC1121 power supply?
Your reply would be much appreciated.
Best regards,
Kazuya.
Which input voltage and output voltage for the LDO do you target?
Have you a buck/ boost converter (TPS62740 family) to save current?
Hello TER,
Thank you for your reply.
LDO input voltage is 2.5V (min) and output voltage is 2.2V.
They want to use LDO as the power supply of CC1121 for lower cost, and high PSRR, low noise.
Also they think that all of these LDOs can supply the current which CC1121 needs.
Could you please tell me if you have any concern to use these LDOs for CC1121?
Thank you again and best regards,
Kazuya.
Hello TER,
Thank you for your reply.
I have CC1121 datasheet, version SWRS111F.
https://www.ti.com/lit/ds/symlink/cc1121.pdf.
Could you tell me where I can see a description for the LDO in the datasheet?
Is it "2.0–3.6 V VDD to internal digital regulator" in setion 3.2 Pin Configuration on page 6?
Thank you again and best regards,
Kazuya.
The spec of the internal LDOs is not covered in the datasheet but I have fairly good overview of the PSRR of the internal LDOs since I designed some of them.
Could you share the spec for the full power system?
CC1121 is designed be connected to a power source without having to include a LDO with high PSRR. If you are unsure of the performance you can buy some CC112x modules and test if the performance is degraded by your power system or not.
Hello TER,
Thank you very much for your reply.
I understood CC1121 has high PSRR LDO internally.
I will get the full power system and share with you on new thread.
Thank you again and best regards,
Kazuya.