This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC1310 technology consultancy

Part Number: CC1310

Dear:

A: If CMOS sensor is connected to cc1310, do you need to install the following 2, 4 and 5?

2FPS_RevB_1225.pdf1. Ti Code Composer Studio:: 9.1.0 - > installed

2. IAR Embedded Workbench for ARM:: 8.32.2

3. C compiler for arm: 18.12.2. Lts - > installed

4. XDCTools: 3.51.03.28

5. TI-RTOS for CC13XX: 4.20.03.01

B: Does cc1310 have a sample code with ov07676?

C: Please help check the attached schematic diagram.

  • A. To work with CC1310, I think you only need to install CCS 10 and latest SIMPLELINK-CC13X0-SDK 4.10.02.04.

    B. There is no such sample code and I suspect if CC1310 can read frame data from ov07676 smoothly.

  • I edited the original post since the datasheet for the sensor was marked "confidential" 

    You don't need both IAR and CSS, use the one you prefer. 3 and 4: These are normally installed as part of the SDK and you should not have to think about installing these. 

    You have to make your own driver for the ov07676. In the SDK you find examples on how to use the I2C interface. I'm not familiar with DVP or with requirements this interface has. 

    When I reviewed this schematic I only looked at the RF part.