This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC1310 Power Consumption with led blink

Part Number: CC1310
Other Parts Discussed in Thread: CC1190, SYSBIOS,

Hi,

I have a custom board inlcludes cc1310f128 mcu and cc1190 rf front end. I want to see what is my minimum  power consumption. I have a project as I mentioned in different Forum Thread, I adapted it to pinstandby example as much as possible. and I see there while not blinking led consumption is 810 uA , while blinking 1.2 mA. Are these values normal ? I don't think so. How can I reduce consumption ? How am I measuring current ? I have power supply and powering my board via it (3.3V). I have 1.1 ohm resistor on the ground side and looking the voltages on resistor's two sides.

I am using XDCtools 3.32.0.06_core,

TI-RTOS for CC13XX and CC26XX [2.21.0.06]

SimpleLink CC13x0 SDK [4.10.2.04]


I tried to use pinStandby example without any change on my custom board but it stucks in while loop below; (Error with PIN init). 2. question is how can I make it works on my custom board ?

void CC1310_LAUNCHXL_initGeneral(void)
{
Power_init();

if (PIN_init(BoardGpioInitTable) != PIN_SUCCESS) {
/* Error with PIN_init */
while (1);
}

/* Perform board-specific initialization */
Board_initHook();
}



///// My Adapted Project ///////

#include <stdlib.h>
#include <stdio.h>
#include <xdc/std.h>
#include <xdc/cfg/global.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/drivers/rf/RF.h>
#include <ti/drivers/PIN.h>
#include <ti/drivers/Watchdog.h>
#include <ti/drivers/SPI.h>
#include <ti/drivers/I2C.h>
#include <ti/drivers/UART.h>
#include <ti/drivers/pin/PINCC26XX.h>
#include <ti/drivers/Power.h>
#include <ti/sysbios/hal/Seconds.h>
#include <driverlib/rf_prop_mailbox.h>
#include <driverlib/aon_batmon.h>
#include <time.h>
#include "Board.h"
#include "GenericUtils.h"
#include "RFQueue.h"
#include "smartrf_settings/smartrf_settings.h"
#include "functions.h"
#include <driverlib/aon_batmon.h>
#include "unistd.h"

static PIN_Handle ledPinHandle;
static PIN_State ledPinState;
PIN_Handle pinHandle;

PIN_Config pinTable[] =
{
    0x00000003 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    PIN_TERMINATE
};

static Task_Params BlinkTaskParams;
Task_Struct blinkTask;    /* not static so you can see in ROV */
static uint8_t blinkTaskStack[512];

static void blinkTaskFunction(UArg arg0, UArg arg1)
{
    while(1)
    {
        sleep(5);
        PIN_setOutputValue(pinHandle, 0x00000003,!PIN_getOutputValue(0x00000003));
    }
}

void BlinkTask_init(PIN_Handle inPinHandle)
{
    pinHandle = inPinHandle;

    Task_Params_init(&BlinkTaskParams);
    BlinkTaskParams.stackSize = 512;
    BlinkTaskParams.priority = 1;
    BlinkTaskParams.stack = &blinkTaskStack;
    BlinkTaskParams.arg0 = (UInt)1000000;

    Task_construct(&blinkTask, blinkTaskFunction, &BlinkTaskParams, NULL);
}

int main(void)
{
    Power_init();

    PIN_init(pinTable);
    ledPinHandle = PIN_open(&ledPinState, pinTable);
    BlinkTask_init(ledPinHandle);

    BIOS_start();

    return (0);
}






#include <stdlib.h>#include <stdio.h>#include <xdc/std.h>#include <xdc/cfg/global.h>#include <xdc/runtime/System.h>#include <ti/sysbios/BIOS.h>#include <ti/sysbios/knl/Task.h>#include <ti/sysbios/knl/Clock.h>#include <ti/drivers/rf/RF.h>#include <ti/drivers/PIN.h>#include <driverlib/rf_prop_mailbox.h>#include <ti/drivers/UART.h>#include <ti/drivers/pin/PINCC26XX.h>#include "Board.h"#include "GenericUtils.h"#include "RFQueue.h"#include "smartrf_settings/smartrf_settings.h"#include "functions.h"#include <driverlib/aon_batmon.h>#include <time.h>#include <ti/sysbios/hal/Seconds.h>#include "Timer.h"#include <ti/drivers/Watchdog.h>#include <ti/drivers/SPI.h>#include <ti/drivers/I2C.h>#include <driverlib/aon_batmon.h>#include "unistd.h"
static PIN_Handle ledPinHandle;static PIN_State ledPinState;PIN_Handle pinHandle;
PIN_Config pinTable[] ={    0x00000003 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,    PIN_TERMINATE};
static Task_Params BlinkTaskParams;Task_Struct blinkTask;    /* not static so you can see in ROV */static uint8_t blinkTaskStack[512];
static void blinkTaskFunction(UArg arg0, UArg arg1){    while(1)    {        sleep(5);        PIN_setOutputValue(pinHandle, 0x00000003,!PIN_getOutputValue(0x00000003));    }}
void BlinkTask_init(PIN_Handle inPinHandle){    pinHandle = inPinHandle;
    Task_Params_init(&BlinkTaskParams);    BlinkTaskParams.stackSize = 512;    BlinkTaskParams.priority = 1;    BlinkTaskParams.stack = &blinkTaskStack;    BlinkTaskParams.arg0 = (UInt)1000000;
    Task_construct(&blinkTask, blinkTaskFunction, &BlinkTaskParams, NULL);}
int main(void){    Board_initGeneral();
    ledPinHandle = PIN_open(&ledPinState, pinTable);    BlinkTask_init(ledPinHandle);
    BIOS_start();
    return (0);}

  • ccfg.c and cfg files are here.


    ccfg.c

    /******************************************************************************
    *  Filename:       ccfg.c
    *  Revised:        $Date: 2016-03-14 10:46:32 +0100 (ma, 14 mar 2016) $
    *  Revision:       $Revision: 16862 $
    *
    *  Description:    Customer Configuration for CC13xx device family (HW rev 2).
    *
    *  Copyright (C) 2014 Texas Instruments Incorporated - http://www.ti.com/
    *
    *
    *  Redistribution and use in source and binary forms, with or without
    *  modification, are permitted provided that the following conditions
    *  are met:
    *
    *    Redistributions of source code must retain the above copyright
    *    notice, this list of conditions and the following disclaimer.
    *
    *    Redistributions in binary form must reproduce the above copyright
    *    notice, this list of conditions and the following disclaimer in the
    *    documentation and/or other materials provided with the distribution.
    *
    *    Neither the name of Texas Instruments Incorporated nor the names of
    *    its contributors may be used to endorse or promote products derived
    *    from this software without specific prior written permission.
    *
    *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    ******************************************************************************/
    
    #include <stdint.h>
    #include <inc/hw_types.h>
    #include <inc/hw_ccfg.h>
    #include <inc/hw_ccfg_simple_struct.h>
    
    //*****************************************************************************
    //
    // Introduction
    //
    // This file contains fields used by Boot ROM, startup code, and SW radio 
    // stacks to configure chip behavior.
    //
    // Fields are documented in more details in hw_ccfg.h and CCFG.html in 
    // DriverLib documentation (doc_overview.html -> CPU Domain Memory Map -> CCFG).
    //
    //*****************************************************************************
    
    //*****************************************************************************
    //
    // Internal settings, forcing several bit-fields to be set to a specific value.
    //
    //*****************************************************************************
    
    //#####################################
    // Force VDDR high setting (Higher output power but also higher power consumption)
    //#####################################
    
    //Be careful power consumption if enable this setting.
    
    #ifndef CCFG_FORCE_VDDR_HH
    #define CCFG_FORCE_VDDR_HH                              0x0        // Use default VDDR trim
    // #define CCFG_FORCE_VDDR_HH                           0x1        // Force VDDR voltage to the factory HH setting (FCFG1..VDDR_TRIM_HH)
    #endif
    
    //*****************************************************************************
    //
    // Set the values of the individual bit fields.
    //
    //*****************************************************************************
    
    //#####################################
    // Alternative DC/DC settings
    //#####################################
    
    #ifndef SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING    0x0    // Alternative DC/DC setting enabled
    // #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING 0x1    // Alternative DC/DC setting disabled
    #endif
    
    #if ( CCFG_FORCE_VDDR_HH )
    #define SET_CCFG_MODE_CONF_1_ALT_DCDC_VMIN                  0xC    // Special VMIN level (2.5V) when forced VDDR HH voltage
    #else
    #ifndef SET_CCFG_MODE_CONF_1_ALT_DCDC_VMIN
    #define SET_CCFG_MODE_CONF_1_ALT_DCDC_VMIN                  0x8    // 2.25V
    #endif
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN
    // #define SET_CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN          0x0    // Disable
    #define SET_CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN             0x1    // Enable
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_1_ALT_DCDC_IPEAK
    #define SET_CCFG_MODE_CONF_1_ALT_DCDC_IPEAK                 0x0    // 31mA
    #endif
    
    //#####################################
    // XOSC override settings
    //#####################################
    
    #ifndef SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR
    // #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR     0x0        // Enable override
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR        0x1        // Disable override
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_1_DELTA_IBIAS_INIT
    #define SET_CCFG_MODE_CONF_1_DELTA_IBIAS_INIT           0x0        // Delta = 0
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_1_DELTA_IBIAS_OFFSET
    #define SET_CCFG_MODE_CONF_1_DELTA_IBIAS_OFFSET         0x0        // Delta = 0
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_1_XOSC_MAX_START
    #define SET_CCFG_MODE_CONF_1_XOSC_MAX_START             0x10       // 1600us
    #endif
    
    //#####################################
    // Power settings
    //#####################################
    
    #ifndef SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_DELTA
    #define SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_DELTA        0xF        // Signed delta value +1 to apply to the VDDR_TRIM_SLEEP target (0xF=-1=default=no compensation)
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_DCDC_RECHARGE
    #define SET_CCFG_MODE_CONF_DCDC_RECHARGE                0x0        // Use the DC/DC during recharge in powerdown
    // #define SET_CCFG_MODE_CONF_DCDC_RECHARGE             0x1        // Do not use the DC/DC during recharge in powerdown
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_DCDC_ACTIVE
    #define SET_CCFG_MODE_CONF_DCDC_ACTIVE                  0x0        // Use the DC/DC during active mode
    // #define SET_CCFG_MODE_CONF_DCDC_ACTIVE               0x1        // Do not use the DC/DC during active mode
    #endif
    
    #if ( CCFG_FORCE_VDDR_HH )
    #define SET_CCFG_MODE_CONF_VDDS_BOD_LEVEL               0x1        // Special setting to enable forced VDDR HH voltage
    #else
    #ifndef SET_CCFG_MODE_CONF_VDDS_BOD_LEVEL
    // #define SET_CCFG_MODE_CONF_VDDS_BOD_LEVEL            0x0        // VDDS BOD level is 2.0V
    #define SET_CCFG_MODE_CONF_VDDS_BOD_LEVEL               0x1        // VDDS BOD level is 1.8V (or 1.65V for external regulator mode)
    #endif
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_VDDR_CAP
    #define SET_CCFG_MODE_CONF_VDDR_CAP                     0x3A       // Unsigned 8-bit integer representing the min. decoupling capacitance on VDDR in units of 100nF
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC
    #define SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC           0x1        // Temperature compensation on VDDR sleep trim disabled (default)
    // #define SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC        0x0        // Temperature compensation on VDDR sleep trim enabled
    #endif
    
    //#####################################
    // Clock settings
    //#####################################
    
    #ifndef SET_CCFG_MODE_CONF_SCLK_LF_OPTION
    // #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION            0x0        // LF clock derived from High Frequency XOSC
    // #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION            0x1        // External LF clock
    #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION               0x2        // LF XOSC
    // #define SET_CCFG_MODE_CONF_SCLK_LF_OPTION            0x3        // LF RCOSC
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_XOSC_CAP_MOD
    // #define SET_CCFG_MODE_CONF_XOSC_CAP_MOD              0x0        // Apply cap-array delta
    #define SET_CCFG_MODE_CONF_XOSC_CAP_MOD                 0x1        // Don't apply cap-array delta 
    #endif
    
    #ifndef SET_CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA
    #define SET_CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA          0xFF       // Signed 8-bit value, directly modifying trimmed XOSC cap-array value
    #endif
    
    #ifndef SET_CCFG_EXT_LF_CLK_DIO
    #define SET_CCFG_EXT_LF_CLK_DIO                         0x01       // DIO number if using external LF clock
    #endif
    
    #ifndef SET_CCFG_EXT_LF_CLK_RTC_INCREMENT
    #define SET_CCFG_EXT_LF_CLK_RTC_INCREMENT               0x800000   // RTC increment representing the external LF clock frequency
    #endif
    
    //#####################################
    // Special HF clock source setting
    //#####################################
    #ifndef SET_CCFG_MODE_CONF_XOSC_FREQ
    // #define SET_CCFG_MODE_CONF_XOSC_FREQ                 0x1        // Use HPOSC as HF source (Unavailable on CC13xx chips)
    // #define SET_CCFG_MODE_CONF_XOSC_FREQ                 0x2        // HF source is a 48 MHz xtal
    #define SET_CCFG_MODE_CONF_XOSC_FREQ                    0x3        // HF source is a 24 MHz xtal (default)
    #endif
    
    //#####################################
    // Bootloader settings
    //#####################################
    
    #ifndef SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE
    #define SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE            0x00       // Disable ROM boot loader
    // #define SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE         0xC5       // Enable ROM boot loader
    #endif
    
    #ifndef SET_CCFG_BL_CONFIG_BL_LEVEL
    // #define SET_CCFG_BL_CONFIG_BL_LEVEL                  0x0        // Active low to open boot loader backdoor
    #define SET_CCFG_BL_CONFIG_BL_LEVEL                     0x1        // Active high to open boot loader backdoor
    #endif
    
    #ifndef SET_CCFG_BL_CONFIG_BL_PIN_NUMBER
    #define SET_CCFG_BL_CONFIG_BL_PIN_NUMBER                0xFF       // DIO number for boot loader backdoor
    #endif
    
    #ifndef SET_CCFG_BL_CONFIG_BL_ENABLE
    // #define SET_CCFG_BL_CONFIG_BL_ENABLE                 0xC5       // Enabled boot loader backdoor
    #define SET_CCFG_BL_CONFIG_BL_ENABLE                    0xFF       // Disabled boot loader backdoor
    #endif
    
    //#####################################
    // Debug access settings
    //#####################################
    
    #ifndef SET_CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE
    #define SET_CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE           0x00       // Disable unlocking of TI FA option
    // #define SET_CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE        0xC5       // Enable unlocking of TI FA option with the unlock code
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE
    // #define SET_CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE       0x00       // Access disabled
    #define SET_CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE          0xC5       // Access enabled if also enabled in FCFG
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE
    #define SET_CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE         0x00       // Access disabled
    // #define SET_CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE      0xC5       // Access enabled if also enabled in FCFG
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE
    // #define SET_CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE      0x00       // Access disabled
    #define SET_CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE         0xC5       // Access enabled if also enabled in FCFG
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE
    #define SET_CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE       0x00       // Access disabled
    // #define SET_CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE    0xC5       // Access enabled if also enabled in FCFG
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE
    #define SET_CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE       0x00       // Access disabled
    // #define SET_CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE    0xC5       // Access enabled if also enabled in FCFG
    #endif
    
    #ifndef SET_CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE
    #define SET_CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE          0x00       // Access disabled
    // #define SET_CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE       0xC5       // Access enabled if also enabled in FCFG
    #endif
    
    //#####################################
    // Alternative IEEE 802.15.4 MAC address
    //#####################################
    #ifndef SET_CCFG_IEEE_MAC_0
    #define SET_CCFG_IEEE_MAC_0                             0xFFFFFFFF // Bits [31:0]
    #endif
    
    #ifndef SET_CCFG_IEEE_MAC_1
    #define SET_CCFG_IEEE_MAC_1                             0xFFFFFFFF // Bits [63:32]
    #endif
    
    //#####################################
    // Alternative BLE address
    //#####################################
    #ifndef SET_CCFG_IEEE_BLE_0
    #define SET_CCFG_IEEE_BLE_0                             0xFFFFFFFF // Bits [31:0]
    #endif
    
    #ifndef SET_CCFG_IEEE_BLE_1
    #define SET_CCFG_IEEE_BLE_1                             0xFFFFFFFF // Bits [63:32]
    #endif
    
    //#####################################
    // Flash erase settings
    //#####################################
    
    #ifndef SET_CCFG_ERASE_CONF_CHIP_ERASE_DIS_N
    // #define SET_CCFG_ERASE_CONF_CHIP_ERASE_DIS_N         0x0        // Any chip erase request detected during boot will be ignored
    #define SET_CCFG_ERASE_CONF_CHIP_ERASE_DIS_N            0x1        // Any chip erase request detected during boot will be performed by the boot FW
    #endif
    
    #ifndef SET_CCFG_ERASE_CONF_BANK_ERASE_DIS_N
    // #define SET_CCFG_ERASE_CONF_BANK_ERASE_DIS_N         0x0        // Disable the boot loader bank erase function
    #define SET_CCFG_ERASE_CONF_BANK_ERASE_DIS_N            0x1        // Enable the boot loader bank erase function
    #endif
    
    //#####################################
    // Flash image valid
    //#####################################
    #ifndef SET_CCFG_IMAGE_VALID_CONF_IMAGE_VALID
    #define SET_CCFG_IMAGE_VALID_CONF_IMAGE_VALID           0x00000000 // Flash image is valid
    // #define SET_CCFG_IMAGE_VALID_CONF_IMAGE_VALID        <non-zero> // Flash image is invalid, call bootloader
    #endif
    
    //#####################################
    // Flash sector write protection
    //#####################################
    #ifndef SET_CCFG_CCFG_PROT_31_0
    #define SET_CCFG_CCFG_PROT_31_0                         0xFFFFFFFF
    #endif
    
    #ifndef SET_CCFG_CCFG_PROT_63_32
    #define SET_CCFG_CCFG_PROT_63_32                        0xFFFFFFFF
    #endif
    
    #ifndef SET_CCFG_CCFG_PROT_95_64
    #define SET_CCFG_CCFG_PROT_95_64                        0xFFFFFFFF
    #endif
    
    #ifndef SET_CCFG_CCFG_PROT_127_96
    #define SET_CCFG_CCFG_PROT_127_96                       0xFFFFFFFF
    #endif
    
    //#####################################
    // Select between cache or GPRAM
    //#####################################
    #ifndef SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM
    // #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM        0x0        // Cache is disabled and GPRAM is available at 0x11000000-0x11001FFF
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM           0x1        // Cache is enabled and GPRAM is disabled (unavailable)
    #endif
    
    //#####################################
    // Select TCXO
    //#####################################
    #ifndef SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO            0x1    // Disable TCXO
    // #define SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO         0x0    // Enable TXCO
    #endif
    
    //*****************************************************************************
    //
    // CCFG values that should not be modified.
    //
    //*****************************************************************************
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_SIZE_OF_CCFG        0x0058
    #define SET_CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS       (CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS_M >> CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS_S)
    
    #if ( CCFG_FORCE_VDDR_HH )
    #define SET_CCFG_MODE_CONF_VDDR_EXT_LOAD                0x0        // Special setting to enable forced VDDR HH voltage
    #else
    #define SET_CCFG_MODE_CONF_VDDR_EXT_LOAD                0x1
    #endif
    
    #define SET_CCFG_MODE_CONF_RTC_COMP                     0x1
    #define SET_CCFG_MODE_CONF_HF_COMP                      0x1
    
    #define SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP45              0xFF
    #define SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP25              0xFF
    #define SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP5               0xFF
    #define SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TM15              0xFF
    
    #define SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP125             0xFF
    #define SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP105             0xFF
    #define SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP85              0xFF
    #define SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP65              0xFF
    
    #define SET_CCFG_RTC_OFFSET_RTC_COMP_P0                 0xFFFF
    #define SET_CCFG_RTC_OFFSET_RTC_COMP_P1                 0xFF
    #define SET_CCFG_RTC_OFFSET_RTC_COMP_P2                 0xFF
    
    #define SET_CCFG_FREQ_OFFSET_HF_COMP_P0                 0xFFFF
    #define SET_CCFG_FREQ_OFFSET_HF_COMP_P1                 0xFF
    #define SET_CCFG_FREQ_OFFSET_HF_COMP_P2                 0xFF
    
    //*****************************************************************************
    //
    // Concatenate bit fields to words.
    // DO NOT EDIT!
    //
    //*****************************************************************************
    #define DEFAULT_CCFG_EXT_LF_CLK          ( \
    	 ( ((uint32_t)( SET_CCFG_EXT_LF_CLK_DIO           << CCFG_EXT_LF_CLK_DIO_S           )) | ~CCFG_EXT_LF_CLK_DIO_M           ) & \
    	 ( ((uint32_t)( SET_CCFG_EXT_LF_CLK_RTC_INCREMENT << CCFG_EXT_LF_CLK_RTC_INCREMENT_S )) | ~CCFG_EXT_LF_CLK_RTC_INCREMENT_M ) )
         
    #define DEFAULT_CCFG_MODE_CONF_1         ( \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_1_ALT_DCDC_VMIN      << CCFG_MODE_CONF_1_ALT_DCDC_VMIN_S      )) | ~CCFG_MODE_CONF_1_ALT_DCDC_VMIN_M      ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN << CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN_S )) | ~CCFG_MODE_CONF_1_ALT_DCDC_DITHER_EN_M ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_1_ALT_DCDC_IPEAK     << CCFG_MODE_CONF_1_ALT_DCDC_IPEAK_S     )) | ~CCFG_MODE_CONF_1_ALT_DCDC_IPEAK_M     ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_1_DELTA_IBIAS_INIT   << CCFG_MODE_CONF_1_DELTA_IBIAS_INIT_S   )) | ~CCFG_MODE_CONF_1_DELTA_IBIAS_INIT_M   ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_1_DELTA_IBIAS_OFFSET << CCFG_MODE_CONF_1_DELTA_IBIAS_OFFSET_S )) | ~CCFG_MODE_CONF_1_DELTA_IBIAS_OFFSET_M ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_1_XOSC_MAX_START     << CCFG_MODE_CONF_1_XOSC_MAX_START_S     )) | ~CCFG_MODE_CONF_1_XOSC_MAX_START_M     ) )
    
    #define DEFAULT_CCFG_SIZE_AND_DIS_FLAGS  ( \
    	 ( ((uint32_t)( SET_CCFG_SIZE_AND_DIS_FLAGS_SIZE_OF_CCFG         << CCFG_SIZE_AND_DIS_FLAGS_SIZE_OF_CCFG_S         )) | ~CCFG_SIZE_AND_DIS_FLAGS_SIZE_OF_CCFG_M         ) & \
    	 ( ((uint32_t)( SET_CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS        << CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS_S        )) | ~CCFG_SIZE_AND_DIS_FLAGS_DISABLE_FLAGS_M        ) & \
    	 ( ((uint32_t)( SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO             << CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO_S             )) | ~CCFG_SIZE_AND_DIS_FLAGS_DIS_TCXO_M             ) & \
    	 ( ((uint32_t)( SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM            << CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM_S            )) | ~CCFG_SIZE_AND_DIS_FLAGS_DIS_GPRAM_M            ) & \
    	 ( ((uint32_t)( SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING << CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING_S )) | ~CCFG_SIZE_AND_DIS_FLAGS_DIS_ALT_DCDC_SETTING_M ) & \
    	 ( ((uint32_t)( SET_CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR         << CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR_S         )) | ~CCFG_SIZE_AND_DIS_FLAGS_DIS_XOSC_OVR_M         ) )
    
    #define DEFAULT_CCFG_MODE_CONF           ( \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_DELTA << CCFG_MODE_CONF_VDDR_TRIM_SLEEP_DELTA_S )) | ~CCFG_MODE_CONF_VDDR_TRIM_SLEEP_DELTA_M ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_DCDC_RECHARGE         << CCFG_MODE_CONF_DCDC_RECHARGE_S         )) | ~CCFG_MODE_CONF_DCDC_RECHARGE_M         ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_DCDC_ACTIVE           << CCFG_MODE_CONF_DCDC_ACTIVE_S           )) | ~CCFG_MODE_CONF_DCDC_ACTIVE_M           ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_VDDR_EXT_LOAD         << CCFG_MODE_CONF_VDDR_EXT_LOAD_S         )) | ~CCFG_MODE_CONF_VDDR_EXT_LOAD_M         ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_VDDS_BOD_LEVEL        << CCFG_MODE_CONF_VDDS_BOD_LEVEL_S        )) | ~CCFG_MODE_CONF_VDDS_BOD_LEVEL_M        ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_SCLK_LF_OPTION        << CCFG_MODE_CONF_SCLK_LF_OPTION_S        )) | ~CCFG_MODE_CONF_SCLK_LF_OPTION_M        ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC    << CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC_S    )) | ~CCFG_MODE_CONF_VDDR_TRIM_SLEEP_TC_M    ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_RTC_COMP              << CCFG_MODE_CONF_RTC_COMP_S              )) | ~CCFG_MODE_CONF_RTC_COMP_M              ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_XOSC_FREQ             << CCFG_MODE_CONF_XOSC_FREQ_S             )) | ~CCFG_MODE_CONF_XOSC_FREQ_M             ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_XOSC_CAP_MOD          << CCFG_MODE_CONF_XOSC_CAP_MOD_S          )) | ~CCFG_MODE_CONF_XOSC_CAP_MOD_M          ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_HF_COMP               << CCFG_MODE_CONF_HF_COMP_S               )) | ~CCFG_MODE_CONF_HF_COMP_M               ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA   << CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA_S   )) | ~CCFG_MODE_CONF_XOSC_CAPARRAY_DELTA_M   ) & \
    	 ( ((uint32_t)( SET_CCFG_MODE_CONF_VDDR_CAP              << CCFG_MODE_CONF_VDDR_CAP_S              )) | ~CCFG_MODE_CONF_VDDR_CAP_M              ) )
    
    #define DEFAULT_CCFG_VOLT_LOAD_0         ( \
    	 ( ((uint32_t)( SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP45 << CCFG_VOLT_LOAD_0_VDDR_EXT_TP45_S )) | ~CCFG_VOLT_LOAD_0_VDDR_EXT_TP45_M ) & \
    	 ( ((uint32_t)( SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP25 << CCFG_VOLT_LOAD_0_VDDR_EXT_TP25_S )) | ~CCFG_VOLT_LOAD_0_VDDR_EXT_TP25_M ) & \
    	 ( ((uint32_t)( SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TP5  << CCFG_VOLT_LOAD_0_VDDR_EXT_TP5_S  )) | ~CCFG_VOLT_LOAD_0_VDDR_EXT_TP5_M  ) & \
    	 ( ((uint32_t)( SET_CCFG_VOLT_LOAD_0_VDDR_EXT_TM15 << CCFG_VOLT_LOAD_0_VDDR_EXT_TM15_S )) | ~CCFG_VOLT_LOAD_0_VDDR_EXT_TM15_M ) )
    
    #define DEFAULT_CCFG_VOLT_LOAD_1         ( \
    	 ( ((uint32_t)( SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP125 << CCFG_VOLT_LOAD_1_VDDR_EXT_TP125_S )) | ~CCFG_VOLT_LOAD_1_VDDR_EXT_TP125_M ) & \
    	 ( ((uint32_t)( SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP105 << CCFG_VOLT_LOAD_1_VDDR_EXT_TP105_S )) | ~CCFG_VOLT_LOAD_1_VDDR_EXT_TP105_M ) & \
    	 ( ((uint32_t)( SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP85  << CCFG_VOLT_LOAD_1_VDDR_EXT_TP85_S  )) | ~CCFG_VOLT_LOAD_1_VDDR_EXT_TP85_M  ) & \
    	 ( ((uint32_t)( SET_CCFG_VOLT_LOAD_1_VDDR_EXT_TP65  << CCFG_VOLT_LOAD_1_VDDR_EXT_TP65_S  )) | ~CCFG_VOLT_LOAD_1_VDDR_EXT_TP65_M  ) )
    
    #define DEFAULT_CCFG_RTC_OFFSET          ( \
    	 ( ((uint32_t)( SET_CCFG_RTC_OFFSET_RTC_COMP_P0 << CCFG_RTC_OFFSET_RTC_COMP_P0_S )) | ~CCFG_RTC_OFFSET_RTC_COMP_P0_M ) & \
    	 ( ((uint32_t)( SET_CCFG_RTC_OFFSET_RTC_COMP_P1 << CCFG_RTC_OFFSET_RTC_COMP_P1_S )) | ~CCFG_RTC_OFFSET_RTC_COMP_P1_M ) & \
    	 ( ((uint32_t)( SET_CCFG_RTC_OFFSET_RTC_COMP_P2 << CCFG_RTC_OFFSET_RTC_COMP_P2_S )) | ~CCFG_RTC_OFFSET_RTC_COMP_P2_M ) )
    
    #define DEFAULT_CCFG_FREQ_OFFSET         ( \
    	 ( ((uint32_t)( SET_CCFG_FREQ_OFFSET_HF_COMP_P0 << CCFG_FREQ_OFFSET_HF_COMP_P0_S )) | ~CCFG_FREQ_OFFSET_HF_COMP_P0_M ) & \
    	 ( ((uint32_t)( SET_CCFG_FREQ_OFFSET_HF_COMP_P1 << CCFG_FREQ_OFFSET_HF_COMP_P1_S )) | ~CCFG_FREQ_OFFSET_HF_COMP_P1_M ) & \
    	 ( ((uint32_t)( SET_CCFG_FREQ_OFFSET_HF_COMP_P2 << CCFG_FREQ_OFFSET_HF_COMP_P2_S )) | ~CCFG_FREQ_OFFSET_HF_COMP_P2_M ) )
    
    #define DEFAULT_CCFG_IEEE_MAC_0          SET_CCFG_IEEE_MAC_0
    #define DEFAULT_CCFG_IEEE_MAC_1          SET_CCFG_IEEE_MAC_1
    #define DEFAULT_CCFG_IEEE_BLE_0          SET_CCFG_IEEE_BLE_0
    #define DEFAULT_CCFG_IEEE_BLE_1          SET_CCFG_IEEE_BLE_1
    
    #define DEFAULT_CCFG_BL_CONFIG           ( \
    	 ( ((uint32_t)( SET_CCFG_BL_CONFIG_BOOTLOADER_ENABLE << CCFG_BL_CONFIG_BOOTLOADER_ENABLE_S )) | ~CCFG_BL_CONFIG_BOOTLOADER_ENABLE_M ) & \
    	 ( ((uint32_t)( SET_CCFG_BL_CONFIG_BL_LEVEL          << CCFG_BL_CONFIG_BL_LEVEL_S          )) | ~CCFG_BL_CONFIG_BL_LEVEL_M          ) & \
    	 ( ((uint32_t)( SET_CCFG_BL_CONFIG_BL_PIN_NUMBER     << CCFG_BL_CONFIG_BL_PIN_NUMBER_S     )) | ~CCFG_BL_CONFIG_BL_PIN_NUMBER_M     ) & \
    	 ( ((uint32_t)( SET_CCFG_BL_CONFIG_BL_ENABLE         << CCFG_BL_CONFIG_BL_ENABLE_S         )) | ~CCFG_BL_CONFIG_BL_ENABLE_M         ) )
    
    #define DEFAULT_CCFG_ERASE_CONF          ( \
    	 ( ((uint32_t)( SET_CCFG_ERASE_CONF_CHIP_ERASE_DIS_N << CCFG_ERASE_CONF_CHIP_ERASE_DIS_N_S )) | ~CCFG_ERASE_CONF_CHIP_ERASE_DIS_N_M ) & \
    	 ( ((uint32_t)( SET_CCFG_ERASE_CONF_BANK_ERASE_DIS_N << CCFG_ERASE_CONF_BANK_ERASE_DIS_N_S )) | ~CCFG_ERASE_CONF_BANK_ERASE_DIS_N_M ) )
    
    #define DEFAULT_CCFG_CCFG_TI_OPTIONS     ( \
    	 ( ((uint32_t)( SET_CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE << CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE_S )) | ~CCFG_CCFG_TI_OPTIONS_TI_FA_ENABLE_M ) )
    
    #define DEFAULT_CCFG_CCFG_TAP_DAP_0      ( \
    	 ( ((uint32_t)( SET_CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE  << CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE_S  )) | ~CCFG_CCFG_TAP_DAP_0_CPU_DAP_ENABLE_M  ) & \
    	 ( ((uint32_t)( SET_CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE << CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE_S )) | ~CCFG_CCFG_TAP_DAP_0_PRCM_TAP_ENABLE_M ) & \
    	 ( ((uint32_t)( SET_CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE << CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE_S )) | ~CCFG_CCFG_TAP_DAP_0_TEST_TAP_ENABLE_M ) )
    
    #define DEFAULT_CCFG_CCFG_TAP_DAP_1      ( \
    	 ( ((uint32_t)( SET_CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE << CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE_S )) | ~CCFG_CCFG_TAP_DAP_1_PBIST2_TAP_ENABLE_M ) & \
    	 ( ((uint32_t)( SET_CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE << CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE_S )) | ~CCFG_CCFG_TAP_DAP_1_PBIST1_TAP_ENABLE_M ) & \
    	 ( ((uint32_t)( SET_CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE    << CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE_S    )) | ~CCFG_CCFG_TAP_DAP_1_WUC_TAP_ENABLE_M    ) )
    
    #define DEFAULT_CCFG_IMAGE_VALID_CONF    ( \
    	 ( ((uint32_t)( SET_CCFG_IMAGE_VALID_CONF_IMAGE_VALID << CCFG_IMAGE_VALID_CONF_IMAGE_VALID_S )) | ~CCFG_IMAGE_VALID_CONF_IMAGE_VALID_M ) )
    
    #define DEFAULT_CCFG_CCFG_PROT_31_0      SET_CCFG_CCFG_PROT_31_0  
    #define DEFAULT_CCFG_CCFG_PROT_63_32     SET_CCFG_CCFG_PROT_63_32 
    #define DEFAULT_CCFG_CCFG_PROT_95_64     SET_CCFG_CCFG_PROT_95_64 
    #define DEFAULT_CCFG_CCFG_PROT_127_96    SET_CCFG_CCFG_PROT_127_96
    
    //*****************************************************************************
    //
    // Customer Configuration Area in Lock Page
    //
    //*****************************************************************************
    #if defined(__IAR_SYSTEMS_ICC__)
    __root const ccfg_t __ccfg @ ".ccfg" =
    #elif defined(__TI_COMPILER_VERSION__)
    #pragma DATA_SECTION(__ccfg, ".ccfg")
    #pragma RETAIN(__ccfg)
    const ccfg_t __ccfg =
    #else
    const ccfg_t __ccfg __attribute__((section(".ccfg"))) __attribute__((used)) =
    #endif
    {                                     // Mapped to address
        DEFAULT_CCFG_EXT_LF_CLK         , // 0x50003FA8 (0x50003xxx maps to last
        DEFAULT_CCFG_MODE_CONF_1        , // 0x50003FAC  sector in FLASH.
        DEFAULT_CCFG_SIZE_AND_DIS_FLAGS , // 0x50003FB0  Independent of FLASH size)
        DEFAULT_CCFG_MODE_CONF          , // 0x50003FB4
        DEFAULT_CCFG_VOLT_LOAD_0        , // 0x50003FB8 
        DEFAULT_CCFG_VOLT_LOAD_1        , // 0x50003FBC
        DEFAULT_CCFG_RTC_OFFSET         , // 0x50003FC0
        DEFAULT_CCFG_FREQ_OFFSET        , // 0x50003FC4
        DEFAULT_CCFG_IEEE_MAC_0         , // 0x50003FC8
        DEFAULT_CCFG_IEEE_MAC_1         , // 0x50003FCC
        DEFAULT_CCFG_IEEE_BLE_0         , // 0x50003FD0
        DEFAULT_CCFG_IEEE_BLE_1         , // 0x50003FD4
        DEFAULT_CCFG_BL_CONFIG          , // 0x50003FD8
        DEFAULT_CCFG_ERASE_CONF         , // 0x50003FDC
        DEFAULT_CCFG_CCFG_TI_OPTIONS    , // 0x50003FE0
        DEFAULT_CCFG_CCFG_TAP_DAP_0     , // 0x50003FE4
        DEFAULT_CCFG_CCFG_TAP_DAP_1     , // 0x50003FE8
        DEFAULT_CCFG_IMAGE_VALID_CONF   , // 0x50003FEC
        DEFAULT_CCFG_CCFG_PROT_31_0     , // 0x50003FF0
        DEFAULT_CCFG_CCFG_PROT_63_32    , // 0x50003FF4
        DEFAULT_CCFG_CCFG_PROT_95_64    , // 0x50003FF8
        DEFAULT_CCFG_CCFG_PROT_127_96   , // 0x50003FFC
    };
    

    .cfg

    /*
     * Copyright (c) 2015-2016, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    
    
    /* ================ Boot configuration ================ */
    var Boot = xdc.useModule('ti.sysbios.family.arm.cc26xx.Boot');
    /*
     * This module contains family specific Boot APIs and configuration settings.
     * See the SYS/BIOS API guide for more information.
     */
    
    
    
    /* ================ Clock configuration ================ */
    var Clock = xdc.useModule('ti.sysbios.knl.Clock');
    /*
     * When using Power and calibrateRCOSC is set to true, this should be set to 10.
     * The timer used by the Clock module supports TickMode_DYNAMIC. This enables us
     * to set the tick period to 10 us without generating the overhead of additional
     * interrupts.
     *
     * Note: The calibrateRCOSC parameter is set within the Power configuration
     *     structure in the "Board.c" file.
     */
    Clock.tickPeriod = 10;
    
    
    
    /* ================ Defaults (module) configuration ================ */
    var Defaults = xdc.useModule('xdc.runtime.Defaults');
    /*
     * A flag to allow module names to be loaded on the target. Module name
     * strings are placed in the .const section for debugging purposes.
     *
     * Pick one:
     *  - true (default)
     *      Setting this parameter to true will include name strings in the .const
     *      section so that Errors and Asserts are easier to debug.
     *  - false
     *      Setting this parameter to false will reduce footprint in the .const
     *      section. As a result, Error and Assert messages will contain an
     *      "unknown module" prefix instead of the actual module name.
     *
     *  When using BIOS in ROM:
     *      This option must be set to false.
     */
    //Defaults.common$.namedModule = true;
    Defaults.common$.namedModule = false;
    
    
    
    /* ================ Error configuration ================ */
    var Error = xdc.useModule('xdc.runtime.Error');
    /*
     * This function is called to handle all raised errors, but unlike
     * Error.raiseHook, this function is responsible for completely handling the
     * error with an appropriately initialized Error_Block.
     *
     * Pick one:
     *  - Error.policyDefault (default)
     *      Calls Error.raiseHook with an initialized Error_Block structure and logs
     *      the error using the module's logger.
     *  - Error.policySpin
     *      Simple alternative that traps on a while(1) loop for minimized target
     *      footprint.
     *      Using Error.policySpin, the Error.raiseHook will NOT called.
     */
    //Error.policyFxn = Error.policyDefault;
    Error.policyFxn = Error.policySpin;
    
    /*
     * If Error.policyFxn is set to Error.policyDefault, this function is called
     * whenever an error is raised by the Error module.
     *
     * Pick one:
     *  - Error.print (default)
     *      Errors are formatted and output via System_printf() for easier
     *      debugging.
     *  - null
     *      Errors are not formatted or logged. This option reduces code footprint.
     *  - non-null function
     *      Errors invoke custom user function. See the Error module documentation
     *      for more details.
     */
    //Error.raiseHook = Error.print;
    Error.raiseHook = null;
    //Error.raiseHook = "&myErrorFxn";
    
    /*
     * If Error.policyFxn is set to Error.policyDefault, this option applies to the
     * maximum number of times the Error.raiseHook function can be recursively
     * invoked. This option limits the possibility of an infinite recursion that
     * could lead to a stack overflow.
     * The default value is 16.
     */
    Error.maxDepth = 2;
    
    
    
    /* ================ Hwi configuration ================ */
    var halHwi = xdc.useModule('ti.sysbios.hal.Hwi');
    var m3Hwi = xdc.useModule('ti.sysbios.family.arm.m3.Hwi');
    /*
     * Checks for Hwi (system) stack overruns while in the Idle loop.
     *
     * Pick one:
     *  - true (default)
     *      Checks the top word for system stack overflows during the idle loop and
     *      raises an Error if one is detected.
     *  - false
     *      Disabling the runtime check improves runtime performance and yields a
     *      reduced flash footprint.
     */
    //halHwi.checkStackFlag = true;
    halHwi.checkStackFlag = false;
    
    /*
     * The following options alter the system's behavior when a hardware exception
     * is detected.
     *
     * Pick one:
     *  - Hwi.enableException = true
     *      This option causes the default m3Hwi.excHandlerFunc function to fully
     *      decode an exception and dump the registers to the system console.
     *      This option raises errors in the Error module and displays the
     *      exception in ROV.
     *  - Hwi.enableException = false
     *      This option reduces code footprint by not decoding or printing the
     *      exception to the system console.
     *      It however still raises errors in the Error module and displays the
     *      exception in ROV.
     *  - Hwi.excHandlerFunc = null
     *      This is the most aggressive option for code footprint savings; but it
     *      can difficult to debug exceptions. It reduces flash footprint by
     *      plugging in a default while(1) trap when exception occur. This option
     *      does not raise an error with the Error module.
     */
    //m3Hwi.enableException = true;
    //m3Hwi.enableException = false;
    m3Hwi.excHandlerFunc = null;
    
    /*
     * Enable hardware exception generation when dividing by zero.
     *
     * Pick one:
     *  - 0 (default)
     *      Disables hardware exceptions when dividing by zero
     *  - 1
     *      Enables hardware exceptions when dividing by zero
     */
    m3Hwi.nvicCCR.DIV_0_TRP = 0;
    //m3Hwi.nvicCCR.DIV_0_TRP = 1;
    
    /*
     * Enable hardware exception generation for invalid data alignment.
     *
     * Pick one:
     *  - 0 (default)
     *      Disables hardware exceptions for data alignment
     *  - 1
     *      Enables hardware exceptions for data alignment
     */
    m3Hwi.nvicCCR.UNALIGN_TRP = 0;
    //m3Hwi.nvicCCR.UNALIGN_TRP = 1;
    
    /*
     * Assign an address for the reset vector.
     *
     * Default is 0x0, which is the start of Flash. Ordinarily this setting should
     * not be changed.
     */
    m3Hwi.resetVectorAddress = 0x0;
    
    /*
     * Assign an address for the vector table in RAM.
     *
     * The default is the start of RAM. This table is placed in RAM so interrupts
     * can be added at runtime.
     *
     * Note: To change, verify address in the device specific datasheets'
     *     memory map.
     */
    m3Hwi.vectorTableAddress = 0x20000000;
    
    
    
    /* ================ Idle configuration ================ */
    var Idle = xdc.useModule('ti.sysbios.knl.Idle');
    /*
     * The Idle module is used to specify a list of functions to be called when no
     * other tasks are running in the system.
     *
     * Functions added here will be run continuously within the idle task.
     *
     * Function signature:
     *     Void func(Void);
     */
    //Idle.addFunc("&myIdleFunc");
    
    
    
    /* ================ Kernel (SYS/BIOS) configuration ================ */
    var BIOS = xdc.useModule('ti.sysbios.BIOS');
    /*
     * Enable asserts in the BIOS library.
     *
     * Pick one:
     *  - true (default)
     *      Enables asserts for debugging purposes.
     *  - false
     *      Disables asserts for a reduced code footprint and better performance.
     *
     *  When using BIOS in ROM:
     *      This option must be set to false.
     */
    //BIOS.assertsEnabled = true;
    BIOS.assertsEnabled = false;
    
    /*
     * Specify default heap size for BIOS.
     */
    BIOS.heapSize = 1024;
    
    /*
     * Specify default CPU Frequency.
     */
    BIOS.cpuFreq.lo = 48000000;
    
    /*
     * A flag to determine if xdc.runtime sources are to be included in a custom
     * built BIOS library.
     *
     * Pick one:
     *  - false (default)
     *      The pre-built xdc.runtime library is provided by the respective target
     *      used to build the application.
     *  - true
     *      xdc.runtime library sources are to be included in the custom BIOS
     *      library. This option yields the most efficient library in both code
     *      footprint and runtime performance.
     */
    //BIOS.includeXdcRuntime = false;
    BIOS.includeXdcRuntime = true;
    
    /*
     * The SYS/BIOS runtime is provided in the form of a library that is linked
     * with the application. Several forms of this library are provided with the
     * SYS/BIOS product.
     *
     * Pick one:
     *   - BIOS.LibType_Custom
     *      Custom built library that is highly optimized for code footprint and
     *      runtime performance.
     *   - BIOS.LibType_Debug
     *      Custom built library that is non-optimized that can be used to
     *      single-step through APIs with a debugger.
     *
     */
    BIOS.libType = BIOS.LibType_Custom;
    //BIOS.libType = BIOS.LibType_Debug;
    
    /*
     * Runtime instance creation enable flag.
     *
     * Pick one:
     *   - true (default)
     *      Allows Mod_create() and Mod_delete() to be called at runtime which
     *      requires a default heap for dynamic memory allocation.
     *   - false
     *      Reduces code footprint by disallowing Mod_create() and Mod_delete() to
     *      be called at runtime. Object instances are constructed via
     *      Mod_construct() and destructed via Mod_destruct().
     *
     *  When using BIOS in ROM:
     *      This option must be set to true.
     */
    BIOS.runtimeCreatesEnabled = true;
    //BIOS.runtimeCreatesEnabled = false;
    
    /*
     * Enable logs in the BIOS library.
     *
     * Pick one:
     *  - true (default)
     *      Enables logs for debugging purposes.
     *  - false
     *      Disables logging for reduced code footprint and improved runtime
     *      performance.
     *
     *  When using BIOS in ROM:
     *      This option must be set to false.
     */
    //BIOS.logsEnabled = true;
    BIOS.logsEnabled = false;
    
    
    
    /* ================ Memory configuration ================ */
    var Memory = xdc.useModule('xdc.runtime.Memory');
    /*
     * The Memory module itself simply provides a common interface for any
     * variety of system and application specific memory management policies
     * implemented by the IHeap modules(Ex. HeapMem, HeapBuf).
     */
    
    
    
    /* ================ Program configuration ================ */
    /*
     *  Program.stack is ignored with IAR. Use the project options in
     *  IAR Embedded Workbench to alter the system stack size.
     */
    if (!Program.build.target.$name.match(/iar/)) {
        /*
         *  Reducing the system stack size (used by ISRs and Swis) to reduce
         *  RAM usage.
         */
        Program.stack = 768;
    }
    
    
    
    /*
     * Uncomment to enable Semihosting for GNU targets to print to the CCS console.
     * Please read the following TIRTOS Wiki page for more information on Semihosting:
     * processors.wiki.ti.com/.../TI-RTOS_Examples_SemiHosting
     */
    
    if (Program.build.target.$name.match(/gnu/)) {
        //var SemiHost = xdc.useModule('ti.sysbios.rts.gnu.SemiHostSupport');
    }
    
    /* ================ ROM configuration ================ */
    /*
     * To use BIOS in flash, comment out the code block below.
     */
    var ROM = xdc.useModule('ti.sysbios.rom.ROM');
    if (Program.cpu.deviceName.match(/CC26/)) {
        ROM.romName = ROM.CC2650;
    }
    else if (Program.cpu.deviceName.match(/CC13/)) {
        ROM.romName = ROM.CC1350;
    }
    
    
    
    /* ================ Semaphore configuration ================ */
    var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
    /*
     * Enables global support for Task priority pend queuing.
     *
     * Pick one:
     *  - true (default)
     *      This allows pending tasks to be serviced based on their task priority.
     *  - false
     *      Pending tasks are services based on first in, first out basis.
     *
     *  When using BIOS in ROM:
     *      This option must be set to false.
     */
    //Semaphore.supportsPriority = true;
    Semaphore.supportsPriority = false;
    
    /*
     * Allows for the implicit posting of events through the semaphore,
     * disable for additional code saving.
     *
     * Pick one:
     *  - true
     *      This allows the Semaphore module to post semaphores and events
     *      simultaneously.
     *  - false (default)
     *      Events must be explicitly posted to unblock tasks.
     *
     *  When using BIOS in ROM:
     *      This option must be set to false.
     */
    //Semaphore.supportsEvents = true;
    Semaphore.supportsEvents = false;
    
    
    /* ================ Event configuration ================ */
    var Event = xdc.useModule('ti.sysbios.knl.Event');
    
    
    /* ================ Swi configuration ================ */
    var Swi = xdc.useModule('ti.sysbios.knl.Swi');
    /*
     * A software interrupt is an object that encapsulates a function to be
     * executed and a priority. Software interrupts are prioritized, preempt tasks
     * and are preempted by hardware interrupt service routines.
     *
     * This module is included to allow Swi's in a users' application.
     */
    
    /*
     * Reduce the number of swi priorities from the default of 16.
     * Decreasing the number of swi priorities yields memory savings.
     */
    Swi.numPriorities = 6;
    
    
    
    /* ================ System configuration ================ */
    var System = xdc.useModule('xdc.runtime.System');
    /*
     * The Abort handler is called when the system exits abnormally.
     *
     * Pick one:
     *  - System.abortStd (default)
     *      Call the ANSI C Standard 'abort()' to terminate the application.
     *  - System.abortSpin
     *      A lightweight abort function that loops indefinitely in a while(1) trap
     *      function.
     *  - A custom abort handler
     *      A user-defined function. See the System module documentation for
     *      details.
     */
    //System.abortFxn = System.abortStd;
    System.abortFxn = System.abortSpin;
    //System.abortFxn = "&myAbortSystem";
    
    /* Enable System_printf() to display floats. */
    System.extendedFormats = '%f%$S';
    
    /*
     * The Exit handler is called when the system exits normally.
     *
     * Pick one:
     *  - System.exitStd (default)
     *      Call the ANSI C Standard 'exit()' to terminate the application.
     *  - System.exitSpin
     *      A lightweight exit function that loops indefinitely in a while(1) trap
     *      function.
     *  - A custom exit function
     *      A user-defined function. See the System module documentation for
     *      details.
     */
    //System.exitFxn = System.exitStd;
    System.exitFxn = System.exitSpin;
    //System.exitFxn = "&myExitSystem";
    
    /*
     * Minimize exit handler array in the System module. The System module includes
     * an array of functions that are registered with System_atexit() which is
     * called by System_exit(). The default value is 8.
     */
    System.maxAtexitHandlers = 0;
    
    /*
     * The System.SupportProxy defines a low-level implementation of System
     * functions such as System_printf(), System_flush(), etc.
     *
     * Pick one pair:
     *  - SysMin
     *      This module maintains an internal configurable circular buffer that
     *      stores the output until System_flush() is called.
     *      The size of the circular buffer is set via SysMin.bufSize.
     *  - SysCallback
     *      SysCallback allows for user-defined implementations for System APIs.
     *      The SysCallback support proxy has a smaller code footprint and can be
     *      used to supply custom System_printf services.
     *      The default SysCallback functions point to stub functions. See the
     *      SysCallback module's documentation.
     */
    //var SysMin = xdc.useModule('xdc.runtime.SysMin');
    //SysMin.bufSize = 128;
    //System.SupportProxy = SysMin;
    var SysCallback = xdc.useModule('xdc.runtime.SysCallback');
    System.SupportProxy = SysCallback;
    //SysCallback.abortFxn = "&myUserAbort";
    //SysCallback.exitFxn  = "&myUserExit";
    //SysCallback.flushFxn = "&myUserFlush";
    //SysCallback.putchFxn = "&myUserPutch";
    //SysCallback.readyFxn = "&myUserReady";
    
    
    
    /* ================ Task configuration ================ */
    var Task = xdc.useModule('ti.sysbios.knl.Task');
    /*
     * Check task stacks for overflow conditions.
     *
     * Pick one:
     *  - true (default)
     *      Enables runtime checks for task stack overflow conditions during
     *      context switching ("from" and "to")
     *  - false
     *      Disables runtime checks for task stack overflow conditions.
     *
     *  When using BIOS in ROM:
     *      This option must be set to false.
     */
    //Task.checkStackFlag = true;
    Task.checkStackFlag = false;
    
    /*
     * Set the default task stack size when creating tasks.
     *
     * The default is dependent on the device being used. Reducing the default stack
     * size yields greater memory savings.
     */
    Task.defaultStackSize = 512;
    
    /*
     * Enables the idle task.
     *
     * Pick one:
     *  - true (default)
     *      Creates a task with priority of 0 which calls idle hook functions. This
     *      option must be set to true to gain power savings provided by the Power
     *      module.
     *  - false
     *      No idle task is created. This option consumes less memory as no
     *      additional default task stack is needed.
     *      To gain power savings by the Power module without having the idle task,
     *      add Idle.run as the Task.allBlockedFunc.
     */
    Task.enableIdleTask = true;
    //Task.enableIdleTask = false;
    //Task.allBlockedFunc = Idle.run;
    
    /*
     * If Task.enableIdleTask is set to true, this option sets the idle task's
     * stack size.
     *
     * Reducing the idle stack size yields greater memory savings.
     */
    Task.idleTaskStackSize = 512;
    
    /*
     * Reduce the number of task priorities.
     * The default is 16.
     * Decreasing the number of task priorities yield memory savings.
     */
    Task.numPriorities = 6;
    
    /* ================ TI-RTOS drivers' configuration ================ */
    var driversConfig = xdc.useModule('ti.drivers.Config');
    /*
     * Include TI-RTOS drivers
     *
     * Pick one:
     *  - driversConfig.LibType_NonInstrumented (default)
     *      Use TI-RTOS drivers library optimized for footprint and performance
     *      without asserts or logs.
     *  - driversConfig.LibType_Instrumented
     *      Use TI-RTOS drivers library for debugging with asserts and logs enabled.
     */
     
     
    /* ================ Text configuration ================ */
    var Text = xdc.useModule('xdc.runtime.Text');
    /*
     * These strings are placed in the .const section. Setting this parameter to
     * false will save space in the .const section. Error, Assert and Log messages
     * will print raw ids and args instead of a formatted message.
     *
     * Pick one:
     *  - true (default)
     *      This option loads test string into the .const for easier debugging.
     *  - false
     *      This option reduces the .const footprint.
     */
    //Text.isLoaded = true;
    Text.isLoaded = false;
    
    
    
    /* ================ Types configuration ================ */
    var Types = xdc.useModule('xdc.runtime.Types');
    /*
     * This module defines basic constants and types used throughout the
     * xdc.runtime package.
     */
    
    
    
    /* ================ Application Specific Instances ================ */
    
    /* ================ Diagnostics configuration ================ */
    //var Diags = xdc.useModule('xdc.runtime.Diags');
    /*
     * You use the Diags module to set and clear bits in a module's diagnostics
     * mask for the purpose of controlling diagnostics within that module. A
     * module diagnostics mask controls both Assert and Log statements
     * within that module, disabling these statements yields
     * code savings.
     */
    
    /* ================ Logging configuration ================ */
    //var Log = xdc.useModule('xdc.runtime.Log');
    /*
     * Modules and the application code generate Log_Event events by calling
     * the Log module's functions.
     * Disabling all Log statements here will allow the optimizer to completely
     * remove all Log code from the application.
     *
     * Note: In order to generate Log events in your application both the Diags
     *       and the Log mask must be set. See the SYS/BIOS API guide for
     *       more information.
     */
    
    /*
     * LoggingSetup configures TI-RTOS modules to capture user-specified information
     * such as CPU Load, Task Load and Task Execution so that it can be
     * displayed by System Analyzer.
     */
    //var LoggingSetup = xdc.useModule('ti.uia.sysbios.LoggingSetup');
    //LoggingSetup.loadLoggerSize = 256;
    //LoggingSetup.mainLoggerSize = 512;
    //LoggingSetup.sysbiosLoggerSize = 1024;
    
    /* ================ Main configuration ================ */
    var Main = xdc.useModule('xdc.runtime.Main');
    /*  Configuration of this Main module is used for all code not in a module */
    
    
    
    /* ================ POSIX configuration ================ */
    //var Settings = xdc.useModule('ti.posix.tirtos.Settings');
    
    if (Program.build.target.$name.match(/iar/)) {
        /* 
         * For the IAR target, the 'ti.posix.tirtos.Settings' uses the
         * MultithreadSupport module. By default, the MultithreadSupport module
         * use the '--threaded_lib' library which provides a separate 'errno'
         * per thread and makes other rts libraries reentrant. This library has
         * a larger footprint which can be a problem for some apps, so we
         * override the default and disable it here.
         */
        var MultithreadSupport = 
            xdc.useModule('ti.sysbios.rts.iar.MultithreadSupport');
        MultithreadSupport.enableMultithreadSupport = false;
    }
    
    /* ================ Event configuration ================ */
    var Event = xdc.useModule('ti.sysbios.knl.Event');
    
    
    
    /* ================ Mailbox configuration ================ */
    var Mailbox = xdc.useModule('ti.sysbios.knl.Mailbox');
     
    var Settings = xdc.useModule('ti.sysbios.posix.Settings');

  • - For how to adapt to a custom board: https://dev.ti.com/tirex/content/simplelink_cc13x0_sdk_4_10_01_01/docs/proprietary-rf/proprietary-rf-users-guide/proprietary-rf-guide/custom-hardware.html#dio-mapping

    - You are using a very old version of SW. Use this version: https://dev.ti.com/tirex/explore/node?node=AFUdF2MFjhZ-sEr1NZrjvw__eCfARaV__LATEST

    - Do you have the debugger connected when you measure current? If that is the case the chip will not be able to go down to the lowest power level

  •  - I converted  the pinstandby example with your help TER, consumption is the same as my own codes.  

    - I referenced similar SDK as you mentioned while working on pinstandby example. I will try to update my custom board's code.

    - I am not using debugger, just powering my custom board.

  • Could you refer to the exact post where I have helped you before? 

  • I have just given some clues about my project. It is below.  I still have this problem, I can see received datas, I can't see sent datas while debugging, but it is not much more important than this topic now.

    e2e.ti.com/.../972319

  • I could not find any mention of this " I converted  the pinstandby example with your help TER, consumption is the same as my own codes.  " in the posts from you? The only posts I can see is basic debug posts. 

  • I wrote about your previous message on this post. You said " - For how to adapt to a custom board: https://dev.ti.com/tirex/content/simplelink_cc13x0_sdk_4_10_01_01/docs/proprietary-rf/proprietary-rf-users-guide/proprietary-rf-guide/custom-hardware.html#dio-mapping " . pinStandby example was not working on my side as I said in the first message. I did somethings according to this document and it is working now. There is no post about pinstandby asked by me before. I just wanted to say your solution about pinstandby example on custom board helped me.

  • One step back: Do you see high current consumption when you run the pinstandby on your custom hardware after you modified the pin table? 

    Have you ensured that the CC1190 is in power down? 

  • Yes, I just opened the led pin and no another pin was opened. I see same consumption, I didn't configure cc1190 pins, could it be powered while not using it pins ?

  • If you require low current on your board, all part of the board has to be in power down, including CC1190. You have to set the control signals to CC1190 to ensure PD. 

  • I have another board with CC1310 and without CC1190, with same code power consumption is same. There is no CC1190, there is just cc1310, but I still see same consumption level.

  • Would it be possible to share the schematic of the board with just the CC1310? 

  • Is it possible to share it just with you ?

  • I accepted the friend request. Just send it to me in a private message.  

  • Hi TER, now I am working on power consumption again. Reason of the high power consumption is tantalum capacitors. We changed them with seramic ones and now it is consuming about 1 uA in sleep mode. Thanks for your help.