Since we are currently in the test lab we need to find an answer for this quickly.
1.) How is the long range mode intended to be used since it is not meeting 500KHz bandwith and therefore not FCC compliant?
2.) How do we setup the receive mode in the radio command API for certification testing. It is a Part 15B requirement to pass radiated spurious emissions with the radio receiver ON if the radio operates below 960MHz.