Other Parts Discussed in Thread: CC1101
Hi,
I have a question if the optional radio control feature is included in CC113L also.
According to CC1101 or CC11x1-Q1 datasheets, the description about this feature is on pages 34 or 28. However, there is no description on CC113L datasheet. Does it mean that the feature is not included in CC113L? If Yes, I think that no longer meaning to "Set SCLK=1 and SI=0" at the initial step in the manual reset sequence which is stated on page 37 of CC113L datasheet.
Regards,
Sinsan