This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: reset level

Part Number: CC1310

Hello,
what is the voltage level to for the reset pin to go into reset state and also for coming out? Are these the same like for the GPIOs?

VDDS=1.8V

VDDS=3.8V

Is the reset pin with hysteresis or without?

Regards, Holger