Other Parts Discussed in Thread: CC1190
We are testing the indoor range of two CC13-90 boards with the rfPacketErrorRate Example.
The example seems to run with 25 dBm on Rx and Tx.
I only see 26dBm option in the table (file: smartrf_settings_predefined.c):
RF_TxPowerTable_Entry RF_PROP_txPowerTableREUS[RF_PROP_TX_POWER_TABLE_SIZE_REUS] = { {7, RF_TxPowerTable_DEFAULT_PA_ENTRY(0, 3, 0, 0) }, {14, RF_TxPowerTable_DEFAULT_PA_ENTRY(1, 3, 0, 0) }, {18, RF_TxPowerTable_DEFAULT_PA_ENTRY(2, 3, 0, 0) }, {20, RF_TxPowerTable_DEFAULT_PA_ENTRY(3, 3, 0, 0) }, {22, RF_TxPowerTable_DEFAULT_PA_ENTRY(4, 3, 0, 0) }, {23, RF_TxPowerTable_DEFAULT_PA_ENTRY(5, 3, 0, 0) }, {24, RF_TxPowerTable_DEFAULT_PA_ENTRY(6, 3, 0, 0) }, {25, RF_TxPowerTable_DEFAULT_PA_ENTRY(9, 3, 0, 0) }, {26, RF_TxPowerTable_DEFAULT_PA_ENTRY(14, 3, 0, 0) }, RF_TxPowerTable_TERMINATION_ENTRY };
How can I enable 27dBm on the Tx side and max gain at the Rx side?
We are using Simple Link Long range 915 Mhz.