Other Parts Discussed in Thread: CC1352R, CC1350, CC1310, ENERGYTRACE, CC1312R
Hey guys,
we want to design our board based on the CC1352R1 Launchpad. Since we are basically satisfied with the performance we are planning to remove the whole energy trace stuff and keep most of the rest.
What we need is obviously the CC1352R1 chip and the RF path for the sub GHz application. Besides, we keep the XDS Probe circutry to be able to flash the device via USB. Both mini JTAG Header will be removed as well. Since we do not have an altium licence (re-design will be outsourced) I was wondering if
- we can simply remove all the energy trace stuff (all from page 5 + 6 of the rev. B schematics of the launchpad) without further adaptions
- and is there a possibilty to view the board files with EAGLE?
- Is there a recommendable replacement for the RF frequency filter? According to Murata, this device is currently not available on the market. I found this so far: LFD21892MDP2B860
Best wishes
Slev1n