This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1312R1: Do TI have any time of releasing wmbus patch on CC1312?

Part Number: LAUNCHXL-CC1312R1
Other Parts Discussed in Thread: CC1350, CC1310, WMBUS

As title,

so far only support only have CC1310 and CC1350 support.

I saw forum say 2020 Q4 release for CC1312/CC1352 ,

may i ask how s the update on it?

Thanks

  • The WMBUS patches is available in the simplelink_cc13x2_26x2_sdk_4_40_04_04 SDK under:

    C:\ti\simplelink_cc13x2_26x2_sdk_4_40_04_04\source\ti\devices\cc13x2_cc26x2\rf_patches

    There are also settings available in SmartRF Studio.

    However, there are no wmbus stack available for the CC13x2 devices yet.

    BR

    Siri