I have a proprietry CC1310 design. Using an EByte module with the RSM package. The module has no 32KHz crystal. It all works fine with ccfg set use the HF oscillator as the clock source. I have a new layout with an external crystal. Configuring for the crystal, the RTC frequency, as far as I can determine seems unchanged. Looking at the Q pins with a scope the signal is pretty awful but likely caused by the scope probe. Some questions;
1 - It seems the clock uses the internal source if the external oscllator is not working, regardless of the ccfg setting. Is that correct?
2 - Is there a way to verify which source is actually used for the 32KHz clock?
3 - I have been not very successful with steering the clock to an output to measure, using the TRM notes. Does TI have an example of this?
Thanks for the help.