Other Parts Discussed in Thread: CC1310, CC1312R
Hello,
When I try to set/clear GPIO22 in my main task, it work perfectly, but when I'm trying to set/clear GPIO22 in watchdog timer callback noting happen, the GPIO state is not modified.
Using below GPIO:
#define Board_GPIO_TEST1 GPIOCC26XX_DIO_22
GPIO configuration: GPIO_PinConfig gpioPinConfigs[] = {
/* GPIO_TEST1 */
GPIOCC26XX_DIO_22 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_MED | GPIO_CFG_OUT_LOW,
Set/clear function I use:
PIN_setOutputValue(PIN_Handle handle, PIN_Id pinId, uint32_t val);