Hi,
I'm designing a project with a CC1352P1 based E79-900DM2005S module from ebyte on a custom board.
Testing the RF signal on the Smart RF Studio works great, It enables the High PA 20dbm with no problems but when I'm trying to do it in the Code Composer Studio the debug sends me this error:
Cortex_M4_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or
try
more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.1.0.00001)
Cortex_M4_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or
try
more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.1.0.00001)