Hi ti team,
At present, my client encounters the problem that CC1101 cannot be connected, as follows
1. The performance of the undesirable phenomenon is: the assembled finished product cannot be connected, and the semi-finished product is connected normally. The preliminary judgment is that the signal strength is problematic.
2. Replace the bad PCB with a new CC1101 and reassemble it into a finished product. The CC1101 can be connected normally.
3. The bad IC is restored to the bad PCB, and then assembled into a finished product, the CC1101 cannot be connected