Other Parts Discussed in Thread: HDC2080, TMP117, CC1352R, OPT3001
I am trying to get temperature and humidity data from the HDC2080 sensor of LPSTK. For this, I have first try to run an example project. When I am running this project on LPSTK, it shows only zero all the time as a temperature value. Please suggest I resolve this problem. I want to access the TMP117 sensor from this example project to get temperature value so that I can learn to use HDC2080. In the attached image I am showing the output result of the example project i2ctmp.