This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The debug interface is locked



Hi,

 

I’m having problem with enabling debug interface with “Forced Mass Erase” function that provides SmratRF Flash Programmer 2.

I’m using CC13xxEM-7XD board on a SmratRF06 Evaluation Board (XDS100v3 debug probe).

Status when using Forced Mass Erase:

>Initiate access to target: XDS-06EB122F1227A.

>Failed to read target memory.

>Error while reading memory range. Address 0x40091090.

>Start flash erase ...

>Erase finished successfully.

>Reset target ...

>Reset of target successfull.

Status when uploading a program in to flash:

>Initiate access to target: XDS-06EB122F1227A.

>Failed to read target memory.

>Error while reading memory range. Address 0x40091090.

>Debug interface is locked. Aborting action. Only forced mass erase is possible.

>Reset target ...

>Reset of target successfull.

Is it maybe the flash that is broken?

I also tried the Forced Mass Erase and programming the flash on another same board set and it works. So I assume there is some hardware issues.

 

Daniel