Part Number: CC1352P
Other Parts Discussed in Thread: UNIFLASH
Tool/software: TI-RTOS
Hi,
CC1352P - FH Mode - Collector code.
Is it possible to get the Network information( Like Sensor details, Security information, Number of Connected device etc) from the Non Volatile Memory using already available function.
So, i can store Network information in external Flash and i will do the FOTA using UART.
So, after FOTA at very initial time i can get back the network information from flash and again insert in Non Volatile memory of CC1352.
Is it possible to do like this?
if yes, then how?
if no, then how can i save network info even after flashing also?
Regards,
Anil.