This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: Sub-GHz TX-20dBm output

Part Number: CC1352P
Other Parts Discussed in Thread: , , CC2652P, CC1310

Hi,

As I know, there are three versions of LAUNCHXL-CC1352P as below.

LAUNCHXL-CC1352P1: 868/915 MHz up to 20 dBm, 2.4 GHz up to 5 dBm
LAUNCHXL-CC1352P-2: 868/915 MHz up to 14 dBm, 2.4 GHz up to 20 dBm which can be used to support both CC1352P and CC2652P
LAUNCHXL-CC1352P-4: 433 MHz up to 14 dBm, 2.4 GHz up to 10 dBm

I want to design like as below, is it possible?

433MHz(470-527MHz exactly) up to 20dBm, 2.4GHz up to 5dBm

If yes, can I get the reference design files?

Thanks in advance.

Kevin