Hello expert,
Here I have 2 questions from our customers.
1) When they evaluate the RX packet rate with the following Calibarator tool command.
calibrator wlan0 plt power_mode on
calibrator wlan0 wl18xx_plt tune_channel 5 0 1
calibrator wlan0 wl18xx_plt start_rx 00:00:00:00:00:01 00:00:00:00:00:02
THe command "calibrator wlan0 wl18xx_plt get_rx_stats" result shows some good packets even though the no input.
What is happening here?
2) When they evaluate the TX waveforms on the following channels,
The TX power DIP is observed on the following channels, any other channel is OK.
60ch(5300MHz)、64ch(5320MHz)、120ch(5600MHz)、124ch(5620MHz)

They uses following commands.
calibrator wlan0 plt power_mode on
calibrator wlan0 wl18xx_plt tune_channel 64 1 1
calibrator wlan0 wl18xx_plt set_tx_power 12500 0 1 64 0 0 0 0 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 500 19 1000 0 0 0 0 0 00:11:22:33:44:55 01:02:03:04:05:06 0
Can you please tell what is the root cause of this issue?
Regards,
A.Fujinaka