This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC3235SF: CC3235SF MAC address

Part Number: LAUNCHXL-CC3235SF
Other Parts Discussed in Thread: CC3235SF

Hi, 

 

I know that TI's MAC address start 34-03-DE.

 

Is the remaining MAC address of each CC3235SF chip a unique number?

And can I change the MAC address?

Thanks.

  • Hi Jinhyeong Lee,

    Each SimpleLink Wi-Fi device is loaded with an individual MAC address, but this is not guaranteed to be unique because the MAC address can be changed. The MAC address can be changed in ImageCreator or using sl_NetCfgSet(). See the Device section of the NWP user's guide.

    If you need a unique identifier for your application, you can use the device identity UDID that is stored in hardware. More details in the security app note.

    Best regards,

    Sarah