This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235MODSF: AT Commands Example Project Ready For Production

Part Number: CC3235MODSF


Hi,


We would like to use the AT commands example projet for our production product.

Is it just a sample project or is viable without any changes for production ?

Best regards,

  • Hi,

    If you wanted to use the CC3235MODSF as purely a Wi-Fi network processor, without using any of the GPIOs or other peripherals then yes, you can consider the AT commands example as ready for production.

    I do suggest you perform testing to ensure that your host device's application can work without errors with the AT command implementation on the CC3235, but in terms of functionality I do not see any major issue with taking the AT commands project as-is.

    Regards,

    Michael