This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3120MOD: FCC/IC/CE Certification Requirements

Part Number: CC3120MOD
Other Parts Discussed in Thread: CC3120

Hello, 

I'm using the CC3120MOD (Wi-Fi module) on my device. This is the first time I'm certifying a device for FCC/IC/CE. Please help with understanding the below:-

1) Even though the Module is FCC Certified, there is a need for additional testing for unintentional emissions? Yes/No ? 

2) If additional testing needed, how different is this from regular certification? 

3) Are we allowed to use a different antenna other than the ones mentioned in the list of antennas? 
If we use a differnent antenna, what additional testing is to be done? 

4) If the device is using the CC3120 module and the recommended antenna? is additional certification/testing necessary or can we use the same FC certification of the CC3120 Module? 


Please advice .