Part Number: CC3230S
Other Parts Discussed in Thread: UNIFLASH
Hi,
I am using uniflash version 6.3.0. I tried to create project from uniflash CLI. I can do this successfully in one PC.
I am following command line instruction from swru469h.
In this process When I add service pack with below command, it is successful on one PC. Below is the log.
C:\ti\uniflash_6.3.0>dslite --mode cc32xx project set_sp --name C:\Users\h463279\.SLImageCreator\projects\WSD_CLI --file C:\Users\h463279\.SLImageCreator\projects\CLI_test\sp_4.9.0.2_3.7.0.1_3.1.0.26.bin
Executing the following command:
> C:\ti\uniflash_6.3.0\simplelink\imagecreator\bin\SLImageCreator.exe project set_sp --name C:\Users\h463279\.SLImageCreator\projects\WSD_CLI --file C:\Users\h463279\.SLImageCreator\projects\CLI_test\sp_4.9.0.2_3.7.0.1_3.1.0.26.bin
For more details and examples, please refer to the UniFlash Quick Start guide.
Config file (cfg.json) doesn't exist, using defaults
But, When I am following the similar process on other PC, it is giving me error. Below is the log for the same.
C:\ti\uniflash_6.3.0>dslite --mode cc32xx project set_sp --name C:\Users\h386154\.SLImageCreator\projects\WSD_CLI --file C:\Users\h386154\.SLImageCreator\projects\CLI_test\sp_4.9.0.2_3.7.0.1_3.1.0.26.bin
Executing the following command:
> C:\ti\uniflash_6.3.0\simplelink\imagecreator\bin\SLImageCreator.exe project set_sp --name C:\Users\h386154\.SLImageCreator\projects\WSD_CLI --file C:\Users\h386154\.SLImageCreator\projects\CLI_test\sp_4.9.0.2_3.7.0.1_3.1.0.26.bin
For more details and examples, please refer to the UniFlash Quick Start guide.
Config file (cfg.json) doesn't exist, using defaults
Traceback (most recent call last):
File "<string>", line 5189, in <module>
File "<string>", line 5185, in main
File "<string>", line 5157, in cmdline
File "<string>", line 4154, in command_project_set_sp
File "W:\slimagecreatorglobals.py", line 355, in rmtree_from_projects
slimagecreatorglobals.SLImageCreatorError: Not a directory within the projects directory: C:\Users\h386154\.SLImageCreator\projects\WSD_CLI\sl_sp
SLImageCreator returned -1
Why the same process has different behavior on different PC? What is this error?
Please guide.
Thanks
Rushina