Part Number: CC3100
Other Parts Discussed in Thread: CC3130
Hi
We are using a RX65 connected via UART and SPI to the CC3130.
Since we are using the SPI for communication through TIs SDK (sl_Start ,, etc..) and we can program new ServicePackages by using the Sl_FsProgram,
then the question is, do we need the UART at all ?
Another question is that it seems the stored accesspoint is deleted when programming new servicepack into the CC3130. Could this be avoided.
BR
Jørgen