Part Number: CC3200-LAUNCHXL
Other Parts Discussed in Thread: CC3200
Hello, I am using the i2c_if.c library to receive the DateTime from the DS3231 but I am receiving wrong data.
If I connect the DS3231 to the arduino it works, but when I connect it to the CC3200 (PIN1, PIN2) I do not receive the expected data.
If I use the i2c_demo program with the command:
readreg 0x68 0x00 7
He answers the following: 0x37, 0x20, 0x0, 0x1, 0x1, 0x1, 0x0,
which does not correspond to any date.
I have captured the i2c bus with a analyzer and the following is received:

Are there any missing settings?