This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1801: Can we replace WL1801 with WL1803 without any change of driver/firmware ?

Part Number: WL1801


Hi 

Our product has WL1801 working with Wilink8 software.

Just 2.4GHz WLAN works on it. 5GHz WLAN and Bluetooth is not needed.

WL1801 silicon is not available right now but we have some stock of WL1803 chips.

Then now we are wondering if we can replace WL1801 with WL1803 without any change of driver/firmware.

Does the WL1801's software including WL1801's firmware work on WL1803 without change ?

Or What do we need to do to replace WL1801 with WL1803 (5GHz and Bluetooth are not used) ?

BR, Nobby