Part Number: CC3235MODSF
Other Parts Discussed in Thread: UNIFLASH
Hi experts,
Is it possible for UniFlash to use (for example) pins 10 and 4 of UART0 instead of pins 46 and 47 of UART0 to program the flash of CC3235MODx?
I could not find the reason why the 46 and 47 pins should be used in the documentation. Just in case, I would appreciate it if you could tell me if it is possible to use other pins for UART0 and if not, why.
Basically, we plan to comply with the following document.
- CC3235MOD Production Line Guide:4.3 Configuration of the UART"
- CC3x35 Hardware Design Checklist (Rev. A):"CC3235MODx & CC3235MODAx" tab
Best regards,
O.H