Other Parts Discussed in Thread: CC3200
Hi,
Customer encountered an error when using the device, please see details below.
"When loading the blinky project, error is encountered



Thank you.
Regards,
Maynard
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Customer encountered an error when using the device, please see details below.
"When loading the blinky project, error is encountered



Thank you.
Regards,
Maynard
Hi Maynard,
Have they verified that the board has the correct configuration of the jumpers? When flashing the board make sure to apply a jumper on pin J15 (also labeled as 2) in the SOP group. For reference follow "Figure 1. Jumpers on the CC3200-LAUNCHXL" in document www.ti.com/.../swru376, and for more information on the hardware see www.ti.com/.../swru372. Let me know if this resolves the problem.
Best Regards,
Jessica M. Torres
Hi Jessica,
Thank you for your response. I just received a reply from customer, details below.
Now I want to know the usb port is u1 or u0 ,i mean ,the cc3200 have two com ,one is u0 other is u1 ,i want know which pin is u0 ,can you send me the instructions for the two serial ports.
Regards,
Maynard
Could you clarify on what is the "u0" and "u1" that the customer refers too, could they mean the USB communication data lines D- and D+? Because the CC3200 Launchpad only has one USB port that traces by a "U1" component, which is just an ESD protection diode. If they refer to which pins are D- and D+ those are pins 2 and 3 respectively on the Micro USB port. I recommend they refer to page 3 of the Launchpad Board schematic from the Design Files at https://www.ti.com/tool/CC3200-LAUNCHXL#design-files.

Best Regards,
Jessica M. Torres
Hi Jessica,
This inquiry in our side is already closed. We did not received any response from them.
Considered this as closed as well. Thank you for your support.
Regards,
Maynard