This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3100MOD: Interconnection of TIDA-00637 and TIDC-CC3100MODBOOST

Part Number: CC3100MOD

 Dear ,

Please help us to clarify the following questions, thank you.

  1. Is J10 in CC3100MOD connect to RH2 in TIDA-00637?
  2. If question 1 is YES. Some connection looks like no sense

For example: J10.pin14 (CC_SPI_CLK, connect to CC3100MOD.pin5) need connect to HOST. But RH2 pin 10 is NC.

Regards,

bard