Part Number: CC3130
Other Parts Discussed in Thread: CC3100, CC3135, CC3120
Hi
I've succeded in making the break signaling over uart to our CC3130.
After this I can get version and start programming the external flash.
But according to other specs, a doc swra658.pdf chapter 16, it should be possible to format the external flash, however when trying this I always get a NACK back from the TI.
Do you have any idea why ?
We are using a WINBOND: W25Q16JVUXIQ (16 Mbyte flash). sending cmd:
0x00,0x17,0x3C,0x28,0x00,0x00,0x00,0x02,0x00,0x00,0x10,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x02
I've also tried other format commands, but get NACK everytime.
BR
Jørgen Busch