Part Number: CC3135
Hi,
I couldn't find any resolution in the previous post.
He're my problem :
i'm using the out_of_the_box example and try to handle from the HTML page some queries.
So far managed to use GET/PUT and post working but i'm having trouble with post query with the the data in the body instead of the url.
this query is directly made with standard html form.
Theses query end up in the SimpleLinkHttpServerEventHandler method instead of SimpleLinkNetAppRequestEventHandler, which is quite empty in the example
void SimpleLinkHttpServerEventHandler(
SlNetAppHttpServerEvent_t *pHttpEvent,
SlNetAppHttpServerResponse_t *pHttpResponse)
{
/* Unused in this application */
UART_PRINT("[HTTP SERVER EVENT] Unexpected HTTP server event \n\r");
}
Any idead of how to transfer back to SimpleLinkNetAppRequestEventHandler this form post query ?
Regards,
Théodore