Part Number: LAUNCHCC3235MOD

Hello,
In CC3235MOD datasheet, it is mentioned TCP throughput is 13Mbps.
Which example or test code can be used to test the throughput on the LAUNCHCC3235MOD board?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LAUNCHCC3235MOD

Hello,
In CC3235MOD datasheet, it is mentioned TCP throughput is 13Mbps.
Which example or test code can be used to test the throughput on the LAUNCHCC3235MOD board?
We don't have ab example fdedicated for the throughput testing.
The NetworkTerminal contains TCPServer and TCPClient options that can be used as the base for such measurement (i.e. measuring throughput between 2 devices). It currently just counts bytes, so the time needs to be added to the calculation.
Br,
Kobi