Other Parts Discussed in Thread: CC3120, CC3130
1. If a customer utilizes the CC3120 today, can it be interchangeably replaced on the same PCB with the CC3220S?
a. Can the CPU and all peripherals of the CC3220 be turned off, so both options run at the same power consumption?
b. What is the implication for creating a SPI interface in the CC3220 to mimic the behavior of the CC3120?
2, When switching between the CC3120 and CC3130, can the same board layout be used, considering the 2.4GHz arbitration is not to be used?
3. Do we have examples of FCC approvals when switching between gen 2 and gen 3 (CC3120 → CC3130)? Is this considered a permissive change Class I?
Thank you!