Part Number: CC3235S
Hi,
I want to get complete list of networks as soon as possible after starting network scan.
How long should I wait after I enable SCAN POLICY?
BR,
Masashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC3235S
Hi,
I want to get complete list of networks as soon as possible after starting network scan.
How long should I wait after I enable SCAN POLICY?
BR,
Masashi
Hi Masashi,
If there are no scan results available yet (or if they are old), calling sl_WlanGetNetworkList() will immediately trigger a one-shot scan and return. You shouldn't have to set a delay in the application.
Best regards,
Sarah
Hi Sarah,
Thank you.
sl_WlanGetNetworkList() sometimes return empty list or few APs even though there are many APs around.
In particular, it seems that 5GHz APs are often missed.
Setting the channel mask did not change the situation.
Is there a solution to this?
Best Regards,
Masashi
Hi Masashi,
(Edited) Please try using sl_WlanGetExtNetworkList(). This should scan the 5GHz channels by default.
Is the latest servicepack version flashed to the file system? Is 5Ghz enabled? (This can be done in the application or in the radio settings in ImageCreator.)
What channel is the desired network on? What country code is being used?
Keep in mind the network list will only returns APs with a RSSI above the threshold (default -95 dBm), and the network list is filled at 30 entries.
Best regards,
Sarah