This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1837MOD: Test Report - EN 300328, EN 301893, EN 62311

Part Number: WL1837MOD

Dear expert(s),

I would like to obtain information about the maximum transmit power for WL1837MOD.

The information is likely contain within the test report of this component, mainly:

- EN 300 328 V2.1.1

- EN 301 893 V2.1.1

- EN 62311:2008

I could not locate the correct FCC ID report for this component.

This is required by our test house to conduct a local assessment for the WIFI of an equipment which incorporate this component.

best regards,

Joon Kwan