This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1831: Unable to connect to wifi network

Part Number: WL1831


Hi,

We have an issue where one of our devices in the field is unable to connect to a wifi network on our device running a WL1831 chip. All we've been able to work out is that the authentication is timing out. The wifi network is a very standard home wifi network running on a TP-Link Deco M5 (EU variant) and we have deployed our solution on thousands of locations with no similar issue. Do you have any idea what could cause this?

Software running

  • Linux kernel 4.9.281 (mainline)
  • wpa_supplicant 2.9
  • Connman 1.38
  • WL18xx Firmware 8.9.0.0.88

iw dev wlan0 scan results

root@noah-hmi:~# iw dev wlan0 scan
BSS 42:84:6a:14:9a:7a(on wlan0)
        last seen: 3830.065s [boottime]
        TSF: 2845491589 usec (0d, 00:47:25)
        freq: 2442
        beacon interval: 100 TUs
        capability: ESS Privacy ShortPreamble ShortSlotTime RadioMeasure (0x1431)
        signal: -60.00 dBm
        last seen: 23260 ms ago
        Information elements from Probe Response frame:
        SSID: stefans_Guest
        Supported rates: 1.0* 2.0* 5.5* 11.0* 6.0 9.0 12.0 18.0
        DS Parameter set: channel 7
        TIM: DTIM Count 0 DTIM Period 1 Bitmap Control 0x0 Bitmap[0] 0x0
        Country: DE     Environment: Indoor/Outdoor
                Channels [1 - 13] @ 20 dBm
        ERP: <no flags>
        Extended supported rates: 24.0 36.0 48.0 54.0
        HT capabilities:
                Capabilities: 0x19ef
                        RX LDPC
                        HT20/HT40
                        SM Power Save disabled
                        RX HT20 SGI
                        RX HT40 SGI
                        TX STBC
                        RX STBC 1-stream
                        Max AMSDU length: 7935 bytes
                        DSSS/CCK HT40
                Maximum RX AMPDU length 65535 bytes (exponent: 0x003)
                Minimum RX AMPDU time spacing: No restriction (0x00)
                HT TX/RX MCS rate indexes supported: 0-15
        HT operation:
                 * primary channel: 7
                 * secondary channel offset: above
                 * STA channel width: any
                 * RIFS: 0
                 * HT protection: no
                 * non-GF present: 0
                 * OBSS non-GF present: 0
                 * dual beacon: 0
                 * dual CTS protection: 0
                 * STBC beacon: 0
                 * L-SIG TXOP Prot: 0
                 * PCO active: 0
                 * PCO phase: 0
        Extended capabilities:
                 * TFS
                 * WNM-Sleep Mode
                 * TIM Broadcast
                 * BSS Transition
                 * SSID List
                 * Operating Mode Notification
                 * Max Number Of MSDUs In A-MSDU is unlimited
        VHT capabilities:
                VHT Capabilities (0x338959b2):
                        Max MPDU length: 11454
                        Supported Channel Width: neither 160 nor 80+80
                        RX LDPC
                        short GI (80 MHz)
                        TX STBC
                        SU Beamformer
                        SU Beamformee
                        MU Beamformer
                        RX antenna pattern consistency
                        TX antenna pattern consistency
                VHT RX MCS set:
                        1 streams: MCS 0-9
                        2 streams: MCS 0-9
                        3 streams: not supported
                        4 streams: not supported
                        5 streams: not supported
                        6 streams: not supported
                        7 streams: not supported
                        8 streams: not supported
                VHT RX highest supported: 0 Mbps
                VHT TX MCS set:
                        1 streams: MCS 0-9
                        2 streams: MCS 0-9
                        3 streams: not supported
                        4 streams: not supported
                        5 streams: not supported
                        6 streams: not supported
                        7 streams: not supported
                        8 streams: not supported
                VHT TX highest supported: 0 Mbps
        VHT operation:
                 * channel width: 0 (20 or 40 MHz)
                 * center freq segment 1: 0
                 * center freq segment 2: 0
                 * VHT basic MCS set: 0xfffc
        WMM:     * Parameter version 1
                 * u-APSD
                 * BE: CW 15-1023, AIFSN 3
                 * BK: CW 15-1023, AIFSN 7
                 * VI: CW 7-15, AIFSN 2, TXOP 3008 usec
                 * VO: CW 3-7, AIFSN 2, TXOP 1504 usec
        RSN:     * Version: 1
                 * Group cipher: CCMP
                 * Pairwise ciphers: CCMP
                 * Authentication suites: PSK
                 * Capabilities: 1-PTKSA-RC 1-GTKSA-RC (0x0000)

kernel log with full debug output

kernel.txt

wpa_supplicant log

root@noah-hmi:/var/noah/var/lib/connman# wpa_supplicant -u -dd -t
1636453818.617208: wpa_supplicant v2.9
1636453818.620286: random: Trying to read entropy from /dev/random
1636453818.634447: dbus: Register D-Bus object '/fi/w1/wpa_supplicant1'
1636453818.649284: Providing DBus service 'fi.w1.wpa_supplicant1'.
1636453818.652876: Successfully initialized wpa_supplicant
1636453818.660902: random: Got 20/20 bytes from /dev/random
1636453818.666825: dbus: org.freedesktop.DBus.Properties.GetAll (/fi/w1/wpa_supplicant1) [s]
1636453818.679094: dbus: fi.w1.wpa_supplicant1.GetInterface (/fi/w1/wpa_supplicant1) [s]
1636453818.686843: dbus: fi.w1.wpa_supplicant1.CreateInterface (/fi/w1/wpa_supplicant1) [a{sv}]
1636453818.688550: wpa_dbus_dict_open_read: start reading a dict entry
1636453818.689775: wpa_dbus_dict_get_entry: dict entry key: Ifname
1636453818.690256: wpa_dbus_dict_get_entry: dict entry variant content type: s
1636453818.690724: _wpa_dbus_dict_fill_value_from_variant: string value: [omitted]
1636453818.691199: wpa_dbus_dict_get_entry: dict entry key: Driver
1636453818.691561: wpa_dbus_dict_get_entry: dict entry variant content type: s
1636453818.691919: _wpa_dbus_dict_fill_value_from_variant: string value: [omitted]
1636453818.692647: Initializing interface 'wlan0' conf 'N/A' driver 'nl80211,wext' ctrl_interface 'N/A' bridge 'N/A'
1636453818.701460: nl80211: Supported cipher 00-0f-ac:1
1636453818.703386: nl80211: Supported cipher 00-0f-ac:5
1636453818.704396: nl80211: Supported cipher 00-0f-ac:2
1636453818.705318: nl80211: Supported cipher 00-0f-ac:4
1636453818.706900: nl80211: Supported cipher 00-14-72:1
1636453818.707761: nl80211: Supports Probe Response offload in AP mode
1636453818.708852: nl80211: Using driver-based off-channel TX
1636453818.709801: nl80211: Driver-advertised extended capabilities (default) - hexdump(len=8): 04 00 00 00 00 00 00 40
1636453818.709941: nl80211: Driver-advertised extended capabilities mask (default) - hexdump(len=8): 04 00 00 00 00 00 00 40
1636453818.710440: nl80211: Supported vendor command: vendor_id=0x80028 subcmd=0
1636453818.710528: nl80211: Supported vendor command: vendor_id=0x80028 subcmd=1
1636453818.710594: nl80211: Supported vendor command: vendor_id=0x80028 subcmd=2
1636453818.710654: nl80211: Supported vendor event: vendor_id=0x80028 subcmd=0
1636453818.711543: nl80211: Supported vendor event: vendor_id=0x80028 subcmd=1
1636453818.713106: nl80211: Use separate P2P group interface (driver advertised support)
1636453818.713672: nl80211: Enable multi-channel concurrent (driver advertised support)
1636453818.713757: nl80211: use P2P_DEVICE support
1636453818.713824: nl80211: interface wlan0 in phy phy0
1636453818.714530: nl80211: Set mode ifindex 3 iftype 2 (STATION)
1636453818.716889: nl80211: Subscribe to mgmt frames with non-AP handle 0x13e448
1636453818.717846: nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x13e448 match=06
1636453818.718449: nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x13e448 match=0a07
1636453818.719744: nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x13e448 match=0a11
1636453818.720539: nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x13e448 match=1101
1636453818.721474: nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x13e448 match=1102
1636453818.722510: nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x13e448 match=0505
1636453818.724394: nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x13e448 match=0500
1636453818.728712: rfkill: initial event: idx=0 type=1 op=0 soft=0 hard=0
1636453818.730363: netlink: Operstate: ifindex=3 linkmode=1 (userspace-control), operstate=5 (IF_OPER_DORMANT)
1636453818.743229: Add interface wlan0 to a new radio phy0
1636453818.753492: nl80211: Regulatory information - country=SE (DFS-ETSI)
1636453818.753609: nl80211: 2400-2483 @ 40 MHz 20 mBm
1636453818.753652: nl80211: 5150-5250 @ 80 MHz 23 mBm (no outdoor)
1636453818.753684: nl80211: 5250-5350 @ 80 MHz 20 mBm (no outdoor) (DFS)
1636453818.753714: nl80211: 5470-5725 @ 160 MHz 27 mBm (DFS)
1636453818.753743: nl80211: 5725-5875 @ 80 MHz 14 mBm
1636453818.753805: nl80211: 57000-66000 @ 2160 MHz 40 mBm
1636453818.753945: nl80211: Added 802.11b mode based on 802.11g information
1636453818.754019: nl80211: Mode IEEE 802.11g: 2412 2417 2422 2427 2432 2437 2442 2447 2452 2457 2462 2467 2472 2484[DISABLED][NO_IR]
1636453818.754046: nl80211: Mode IEEE ?:
1636453818.754102: nl80211: Mode IEEE 802.11b: 2412 2417 2422 2427 2432 2437 2442 2447 2452 2457 2462 2467 2472 2484[DISABLED][NO_IR]
1636453818.778659: wlan0: Own MAC address: 34:15:13:6b:3c:84
1636453818.778905: wpa_driver_nl80211_set_key: ifindex=3 (wlan0) alg=0 addr=(nil) key_idx=0 set_tx=0 seq_len=0 key_len=0
1636453818.779289: wpa_driver_nl80211_set_key: ifindex=3 (wlan0) alg=0 addr=(nil) key_idx=1 set_tx=0 seq_len=0 key_len=0
1636453818.779510: wpa_driver_nl80211_set_key: ifindex=3 (wlan0) alg=0 addr=(nil) key_idx=2 set_tx=0 seq_len=0 key_len=0
1636453818.779696: wpa_driver_nl80211_set_key: ifindex=3 (wlan0) alg=0 addr=(nil) key_idx=3 set_tx=0 seq_len=0 key_len=0
1636453818.779841: wlan0: RSN: flushing PMKID list in the driver
1636453818.779871: nl80211: Flush PMKIDs
1636453818.779994: wlan0: State: DISCONNECTED -> INACTIVE
1636453818.791925: wlan0: WPS: UUID based on MAC address: 1c437b75-09d1-5a16-b0cd-b61330751f4b
1636453818.796976: GnuTLS: Library version 3.6.14 (runtime) - 3.6.14 (build)
1636453818.807778: EAPOL: SUPP_PAE entering state DISCONNECTED
1636453818.812023: EAPOL: Supplicant port status: Unauthorized
1636453818.813274: nl80211: Skip set_supp_port(unauthorized) while not associated
1636453818.813744: EAPOL: KEY_RX entering state NO_KEY_RECEIVE
1636453818.813824: EAPOL: SUPP_BE entering state INITIALIZE
1636453818.813897: EAP: EAP entering state DISABLED
1636453818.814204: dbus: Register interface object '/fi/w1/wpa_supplicant1/Interfaces/0'
1636453818.837015: wlan0: Added interface wlan0
1636453818.838752: wlan0: State: INACTIVE -> DISCONNECTED
1636453818.839530: nl80211: Set wlan0 operstate 0->0 (DORMANT)
1636453818.840166: netlink: Operstate: ifindex=3 linkmode=-1 (no change), operstate=5 (IF_OPER_DORMANT)
1636453818.847788: dbus: org.freedesktop.DBus.Properties.GetAll (/fi/w1/wpa_supplicant1/Interfaces/0) [s]
1636453818.852397: dbus: org.freedesktop.DBus.Properties.GetAll (/fi/w1/wpa_supplicant1/Interfaces/0) [s]
1636453818.869709: RTM_NEWLINK: ifi_index=3 ifname=wlan0 operstate=2 linkmode=1 ifi_family=0 ifi_flags=0x9003 ([UP])
1636453818.875169: dbus: org.freedesktop.DBus.Properties.Set (/fi/w1/wpa_supplicant1/Interfaces/0) [ssv]
1636453818.877933: properties_get_or_set: Set(ConfigMethods)
1636453818.880426: WPS: Converting push_button to virtual_push_button for WPS 2.0 compliance
1636453818.911665: dbus: fi.w1.wpa_supplicant1.Interface.Scan (/fi/w1/wpa_supplicant1/Interfaces/0) [a{sv}]
1636453818.920385: wlan0: Setting scan request: 0.000000 sec
1636453818.925711: wlan0: State: DISCONNECTED -> SCANNING
1636453818.927238: wlan0: Starting AP scan for wildcard SSID
1636453818.929620: wlan0: Add radio work 'scan'@0x141b68
1636453818.930619: wlan0: First radio work item in the queue - schedule start immediately
1636453818.931052: wlan0: Starting radio work 'scan'@0x141b68 after 0.000432 second wait
1636453818.931956: wlan0: nl80211: scan request
1636453818.932712: nl80211: Scan SSID
1636453818.933443: nl80211: Scan extra IEs - hexdump(len=10): 7f 08 04 00 00 00 00 00 00 40
1636453818.942826: Scan requested (ret=0) - scan timeout 10 seconds
1636453818.944554: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453818.945833: nl80211: Event message available
1636453818.947029: nl80211: Drv Event 33 (NL80211_CMD_TRIGGER_SCAN) received for wlan0
1636453818.947411: wlan0: nl80211: Scan trigger
1636453818.947983: wlan0: Event SCAN_STARTED (47) received
1636453818.948429: wlan0: Own scan request started a scan in 0.003905 seconds
1636453818.959370: dbus: org.freedesktop.DBus.Properties.Set (/fi/w1/wpa_supplicant1/Interfaces/0) [ssv]
1636453818.960615: no property handler for fi.w1.wpa_supplicant1.Interface.P2PDevice.P2PDeviceConfig on /fi/w1/wpa_supplicant1/Interfaces/0
1636453818.963294: dbus: org.freedesktop.DBus.Properties.GetAll (/fi/w1/wpa_supplicant1/Interfaces/0) [s]
1636453819.392681: nl80211: Event message available
1636453819.392933: nl80211: Drv Event 34 (NL80211_CMD_NEW_SCAN_RESULTS) received for wlan0
1636453819.392999: wlan0: nl80211: New scan results available
1636453819.393036: nl80211: Scan probed for SSID ''
1636453819.393084: nl80211: Scan included frequencies: 2412 2417 2422 2427 2432 2437 2442 2447 2452 2457 2462 2467 2472
1636453819.393122: wlan0: Event SCAN_RESULTS (3) received
1636453819.393163: wlan0: Scan completed in 0.444754 seconds
1636453819.393900: nl80211: Received scan results (5 BSSes)
1636453819.394231: wlan0: BSS: Start scan result update 1
1636453819.394314: wlan0: BSS: Add new id 0 BSSID 42:84:6a:14:9a:7a SSID 'stefans_Guest' freq 2442
1636453819.394358: dbus: Register BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/0'
1636453819.402762: wlan0: BSS: Add new id 1 BSSID 3c:84:6a:14:9a:7a SSID 'stefans' freq 2442
1636453819.404278: dbus: Register BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/1'
1636453819.411806: wlan0: BSS: Add new id 2 BSSID 46:84:6a:14:9a:7a SSID '' freq 2442
1636453819.413536: dbus: Register BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/2'
1636453819.420842: wlan0: BSS: Add new id 3 BSSID 3c:84:6a:14:9a:2a SSID 'stefans' freq 2442
1636453819.423067: dbus: Register BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/3'
1636453819.429889: wlan0: BSS: Add new id 4 BSSID d8:d8:66:25:9a:52 SSID 'NIBE STRONG_2.4GHz' freq 2417
1636453819.431433: dbus: Register BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/4'
1636453819.444845: BSS: last_scan_res_used=5/32
1636453819.450701: wlan0: New scan results available (own=1 ext=0)
1636453819.459333: WPS: AP 3c:84:6a:14:9a:7a type 0 added
1636453819.460645: WPS: AP 3c:84:6a:14:9a:2a type 0 added
1636453819.462212: WPS: AP[0] 3c:84:6a:14:9a:7a type=0 tries=0 last_attempt=-1 sec ago blacklist=0
1636453819.462941: WPS: AP[1] 3c:84:6a:14:9a:2a type=0 tries=0 last_attempt=-1 sec ago blacklist=0
1636453819.463244: wlan0: Radio work 'scan'@0x141b68 done in 0.532191 seconds
1636453819.463448: wlan0: radio_work_free('scan'@0x141b68): num_active_works --> 0
1636453819.463536: wlan0: No suitable network found
1636453819.463619: wlan0: Use normal scan instead of sched_scan for initial scans (normal_scans=1)
1636453819.463696: wlan0: Short-circuit new scan request since there are no enabled networks
1636453819.463772: wlan0: State: SCANNING -> INACTIVE
1636453819.467380: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453819.481505: dbus: org.freedesktop.DBus.Properties.Get (/fi/w1/wpa_supplicant1/Interfaces/0) [ss]
1636453819.483834: properties_get_or_set: Get(BSSs)
1636453819.814327: EAPOL: disable timer tick
1636453821.801947: dbus: fi.w1.wpa_supplicant1.Interface.Scan (/fi/w1/wpa_supplicant1/Interfaces/0) [a{sv}]
1636453821.802148: wlan0: Setting scan request: 0.000000 sec
1636453821.802696: wlan0: State: INACTIVE -> SCANNING
1636453821.802782: wlan0: Starting AP scan for wildcard SSID
1636453821.802855: wlan0: Add radio work 'scan'@0x142a28
1636453821.802936: wlan0: First radio work item in the queue - schedule start immediately
1636453821.803015: wlan0: Starting radio work 'scan'@0x142a28 after 0.000076 second wait
1636453821.803067: wlan0: nl80211: scan request
1636453821.803135: nl80211: Scan SSID
1636453821.803165: nl80211: Scan extra IEs - hexdump(len=10): 7f 08 04 00 00 00 00 00 00 40
1636453821.820623: Scan requested (ret=0) - scan timeout 30 seconds
1636453821.824083: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453821.825962: nl80211: Event message available
1636453821.831185: nl80211: Drv Event 33 (NL80211_CMD_TRIGGER_SCAN) received for wlan0
1636453821.833828: wlan0: nl80211: Scan trigger
1636453821.834302: wlan0: Event SCAN_STARTED (47) received
1636453821.840380: wlan0: Own scan request started a scan in 0.015229 seconds
1636453822.200629: nl80211: Event message available
1636453822.200876: nl80211: Drv Event 34 (NL80211_CMD_NEW_SCAN_RESULTS) received for wlan0
1636453822.200939: wlan0: nl80211: New scan results available
1636453822.200976: nl80211: Scan probed for SSID ''
1636453822.201023: nl80211: Scan included frequencies: 2412 2417 2422 2427 2432 2437 2442 2447 2452 2457 2462 2467 2472
1636453822.201063: wlan0: Event SCAN_RESULTS (3) received
1636453822.201104: wlan0: Scan completed in 0.362020 seconds
1636453822.201822: nl80211: Received scan results (5 BSSes)
1636453822.205204: wlan0: BSS: Start scan result update 2
1636453822.206193: wlan0: BSS: Add new id 5 BSSID 46:84:6a:14:9a:2a SSID '' freq 2442
1636453822.206744: dbus: Register BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/5'
1636453822.215255: BSS: last_scan_res_used=5/32
1636453822.216610: wlan0: New scan results available (own=1 ext=0)
1636453822.222666: WPS: AP[0] 3c:84:6a:14:9a:7a type=0 tries=0 last_attempt=-1 sec ago blacklist=0
1636453822.223492: WPS: AP[1] 3c:84:6a:14:9a:2a type=0 tries=0 last_attempt=-1 sec ago blacklist=0
1636453822.223663: wlan0: Radio work 'scan'@0x142a28 done in 0.420629 seconds
1636453822.223752: wlan0: radio_work_free('scan'@0x142a28): num_active_works --> 0
1636453822.224594: wlan0: No suitable network found
1636453822.225366: wlan0: Use normal scan instead of sched_scan for initial scans (normal_scans=2)
1636453822.227826: wlan0: Short-circuit new scan request since there are no enabled networks
1636453822.227944: wlan0: State: SCANNING -> INACTIVE
1636453822.229156: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453822.246500: dbus: org.freedesktop.DBus.Properties.Get (/fi/w1/wpa_supplicant1/Interfaces/0) [ss]
1636453822.247502: properties_get_or_set: Get(BSSs)
1636453829.167787: dbus: fi.w1.wpa_supplicant1.Interface.AddNetwork (/fi/w1/wpa_supplicant1/Interfaces/0) [a{sv}]
1636453829.168026: dbus: Register network object '/fi/w1/wpa_supplicant1/Interfaces/0/Networks/0'
1636453829.171959: wpa_dbus_dict_open_read: start reading a dict entry
1636453829.176299: wpa_dbus_dict_get_entry: dict entry key: scan_ssid
1636453829.177438: wpa_dbus_dict_get_entry: dict entry variant content type: u
1636453829.179241: _wpa_dbus_dict_fill_value_from_variant: uint32 value: 1
1636453829.179631: scan_ssid=1 (0x1)
1636453829.181208: wpa_dbus_dict_get_entry: dict entry key: bgscan
1636453829.181767: wpa_dbus_dict_get_entry: dict entry variant content type: s
1636453829.186116: _wpa_dbus_dict_fill_value_from_variant: string value: [omitted]
1636453829.188064: bgscan - hexdump_ascii(len=17):
     73 69 6d 70 6c 65 3a 33 30 3a 2d 36 35 3a 33 30   simple:30:-65:30
     30                                                0
1636453829.195530: wpa_dbus_dict_get_entry: dict entry key: mode
1636453829.196395: wpa_dbus_dict_get_entry: dict entry variant content type: u
1636453829.196491: _wpa_dbus_dict_fill_value_from_variant: uint32 value: 0
1636453829.196629: wpa_dbus_dict_get_entry: dict entry key: psk
1636453829.197132: wpa_dbus_dict_get_entry: dict entry variant content type: s
1636453829.197220: _wpa_dbus_dict_fill_value_from_variant: string value: [omitted]
1636453829.197320: PSK (ASCII passphrase) - hexdump_ascii(len=8): [REMOVED]
1636453829.202264: wpa_dbus_dict_get_entry: dict entry key: key_mgmt
1636453829.202434: wpa_dbus_dict_get_entry: dict entry variant content type: s
1636453829.202511: _wpa_dbus_dict_fill_value_from_variant: string value: [omitted]
1636453829.202602: key_mgmt: 0x2
1636453829.202673: wpa_dbus_dict_get_entry: dict entry key: ssid
1636453829.202743: wpa_dbus_dict_get_entry: dict entry variant content type: a
1636453829.203658: _wpa_dbus_dict_entry_get_array: array_type y
1636453829.206694: dbus: byte array contents - hexdump(len=13): [REMOVED]
1636453829.210043: ssid - hexdump_ascii(len=13):
     73 74 65 66 61 6e 73 5f 47 75 65 73 74            stefans_Guest
1636453830.084052: PSK (from passphrase) - hexdump(len=32): [REMOVED]
1636453830.091224: dbus: fi.w1.wpa_supplicant1.Interface.SelectNetwork (/fi/w1/wpa_supplicant1/Interfaces/0) [o]
1636453830.092613: Fast associate: Old scan results
1636453830.098763: wlan0: Setting scan request: 0.000000 sec
1636453830.108919: wlan0: State: INACTIVE -> SCANNING
1636453830.110384: Scan SSID - hexdump_ascii(len=13):
     73 74 65 66 61 6e 73 5f 47 75 65 73 74            stefans_Guest
1636453830.115800: wlan0: Starting AP scan for wildcard SSID (Interleave with specific)
1636453830.117152: wlan0: Add radio work 'scan'@0x146b80
1636453830.117945: wlan0: First radio work item in the queue - schedule start immediately
1636453830.118117: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453830.124953: wlan0: Starting radio work 'scan'@0x146b80 after 0.006990 second wait
1636453830.126308: wlan0: nl80211: scan request
1636453830.126864: nl80211: Scan SSID
1636453830.127456: nl80211: Scan extra IEs - hexdump(len=10): 7f 08 04 00 00 00 00 00 00 40
1636453830.133447: Scan requested (ret=0) - scan timeout 30 seconds
1636453830.136407: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453830.141755: nl80211: Event message available
1636453830.142982: nl80211: Drv Event 33 (NL80211_CMD_TRIGGER_SCAN) received for wlan0
1636453830.143908: wlan0: nl80211: Scan trigger
1636453830.149358: wlan0: Event SCAN_STARTED (47) received
1636453830.149678: wlan0: Own scan request started a scan in 0.013303 seconds
1636453830.514095: nl80211: Event message available
1636453830.514368: nl80211: Drv Event 34 (NL80211_CMD_NEW_SCAN_RESULTS) received for wlan0
1636453830.514439: wlan0: nl80211: New scan results available
1636453830.514493: nl80211: Scan probed for SSID ''
1636453830.514542: nl80211: Scan included frequencies: 2412 2417 2422 2427 2432 2437 2442 2447 2452 2457 2462 2467 2472
1636453830.514581: wlan0: Event SCAN_RESULTS (3) received
1636453830.514621: wlan0: Scan completed in 0.364958 seconds
1636453830.518524: nl80211: Received scan results (6 BSSes)
1636453830.521545: wlan0: BSS: Start scan result update 3
1636453830.523200: BSS: last_scan_res_used=6/32
1636453830.524711: wlan0: New scan results available (own=1 ext=0)
1636453830.533650: WPS: AP[0] 3c:84:6a:14:9a:7a type=0 tries=0 last_attempt=-1 sec ago blacklist=0
1636453830.536651: WPS: AP[1] 3c:84:6a:14:9a:2a type=0 tries=0 last_attempt=-1 sec ago blacklist=0
1636453830.536839: wlan0: Radio work 'scan'@0x146b80 done in 0.411902 seconds
1636453830.537546: wlan0: radio_work_free('scan'@0x146b80): num_active_works --> 0
1636453830.538840: wlan0: Scan results matching the currently selected network
1636453830.539727: wlan0: 0: 42:84:6a:14:9a:7a freq=2442 level=-58 snr=31 est_throughput=135000
1636453830.539967: wlan0: Selecting BSS from priority group 0
1636453830.541277: wlan0: 0: 42:84:6a:14:9a:7a ssid='stefans_Guest' wpa_ie_len=0 rsn_ie_len=20 caps=0x1431 level=-58 freq=2442
1636453830.541414: wlan0:    selected based on RSN IE
1636453830.542229: wlan0:    selected BSS 42:84:6a:14:9a:7a ssid='stefans_Guest'
1636453830.543434: wlan0: Considering connect request: reassociate: 1  selected: 42:84:6a:14:9a:7a  bssid: 00:00:00:00:00:00  pending: 00:00:00:00:00:00  wpa_state: SCANNING  ssid=0x1467a0  current_ssid=0x1467a0
1636453830.543562: wlan0: Request association with 42:84:6a:14:9a:7a
1636453830.543647: wlan0: No ongoing scan/p2p-scan found to abort
1636453830.543732: wlan0: Add radio work 'sme-connect'@0x151170
1636453830.545736: wlan0: First radio work item in the queue - schedule start immediately
1636453830.545881: RSN: Ignored PMKID candidate without preauth flag
1636453830.546063: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453830.553748: dbus: org.freedesktop.DBus.Properties.Get (/fi/w1/wpa_supplicant1/Interfaces/0) [ss]
1636453830.558440: properties_get_or_set: Get(BSSs)
1636453830.616004: wlan0: Starting radio work 'sme-connect'@0x151170 after 0.070262 second wait
1636453830.625539: wlan0: WPA: clearing own WPA/RSN IE
1636453830.626584: wlan0: Automatic auth_alg selection: 0x1
1636453830.627507: RSN: PMKSA cache search - network_ctx=0x1467a0 try_opportunistic=0 akmp=0x0
1636453830.628949: RSN: Search for BSSID 42:84:6a:14:9a:7a
1636453830.632557: RSN: No PMKSA cache entry found
1636453830.633011: wlan0: RSN: using IEEE 802.11i/D9.0
1636453830.633445: wlan0: WPA: Selected cipher suites: group 16 pairwise 16 key_mgmt 2 proto 2
1636453830.634089: wlan0: WPA: clearing AP WPA IE
1636453830.638781: WPA: set AP RSN IE - hexdump(len=22): 30 14 01 00 00 0f ac 04 01 00 00 0f ac 04 01 00 00 0f ac 02 00 00
1636453830.642173: wlan0: WPA: AP group 0x10 network profile group 0x18; available group 0x10
1636453830.642286: wlan0: WPA: using GTK CCMP
1636453830.642369: wlan0: WPA: AP pairwise 0x10 network profile pairwise 0x18; available pairwise 0x10
1636453830.642663: wlan0: WPA: using PTK CCMP
1636453830.642752: wlan0: WPA: AP key_mgmt 0x2 network profile key_mgmt 0x2; available key_mgmt 0x2
1636453830.642826: wlan0: WPA: using KEY_MGMT WPA-PSK
1636453830.643216: WPA: Set own WPA IE default - hexdump(len=22): 30 14 01 00 00 0f ac 04 01 00 00 0f ac 04 01 00 00 0f ac 02 00 00
1636453830.643359: PSK (set in config) - hexdump(len=32): [REMOVED]
1636453830.644369: WPA: Set PMK based on external data - hexdump(len=32): [REMOVED]
1636453830.645768: RRM: Determining whether RRM can be used - device support: 0x10
1636453830.645863: RRM: Adding RRM IE to Association Request
1636453830.645961: Added supported operating classes IE - hexdump(len=6): 3b 04 51 51 53 54
1636453830.646608: EAPOL: External notification - EAP success=0
1636453830.646731: EAPOL: External notification - EAP fail=0
1636453830.646802: EAPOL: External notification - portControl=Auto
1636453830.646894: wlan0: Cancelling scan request
1636453830.647746: wlan0: SME: Trying to authenticate with 42:84:6a:14:9a:7a (SSID='stefans_Guest' freq=2442 MHz)
1636453830.648811: EAPOL: External notification - portValid=0
1636453830.650617: wlan0: State: SCANNING -> AUTHENTICATING
1636453830.651855: nl80211: Authenticate (ifindex=3)
1636453830.652272:   * bssid=42:84:6a:14:9a:7a
1636453830.653327:   * freq=2442
1636453830.653414:   * SSID=stefans_Guest
1636453830.655650:   * IEs - hexdump(len=0): [NULL]
1636453830.655767:   * Auth Type 0
1636453830.784091: nl80211: Authentication request send successfully
1636453830.785430: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453830.802981: nl80211: Event message available
1636453830.804440: nl80211: Drv Event 19 (NL80211_CMD_NEW_STATION) received for wlan0
1636453830.805741: nl80211: New station 42:84:6a:14:9a:7a
1636453832.879471: nl80211: Event message available
1636453832.879741: nl80211: Drv Event 20 (NL80211_CMD_DEL_STATION) received for wlan0
1636453832.879787: nl80211: Delete station 42:84:6a:14:9a:7a
1636453833.938555: nl80211: Event message available
1636453833.938788: nl80211: Drv Event 37 (NL80211_CMD_AUTHENTICATE) received for wlan0
1636453833.938834: nl80211: MLME event 37; timeout with 42:84:6a:14:9a:7a
1636453833.938892: wlan0: Event AUTH_TIMED_OUT (13) received
1636453833.938927: wlan0: SME: Authentication timed out
1636453833.938975: wlan0: Radio work 'sme-connect'@0x151170 done in 3.322994 seconds
1636453833.939014: wlan0: radio_work_free('sme-connect'@0x151170): num_active_works --> 0
1636453833.939045: Added BSSID 42:84:6a:14:9a:7a into blacklist
1636453833.939093: wlan0: Blacklist count 1 --> request scan in 100 ms
1636453833.939128: wlan0: Setting scan request: 0.100000 sec
1636453833.939169: wlan0: State: AUTHENTICATING -> DISCONNECTED
1636453833.939195: nl80211: Set wlan0 operstate 0->0 (DORMANT)
1636453833.939221: netlink: Operstate: ifindex=3 linkmode=-1 (no change), operstate=5 (IF_OPER_DORMANT)
1636453833.939373: EAPOL: External notification - portEnabled=0
1636453833.939420: EAPOL: External notification - portValid=0
1636453833.939445: EAPOL: External notification - EAP success=0
1636453833.944560: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453833.980513: dbus: fi.w1.wpa_supplicant1.Interface.Disconnect (/fi/w1/wpa_supplicant1/Interfaces/0) []
1636453834.002611: dbus: fi.w1.wpa_supplicant1.Interface.RemoveNetwork (/fi/w1/wpa_supplicant1/Interfaces/0) [o]
1636453834.002810: dbus: Unregister network object '/fi/w1/wpa_supplicant1/Interfaces/0/Networks/0'
1636453834.039532: wlan0: No enabled networks - do not scan
1636453834.039668: wlan0: State: DISCONNECTED -> INACTIVE
1636453834.044981: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453836.802975: dbus: fi.w1.wpa_supplicant1.Interface.Scan (/fi/w1/wpa_supplicant1/Interfaces/0) [a{sv}]
1636453836.803252: wlan0: Setting scan request: 0.000000 sec
1636453836.803862: wlan0: State: INACTIVE -> SCANNING
1636453836.803953: wlan0: Starting AP scan for wildcard SSID
1636453836.804026: wlan0: Add radio work 'scan'@0x142a80
1636453836.804064: wlan0: First radio work item in the queue - schedule start immediately
1636453836.804176: wlan0: Starting radio work 'scan'@0x142a80 after 0.000105 second wait
1636453836.804231: wlan0: nl80211: scan request
1636453836.804308: nl80211: Scan SSID
1636453836.804338: nl80211: Scan extra IEs - hexdump(len=10): 7f 08 04 00 00 00 00 00 00 40
1636453836.814300: Scan requested (ret=0) - scan timeout 30 seconds
1636453836.814523: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453836.820661: nl80211: Event message available
1636453836.822745: nl80211: Drv Event 33 (NL80211_CMD_TRIGGER_SCAN) received for wlan0
1636453836.823789: wlan0: nl80211: Scan trigger
1636453836.824626: wlan0: Event SCAN_STARTED (47) received
1636453836.824857: wlan0: Own scan request started a scan in 0.010378 seconds
1636453837.219893: nl80211: Event message available
1636453837.220140: nl80211: Drv Event 34 (NL80211_CMD_NEW_SCAN_RESULTS) received for wlan0
1636453837.220207: wlan0: nl80211: New scan results available
1636453837.220246: nl80211: Scan probed for SSID ''
1636453837.220291: nl80211: Scan included frequencies: 2412 2417 2422 2427 2432 2437 2442 2447 2452 2457 2462 2467 2472
1636453837.220329: wlan0: Event SCAN_RESULTS (3) received
1636453837.220369: wlan0: Scan completed in 0.395526 seconds
1636453837.221044: nl80211: Received scan results (6 BSSes)
1636453837.221315: wlan0: BSS: Start scan result update 4
1636453837.222932: wlan0: BSS: Add new id 6 BSSID 42:84:6a:14:9a:2a SSID 'stefans_Guest' freq 2442
1636453837.224109: dbus: Register BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/6'
1636453837.231109: BSS: last_scan_res_used=6/32
1636453837.233170: wlan0: New scan results available (own=1 ext=0)
1636453837.240179: WPS: AP[0] 3c:84:6a:14:9a:7a type=0 tries=0 last_attempt=-1 sec ago blacklist=0
1636453837.240794: WPS: AP[1] 3c:84:6a:14:9a:2a type=0 tries=0 last_attempt=-1 sec ago blacklist=0
1636453837.241294: wlan0: Radio work 'scan'@0x142a80 done in 0.437094 seconds
1636453837.241394: wlan0: radio_work_free('scan'@0x142a80): num_active_works --> 0
1636453837.242176: wlan0: No APs found - clear blacklist and try again
1636453837.242624: Removed BSSID 42:84:6a:14:9a:7a from blacklist (clear)
1636453837.242732: wlan0: No suitable network found
1636453837.242818: wlan0: Use normal scan instead of sched_scan for initial scans (normal_scans=1)
1636453837.242894: wlan0: Short-circuit new scan request since there are no enabled networks
1636453837.242969: wlan0: State: SCANNING -> INACTIVE
1636453837.243833: dbus: flush_object_timeout_handler: Timeout - sending changed properties of object /fi/w1/wpa_supplicant1/Interfaces/0
1636453837.250502: dbus: org.freedesktop.DBus.Properties.Get (/fi/w1/wpa_supplicant1/Interfaces/0) [ss]
1636453837.252458: properties_get_or_set: Get(BSSs)
^C1636453839.179630: wlan0: Removing interface wlan0
1636453839.179795: wlan0: Request to deauthenticate - bssid=00:00:00:00:00:00 pending_bssid=00:00:00:00:00:00 reason=3 (DEAUTH_LEAVING) state=INACTIVE
1636453839.179846: wlan0: State: INACTIVE -> DISCONNECTED
1636453839.179873: nl80211: Set wlan0 operstate 0->0 (DORMANT)
1636453839.179902: netlink: Operstate: ifindex=3 linkmode=-1 (no change), operstate=5 (IF_OPER_DORMANT)
1636453839.180073: EAPOL: External notification - portEnabled=0
1636453839.180121: EAPOL: External notification - portValid=0
1636453839.208538: wlan0: WPA: Clear old PMK and PTK
1636453839.208700: wlan0: BSS: Remove id 2 BSSID 46:84:6a:14:9a:7a SSID '' due to wpa_bss_flush
1636453839.208741: dbus: Unregister BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/2'
1636453839.209180: wlan0: BSS: Remove id 0 BSSID 42:84:6a:14:9a:7a SSID 'stefans_Guest' due to wpa_bss_flush
1636453839.209234: dbus: Unregister BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/0'
1636453839.209516: wlan0: BSS: Remove id 1 BSSID 3c:84:6a:14:9a:7a SSID 'stefans' due to wpa_bss_flush
1636453839.209557: dbus: Unregister BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/1'
1636453839.209757: wlan0: BSS: Remove id 3 BSSID 3c:84:6a:14:9a:2a SSID 'stefans' due to wpa_bss_flush
1636453839.209793: dbus: Unregister BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/3'
1636453839.209982: wlan0: BSS: Remove id 6 BSSID 42:84:6a:14:9a:2a SSID 'stefans_Guest' due to wpa_bss_flush
1636453839.210018: dbus: Unregister BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/6'
1636453839.210213: wlan0: BSS: Remove id 5 BSSID 46:84:6a:14:9a:2a SSID '' due to wpa_bss_flush
1636453839.210249: dbus: Unregister BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/5'
1636453839.220031: wlan0: BSS: Remove id 4 BSSID d8:d8:66:25:9a:52 SSID 'NIBE STRONG_2.4GHz' due to wpa_bss_flush
1636453839.221935: dbus: Unregister BSS object '/fi/w1/wpa_supplicant1/Interfaces/0/BSSs/4'
1636453839.227864: wlan0: Cancelling delayed sched scan
1636453839.228057: wlan0: Cancelling scan request
1636453839.228429: wlan0: Cancelling authentication timeout
1636453839.228544: Remove interface wlan0 from radio phy0
1636453839.229075: Remove radio phy0
1636453839.230305: nl80211: deinit ifname=wlan0 disabled_11b_rates=0
1636453839.258359: nl80211: Remove monitor interface: refcount=0
1636453839.258490: netlink: Operstate: ifindex=3 linkmode=0 (kernel-control), operstate=6 (IF_OPER_UP)
1636453839.258791: nl80211: Set mode ifindex 3 iftype 2 (STATION)
1636453839.259147: nl80211: Unsubscribe mgmt frames handle 0x889b6cc1 (mode change)
1636453839.267596: dbus: Unregister interface object '/fi/w1/wpa_supplicant1/Interfaces/0'
1636453839.272636: wlan0: CTRL-EVENT-TERMINATING
1636453839.273055: dbus: Unregister D-Bus object '/fi/w1/wpa_supplicant1'

WL18xx firmware log (for gLogger to interpret)

�u����."����.ρ���.7��a���O��.#FL��.	K	��O�.a3���O�.�L	�	��O�.�5K0T�.�����UP�.ρ�vS�.7��a����S�.�F�S�.	K	�y�.à
�;��.a3�����.�L	�	����.�5L���.��������.ρ���.7��a���T��.�FQ��.	L	��T�.a3��U�.�L	�	�/U�.�5MbY�.������U�.ρ��X�.7��a����X�.�F�X�.	M	�l��.a3�����.�L	�	����.�5N���.�������.ρ�T��.7��a������.�F���.	N	�Z/a3��OZ/�L	�	�_Z/�5O�^/������Z/ρ��]/7��a���^/�F^/	O	���/a3����/�L	�	���/�5P*�/�����O�/ρ�z�/7��a�����/�F��/	P	��/à�$w/à��/à
���/à��/à�5_/a3���_/�L	�	��_/�5Q�c/������_/ρ�c/7��a���Mc/�FJc/	Q	�~/à���/a3���/�L	�	�(�/�5R[�/�������/ρ	���/7��a�����/�F��/	R	�fd/a3���d/�L	�	��d/�5S�h/�����e/ρ
�Dh/7��a���~h/�F{h/	S	���/a3��I�/�L	�	�Y�/�5T��/�������/�/7��a����/�F�/	T	��i
/a3���i
/�L	�	��i
/�5U%n
/�����Jj
/ρ�m
/7��a����m
/�F�m
/	U	�/�/a3��z�/�L	�	���/�5V��/�������/ρ
�
�/7��a���H�/�FE�/	V	��n
/a3��o
/�L	�	�o
/�5o�u
/.����Go
/S��Oo
/���Xo
/ϓ�ao
/+��no
/9��yo
/;���o
/�e�o
/��o
/Ke��d�/ρ��g�/7��a����g�/#F�g�/	q	�a��/à�9�/a3����/�L	�	���/�5q��/�������/ρ�
�/7��a���R�/�FO�/	q	�}>�/à��h�/a3��i�/�L	�	�-i�/�5r`m�/������i�/ρ��l�/7��a����l�/�F�l�/	r	�k�/a3����/�L	�	���/�5s��/������/ρ�I�/7��a�����/�F��/	s	�n�/a3��Nn�/�L	�	�^n�/�5t�r�/������n�/ρ��q�/7��a���'r�/�F$r�/	t	���/a3����/�L	�	���/�5u*��/�����O�/ρ�z�/7��a�����/�F��/	u	�4s�/a3��s�/�L	�	��s�/�5v�w�/������s�/ρ�w�/7��a���Yw�/�FVw�/	v	�!��/à����/à�h�/à�;1�/à�M��/à���/à����/a3��$��/�L	�	�4��/�5wg��/��������/ρ����/7��a������/�F���/	w	�qx�/a3���x�/�L	�	��x�/�5x�|�/�����$y�/ρ	�O|�/7��a����|�/�F�|�/	x	��.�/à�
��/a3��U��/�L	�	�e��/�5y���/��������/ρ
����/7��a���"��/�F��/	y	��}�/a3���}�/�L	�	��}�/�5z0��/�����U~�/ρ����/7��a������/�F���/	z	�uN�/à�;�/a3����/�L	�	���/�5{��/�������/ρ��/7��a���S�/�FP�/	{	�ӂ�/a3����/�L	�	�.��/�5|a��/��������/ρ
����/7��a���솤/�F醤/	|	�\�/a3����/�L	�	���/�5�j�/.������/S����/�����/ϓ��/+���/9���/;��'�/�e$�/�_�/Ke�$�*0ρ�E�*07��a���}�*0#Fz�*0	�	���+0à��|,0a3��},0�L	�	�+},0�5�^�,0������},0ρ���,07��a����,0�F�,0	�	�i�-0a3����-0�L	�	���-0�5��.0�����.0ρ�G.07��a����.0�F.0	�	��/0a3��M�/0�L	�	�]�/0�5���/0�������/0ρ��/07��a����/0�F�/0	�	��10a3���10�L	�	��10�5�(	10�����M10ρ�x107��a����10�F�10	�	�3�20a3��~�20�L	�	���20�5���20������20ρ��207��a���K�20�FH�20	�	��	40a3��
40�L	�	�&
40�5�Y40�����~
40ρ��
407��a����
40�F�
40	�	�u'40à�H40à�I�40à���40à�HQ50à �d�50a3����50�L	�	���50�5��50�����!�50ρ�L�507��a�����50�F��50	�	��60à!�70a3��Q70�L	�	�a70�5��70������70ρ	��707��a���370�F070	�	��N80à"���80a3���g4ρ�=�g47��a���t�g4#Fq�g4	�	��1h4à��i4a3��i4�L	�	�#i4�5�V"i4�����{i4ρ��!i47��a����!i4�F�!i4	�	�`�j4a3����j4�L	�	���j4�5��j4������j4ρ�>�j47��a���x�j4�Fu�j4	�	��"l4a3��C#l4�L	�	�S#l4�5��'l4������#l4ρ��&l47��a���'l4�F'l4	�	���m4a3���m4�L	�	���m4�5�*�m4�����Q�m4ρ���m47��a�����m4�F��m4	�	�6(o4a3���(o4�L	�	��(o4�5��,o4������(o4ρ�,o47��a���O,o4�FL,o4	�	�Ϫp4a3���p4�L	�	�*�p4�5�]�p4�������p4ρ���p47��a����p4�F�p4	�	�kq4à�-q4à��q4à���q4à��r4à�q-r4a3���-r4�L	�	��-r4�5��1r4�����'.r4ρ�R1r47��a����1r4�F�1r4	�	��!s4à�
�s4a3��X�s4�L	�	�h�s4�5���s4�������s4ρ	��s47��a���%�s4�F"�s4	�	��t4à��2u4a3���2u4�L	�	�3u4�5�37u4�����X3u4ρ
��6u47��a����6u4�F�6u4	�	�>�v4a3����v4�L	�	���v4�5�̹v4������v4ρ��v47��a���V�v4�FS�v4	�	��7x4a3��!8x4�L	�	�18x4�5�d<x4������8x4ρ��;x47��a����;x4�F�;x4	�	�o�y4a3����y4�L	�	�ʺy4�5���y4�����"�y4ρ
�M�y47��a�����y4�F��y4	�	��z4à��<{4a3��D={4�L	�	�T={4�5�D{4.�����={4S���={4����={4ϓ��={4+���={49���={4;���={4�e�={4��={4Ke��s�4u��s�4��s�4����s�4+��t�49��t�4��"t�4�et�4�6t�4Ke�O��4u�M��4�\��4і�g��4��!P�x��4������4u����4����4�������4������4Ü�ɏ�4͜�����Տ�4՜�ߏ�4ۜ�ꏛ4���4����4�
���4�����4���"��4��,��4��5��4��@��4�d2�^��4=��i��4)��u��4ٛ����4+��;��4ρ�]��47��a�����4#Fݔ�4��D��4à�›4à��ʛ4à��O�4a3���O�4�L���O�4�5�$T�4�����IP�4ρ�jS�47��a���T�4�F�S�4�����4a3��최4�L�����405�����4R�R��4ρ�}��47��a�����4#F��4����4a3����4�L���405����4R�Z�4ρ���47��a��� �4#F �4��ʁ�4a3�����4�L����405�����4R�l��4ρ����47��a���(��4#F%��4����4a3���4�L��*�405����4Q���4ρ���47��a���B�4#F?�4���N�4a3��4N�4�L��DN�405���M�4R��N�4ρ��Q�47��a���RR�4#FOR�4���_�4à�!}�4à���4à���4a3����4�L����4�5�#�4�����R
�4ρ�|�47��a���
�4�F
�4���r�4a3��s�4�L��s�405���r�4R�es�4ρ	��v�47��a���(w�4#F%w�4���؟4a3��ٟ4�L��ٟ405���؟4R�mٟ4ρ
��ܟ47��a���ݟ4#Fݟ4���>�4a3��?�4�L��?�405���>�4R�u?�4ρ��B�47��a���8C�4#F5C�4��㤠4a3����4�L��'��405�����4R�}��4ρ����47��a���/��4#F,��4���Ӡ4à�xc�4a3���c�4�L���c�4�5�h�4�����+d�4ρ
�Vg�47��a����g�4�F�g�4��Tɡ4ߓ�\ɡ4���dɡ4ϓ�nɡ4+��zɡ49���ɡ4���ɡ4�e�ɡ4��ɡ4Ke��ɡ4a3��ʡ4�L�� ʡ405���ɡ42���4u���4���4������4�����4Ü���4͜�������4՜���4ۜ���4����4����4���4��
��4��'0u��4�
�&�4��/�4��:�4�d�X�4)��d�4ٛ�q�4+��)�4ρ�J�47��a�����4#F~�4	�	��4à��f�4a3�� g�4�L	�	�0g�4�5�ck�4������g�4ρ��j�47��a����j�4�F�j�4	�	�m�4a3����4�L	�	���4�5���4����� �4ρ�K�47��a�����4�F��4	�	�"�4à�l�4a3��Pl�4�L	�	�`l�4�5��p�4������l�4ρ��o�47��a���p�4�Fp�4	�	���4a3����4�L	�	���4�5�,�4�����Q�4ρ���47��a�����4�F��4	�	�6q�4a3���q�4�L	�	��q�4�5��u�4������q�4ρ�u�47��a���Ru�4�FOu�4	�	���4a3���4�L	�	�-�4�5�`��4�������4ρ����47��a������4�F���4	�	����4à���4à��4à�{o�4à�qv�4a3���v�4�L	�	��v�4�5��z�4�����$w�4ρ�cz�47��a����z�4�F�z�4	�	�
��4a3��U��4�L	�	�e��4�5����4��������4ρ	����47��a���"��4�F��4	�	���4à��{�4a3���{�4�L	�	��{�4�5�0��4�����U|�4ρ
���47��a�����4�F��4	�	�/�4à�;��4a3�����4�L	�	����4�5���4��������4ρ��47��a���S�4�FP�4	�	���4à	�Ӏ�4a3����4�L	�	�.��4�5�a��4��������4ρ����47��a���섲4�F鄲4	�	�l�4a3����4�L	�	���4�5���4������4ρ
�J�47��a�����4�F��4	�	����4a3��G��4�L	�	�W��4�5��43�������4S�����4������4ϓ����4+�	����49�����4;��Ɔ�4�eÆ�4����4Ke�s��4u�q��4����4������4+�	����49�����4�	����4�e���4	����4Ke�|&�4u�y&�4��&�4і��&�4��!P��&�4���h.�4u�e.�4�t.�4����}.�4����.�4Ü��.�4͜������.�4՜��.�4ۜ��.�4���.�4���.�4�
��.�4����.�4����.�4���.�4���.�4��	/�4�d2�(/�4=��3/�4)��>/�4ٛ�K/�4+��0�4ρ�'3�47��a����3�4#F�3�4�EB�4à��J�4à�J^�4à�`��4a3�����4�L�����4�5���4�������4ρ�4��47��a������4�F���4���4à����4a3����4�L����4�56��4�����[��4ρ����47��a�����4�F��4�F��4à��l�4a3��<m�4�L��Lm�4�5q�4������m�4ρ��p�47��a���Uq�4�FRq�4���4a3��H��4�L��X��405����4R����4ρ����47��a���q��4#Fn��4�/9�4a3��c9�4�L��s9�405�9�4R��9�4ρ��<�47��a����=�4#F~=�4�?��4a3��s��4�L�����405���4R�ڟ�4ρ���47��a������4#F���4����4à���4à��]�4a3��^�4�L��.^�4�5bb�4������^�4ρ��a�47��a���Ob�4�FLb�4�
��4a3��B��4�L��R��405����4R����4ρ	����47��a���j��4#Fg��4�R��4à����4a3����4�L�����4�51��4�����V��4ρ
����47��a���#��4�F!��4����4a3����4�L����405����4R�i��4ρ����47��a�����4#F��4��N�4a3��O�4�L��O�405��N�4R�qO�4ρ��R�47��a���4S�4#F1S�4�za�4à	�J��4à
�l
�4a3���
�4�L���
�4�5��4������4ρ
�J�47��a�����4�F��4�Hs�4ߓ�Ps�4���Xs�4ϓ�bs�4+�
�ns�49��zs�4�
��s�4�e�s�4
��s�4Ke��s�4a3��t�4�L��t�405��s�42����4u����4����4�������4������4Ü����4͜��������4՜�Ɵ�4ۜ�П�4��۟�4����4����4��
����4��'0u�	��4�
���4����4��'��4�d�F��4)��Q��4ٛ�^��4+����4ρ�8��47��a���o��4#Fl��4		�9�4à��"�4a3��
#�4�L	�	�#�4�5P'�4�����u#�4ρ��&�47��a����&�4�F�&�4		�9��4à�Z��4a3�����4�L	�	����4�5��4�����
��4ρ�8��47��a���r��4�Fo��4		��'�4a3��=(�4�L	�	�M(�4�5�,�4������(�4ρ��+�47��a���,�4�F,�4		����4a3��֪�4�L	�	���4�5��4�����@��4ρ�u��47��a������4�F���4		�%-�4a3��p-�4�L	�	��-�4�5�1�4������-�4ρ�1�47��a���>1�4�F;1�4		����4a3��	��4�L	�	���4�5 L��4�����q��4ρ����47��a���ֳ�4�Fӳ�4	 	����4à�(
�4à�?r�4à����4à����4à���4à�V2�4a3���2�4�L	�	��2�4�5!�6�4�����3�4ρ�;6�47��a���v6�4�Fs6�4	!	�[�4à	����4a3��A��4�L	�	�Q��4�5"���4��������4ρ	�Ը�47��a�����4�F��4	"	�T��4à
��7�4a3���7�4�L	�	��7�4�5#<�4�����A8�4ρ
�l;�47��a����;�4�F�;�4	#	�^"�4à�'��4a3��r��4�L	�	����4�5$���4�����ں�4ρ���47��a���?��4�F<��4	$	��<�4a3��
=�4�L	�	�=�4�5%MA�4�����r=�4ρ��@�47��a����@�4�F�@�4	%	�NB�4à�X��4a3�����4�L	�	����4�5&���4�������4ρ
�6��47��a���p��4�Fm��4	&	��A�4a3��-B�4�L	�	�=B�4�5?�H�4.����pB�4S��xB�4����B�4ϓ��B�4+���B�49���B�4;���B�4�e�B�4��B�4Ke��Rc5u��Rc5��Rc5����Rc5+���Rc59���Rc5���Rc5�e�Rc5�
Sc5Ke�~~c5u�|~c5��~c5і��~c5��!P��~c5����c5u�	�c5��c5����!�c5���+�c5Ü�6�c5͜�����B�c5՜�L�c5ۜ�W�c5��a�c5��m�c5�
�y�c5�����c5�����c5����c5����c5����c5�d2�˂c5=��ւc5)���c5ٛ��c5+����c5ρ�ʆc57��a���N�c5#FK�c5A��c5à��c5à���c5à�Bd5a3��NBd5�L��^Bd5�5A�Fd5������Bd5ρ��Ed57��a���zFd5�FwFd5A�%�d5a3��Y�d5�L��i�d505C���d5R���d5ρ��d57��a���p�d5#Fm�d5C�-e5a3��ae5�L��qe505D�e5R��e5ρ��e57��a����e5#F}e5D�>te5a3��ste5�L���te505E�te5R��te5ρ�
xe57��a����xe5#F�xe5E�Q�e5a3����e5�L����e505F�%�e5Q���e5ρ�$�e57��a�����e5#F��e5F�i@f5a3���@f5�L���@f505G�<@f5R�Af5ρ�-Df57��a����Df5#F�Df5G��_f5à��pf5A.H'�3}f5à�w�f5A.H'���f5a3��H�f5�L��X�f5�5G�g5�������f5ρ��g57��a���lg5�Fig5G�*eg5a3��^eg5�L��neg505I��dg5R��eg5ρ	��hg57��a���uig5#Frig5I�֠g5à��#h5a3��
$h5�L��$h5�5IM(h5�����r$h5ρ
��'h57��a���?(h5�F=(h5I��rh5à��h5a3��R�h5�L��b�h5�5J��h5�������h5ρ���h57��a���}�h5�Fz�h5J�(Ii5a3��\Ii5�L��lIi505L��Hi5R��Ii5ρ��Li57��a���sMi5#FpMi5L��[i5à��j5à	��j5a3��j5�L��j5�5LKj5�����pj5ρ
��j57��a���,j5�F*j5L��mj5ߓ��mj5����mj5ϓ��mj5+�	��mj59���mj5�	��mj5�e�mj5	��mj5Ke�"nj5a3��Vnj5�L��fnj505M�nj52���j5u���j5���j5������j5�����j5Ü���j5͜�����ˊj5՜�֊j5ۜ��j5���j5����j5���j5��
��j5��'0u��j5�
�#�j5��-�j5��8�j5�d�V�j5)��b�j5ٛ�o�j5+��'�j5ρ�H�j57��a����j5#F|�j5	N	���k5à��
l5a3��l5�L	�	�-l5�5N`l5������l5ρ��l57��a����l5�F�l5	N	��"m5à�j�m5a3����m5�L	�	�Őm5�5O��m5������m5ρ�H�m57��a�����m5�F�m5	O	���n5à�o5a3��Mo5�L	�	�]o5�5P�o5������o5ρ��o57��a���o5�Fo5	P	���p5a3���p5�L	�	���p5�5Q)�p5�����N�p5ρ���p57��a�����p5�F��p5	Q	�3r5a3��~r5�L	�	��r5�5R�r5������r5ρ�r57��a���Xr5�FUr5	R	�ךs5a3��"�s5�L	�	�2�s5�5Se�s5�������s5ρ���s57��a�����s5�F��s5	S	���s5à��t5à��ot5à�4�t5à���t5à��u5à	�ou5a3���u5�L	�	��u5�5T�!u5�����"u5ρ�M!u57��a����!u5�F�!u5	T	��v5a3��S�v5�L	�	�c�v5�5U��v5�������v5ρ	��v57��a��� �v5�F�v5	U	��"x5a3���"x5�L	�	��"x5�5V.'x5�����S#x5ρ
�~&x57��a����&x5�F�&x5	V	�9�y5a3����y5�L	�	���y5�5Wǩy5������y5ρ��y57��a���Q�y5�FN�y5	W	��'{5a3��({5�L	�	�,({5�5X_,{5������({5ρ��+{57��a����+{5�F�+{5	X	�j�|5a3����|5�L	�	�Ū|5�5Y��|5������|5ρ
�H�|57��a�����|5�F�|5	Y	��,~5a3��F-~5�L	�	�V-~5�5r4~52�����-~5S���-~5����-~5ϓ��-~5+�	��-~59���-~5;���-~5�e�-~5��-~5Ke���5u���5���5���!��5+�	�.��59��9��5�	�D��5�eA��5	�X��5Ke�:$�53�8$�5=�F$�5����%�53��%�5��%�5}

��&�53��&�5��&�5�}

��#(�53�!(�5�0(�5}

��)�5u��)�5��)�5і��*�5u��*�5�
+�5і�V,�5u�T,�5)�e,�5A����?��,�5���,�5<���������,�5�l�,�5��,�5}k�,�5���,�5�!�,�5�-�5�i-�5<�E-�5����-�5�2�-�5��-�5i��-�5��-�5�#��-�5�#��-�5Y$��-�5�$��-�5%��-�5%��-�5���-�5�.�5_�.�5��.�5_�.�5��,.�5_�(.�5���.�5p�����.�5-l�.�5��.�5#F�.�5
t
�%/�5u�"/�5 �1/�51�B/�5���@@@�R/�57@�c/�5�ۋ@@@�֕�5�iӕ�5$g�镧5m�W��5a3�����5�m��g����5�L
�
����505v�&��5j�˖�50ρ�����Y��5���g��5@y��a�+��5@y�@�̛�5KI�ܛ�5WG2Df����5KH2Tv����5aF�
��5
�M�Bz�j���5�N�&��5?�N�@�pL�2��M��5�O�V��5 @�c��5�e`��5�x��5Ke���5������5��5.Ak�k�5�z��5Fw��5v��֧5I���&��5�&��V��5��A��ز�A������5������5�8���5+��1��5I���V�5@�;
��V�5�8�)+�5+��1�5ۇ�k��5�&�����5��������������53����P0�������5�8���53���5��	�53��	�5	�dW�53�aW�5�jX�53�hX�5	�2��53�0��5�C��53�@��5	�E��53�C��5�J��53�G��5	���53���5���53���5�!��5���<��53�:��5�v��5u�t��5����5і���5u���5��5і�
�5��!S��5���%�53�"�5��53��5,��53��5�,�5E����?���w�5u�u�5���5і���5��1���5�����53���5-���53���5)��	�5u��	�5��	�5M���
�53��
�5��
�5}

���53���5��5�}

����
�53�
�5�,
�5}

�H�53�E�5V�U�5���?�c�5��m�5���53���51���5����53���5�kQ�5�&���Q�5���A�J����Q�5�8�k�5�&����5�����������5�8�kq�5�&���q�5���a�j����q�5�8�k�5�&����5�����������5�8�k��5�&�����5���������ɑ�5�8�k!�5�&���!�5��������!�5�8�l��5�&�����5���������ɱ�5�8�lA�5�&���A�5���1�:����A�5�8�o��5ۇ�5��5c��lѹ5�&���ѹ5����������ѹ5�8�`4�5ۇ��f�5c��"r�5u� r�5	�/r�5��<r�5
�PO@ ��s�5u��s�5��s�5і��s�5��'dF��s�5����x�5u��x�5	��x�5���x�5
�PO@ ���53���5?���53���5*���5u���5���5U��la�5�&���a�5���Q�Z����a�50P������a�5�8�Ms�5u�Ks�5�Zs�5���㠻5u�ᠻ5!�5$����5�#���5(˃@@���5�#� ��5(��@@�8��5{s��E��5��k�5|�u�5���������5o{�����5G����5u���5pG�j�Bz����5
}���5+p���5������5�ۋ�����5���1<�5����b�53��b�5?��}�53��}�5?����5���5��53�3��5?��Ƽ5���l�5�&����5�����������5�8�k�5����[�5���̽5���l��5�&�����5���q�z���́�5�8��ؾ5������5���aſ5���qſ5;}�{ſ5=}��ſ5=k�pƿ5�u��}ƿ5�˃���ƿ5�����l�5�&����5����
�����5�8�m��5�&�����5���������͡�5�8�8��5�+
���53���5/���5�~ ��]�5Ӻ�m1�5�&���1�5���!�*����1�5�8�m��5�&�����5������������5�8�rQ�5�&���Q�5���A�J����Q�5�8�m��5�&�����5�������������5�8�mq�5�&���q�5���a�j����q�5�8�m�5�&����5�����������5�8�m��5�&�����5���������Α�5�8�n!�5�&���!�5��������!�5�8���53���5?�n��5�&�����5���������ϱ�5�8�nA�5�&���A�5���1�:����A�5�8�n��5�&�����5������������5�8�na�5�&���a�5���Q�Z����a�5�8�n��5�&�����5������������5�8�n��5�&�����5���q�z���Ё�5�8�o�5�&����5����
�����5�8�o��5�&�����5���������С�5�8�o1�5�&���1�5���!�*����1�5�8�o��5�&�����5������������5�8�oQ�5�&���Q�5���A�J����Q�5�8�o��5�&�����5������������5�8�oq�5�&���q�5���a�j����q�5�8�o�5�&����5�����������5�8�p��5�&�����5���������Б�5�8�p!�5�&���!�5��������!�5�8�p��5�&�����5���������ѱ�5�8�pA�5�&���A�5���1:���A�5�8�p��5�&�����5����������5�8�pa�5�&���a�5�e�a�5���a�5���Q*Z���a�5�8�ab�5Ke�h�5u�h�5�!h�5U��Qq�5u�Oq�5�]q�5і�iq�5��!S�zq�5����s�5u��s�5��s�5�����s�5����s�5Üst
��s�5͜������s�5՜��s�5ۜ��s�5���s�5���s�5�
��s�5����s�5���t�5��t�5��t�5��$t�5�d�Ct�5=�
�Nt�5)��Zt�5ٛ�gt�5+��p��5�&�����5����������5�8�p��5�&�����5���qz��ҁ�5�8�q�5�&����5���
����5�8�q��5�&�����5����	�	��ҡ�5�8�q1�5�&���1�5���!*���1�5�8�q��5�&�����5����������5�8�qQ�5�&���Q�5���AJ���Q�5�8���5@�;�#��5�8�qq�5�&���q�5���aj ��q�5�8�L.�5@�;�_.�5�8�r��5�&�����5����� �ԑ�5�8�r!6�&���!6������!6�8�r�6�&����6�������ӱ6�8�rA6�&���A6���1:���A6�8�r�6�&����6���������6�8�ra6�&���a6���QZ���a6�8�r�6�&����6���������6�8�r�	6�&����	6���qz��ԁ	6�8���	6a3���
6�|����
6(˃����
6(�����z(
6�L���(
6p5��
6��P)
6ρ��,
67��a���#-
6#F -
6���L
6a3���L
6�L���L
605��SL
6m�5M
6ρ�VP
67��a����P
6#F�P
6��Yp
6a3���p
6�L���p
605��p
6n��p
6ρ�t
67��a����t
6#F�t
6���
6a3��O�
6�L��_�
605��ד
6i���
6ρ�ߗ
67��a���z�
6#Fw�
6��ݷ
6a3���
6�L��!�
605����
6i�v�
6�
67��a���+�
6#F(�
6����
6a3����
6�L����
605��[�
6p�?�
6ρ�j�
67��a���L�
6#FI�
6����
6a3��4�
6�L��D�
6�5�86�����c�
60���6�O�%6 �$6����	6 6��
6�׀�6�F6���6�&��'6��!�!���[6�8��6|��6��������6o{��s�6�&����6����"�"y��ԡ6�8�t�6�|��6���������6|�SY
6�|�_Y
6�������oY
6'{���Y
6�|���Y
6(˃����Y
6(�����Fh
6u�Ch
6�Rh
6і�^h
6��'dF�nh
6����i
63��i
6�xq
6a3��
�
6�L���
6�5���
6����p�
6ρ�Ï
67��a���N�
6�FK�
6���
6a3��4�
6�L��D�
605����
6����
6ρ�ij
67��a���N�
6#FK�
6���
6��
6à�l�
6a3����
6�L����
6�5�_�
6I������
60�����
6�O���
6 ���
6����
6��
6B'6�M�E�
6�FC�
6���'6a3���C6�&��)D6��4$�<$���]D6�8�JF6�L��XF6�5��M6&�����F6ρ�J67��a����J6�F�J6���^6à��h6à�s6à��~6à���6a3��ڄ6�L���6�5�-�6�����	�60ρ�������6�O���6 ��6��Շ6�6M�6xA�i�6�Ff�6����6a3��*�6�L��8�6�5�b�6�������6ρ���67��a�����6�F��6���6a3��Q�6�L��a�605����6����6ρ	���67��a���~�6#F{�6����63���6?�6a3��H6�L��X605���6��u60ρ�����!6�O�+6 �w	6��A	6s	6CT6K��	6F�	6���>6a3���U6�L���U6�5��d6����V6ρ
�hY67��a���Z6�FZ6���q63��q6?��y6a3���y6�L���y605��&y6��9z6ρ�d}67��a���~6#F�}6����6a3��ӝ6�L���605��"�6���60ρ�����ؠ6�O��6 �"�6��M_6�6��63L���6F~�6���6�&��.�6���%��%~�b�6�8�;�6a3���6�L���6p5��61�*	6ρ��67��a���
6�F
6���,6a3���,6�L���,605��&,6��*-6ρ
�U067��a����06#F�06���M6a3���M6�L���M6�5�^U6����N60ρ������O6�O��O6 ��P6��@�6�P66�G�YQ6�FWQ6��;r6a3��Ɵ6�L��ԟ6p5���6 �+�6ρ
�~�67��a����6�F	�6���6ߓ��6����6ϓ�)�6+��5�69��A�6��K�6�eI�6�c�6Ke���6a3���6�L��(�605��~�6��F�60ρ�������6�O��6 �P�6u�N�6�]�6і�h�6��!S�y�6���C�6��6?�6>F63'���6F��6���,6u��,6	��,6���,6
�PO@ �063�06*�sQ6�&���Q6���A'J's���Q6�8��63��6/�+�6�~�9�6�z��6u��6��6U��s�6�&����6����(�(����6�8��
63��
6��
6}

��&63��&6��&6�}

��(63�
(6�(6}

�s)6u�q)6*�)6e���)6�{��@ @@ ��)6�����)6:���a�aa��)6�l��)6%m��)6�m��)6�l��)6�l��)6�l�*6�l�*6�l�(*6�l�6*6�l�C*6'{�b*6���|*6���*6E�������������*6���*62�*6�
+6˄
+6� +6�Ao+6�<+6k�H+6�#�T+6�#���^+6+��}+6WG2Df����+6KH2Tv��+65M��+6��+6�,6�L��a,6a3��q-6�L��k.6p5��P,6�863�86�$86����963��96�>;63�;;6��<63��<6�>63�>6,�a?63�^?6��@63��@6-��B63��B6��E63�E6��F63��F6	�?H63�=H6��I63��I6	�xK63�vK6��L63��L6	�/N63�-N6��O63��O6	���6��?�63�<�6�L�6}

�R�63�O�6�_�6�}

����63���6���6}

�[6u�X6�g6і��6u��6��6і�	6u�6)�6A����?�=6��H6<��������]6�l[6�m6}kj6���6�!�6��6���06�2-6�=6i�:6�U6�#�b6�#�l6Y$�w6�$��6%��6%��6���6��6_��6���6_��6���6_��6��6�i6<�~6p��c���6-l�6��6#F�6

��6u��6 ��61�
6���@@@�67@�06�ۋ@@@�uo6�iro6�h��o6m��o6a3��#p6�mU�i�@p6�L
�
�Pp605��o6j�mp60���r6���r6@y��a��r6@y�@��u6KI��u6WG2Df����u6KH2Tv��u6aF��u6
�M�B*�j��u6�N��u6?�N�@�pL�2��v6�O�v6 @�"v6�ev6�7v6Ke��v6��Ou6�v6��6ap�@w6F=w6���6�&����6���q2z�q�X�6���#�6I���q�6+���h6�&���h6���
��i63����P0����@i6�8���6I� ���6+0�M�63�K�6��6�&��/�6��ٗ	j�	T��c�6�8���63���6	��'6ۇ�SH63�QH6��~63��~6	��63���6��63��6	�-l63�*l6���6�&��ۈ6���!*����6�8���63���6	���63���6���63���6���6����63��6�x�6u�v�6���6і��6u��6��6і�(�6��!S�9�6���9�63�7�6�W�63�T�6,�v�63�t�6���6E����?���y+6u�w+6��+6і��+6��1��+6����463�46-��563��56)��66u��66��66M��863�86�86}

�?963�=96�L96�}

����:63�}:6��:6}

��;63��;6V��;6���?��;6���;6��<63��<61�=6��}>6u�{>6��>6і��>6��'d>��>6����?63��?6��6�&���6�������6�8���6�&��ܨ6���AJ���6�8��86�&���86�������96�8�j63�g6?���6�&����6���aj���6�8��X!6�&���X!6�������Y!6�8���"6�&����"6��������"6�8��w#63��w#6?��x$6�&���x$6�����y$6�8��&6�&���&6�������	&60P�����D	&6�8���&63���&6?�hn'63�fn'6?�/p'63�,p'6?�t�'63�q�'6?���'6�&���'6���1:���'6�8���'6ۇ��'6c����'63���'6?�)(6ۇ��t(6c���(6u��(6	�&�(6��3�(6
�PO@ ���(6u���(6���(6і���(6��'dF���(6�����(6u���(6	���(6����(6
�PO@ ���(63���(6*���(6u���(6���(6U���()6�&���()6�������))6�8�e#*6u�b#*6�r#*6�����*6�&���*6���QZ���*6�8��*6u��*6!��*6$��*6�#�(�*6(˃@@�7�*6�#�C�*6(��@@�\�*6{ɀ�h�*6��+63�+6?�}
+63�{
+6?�bv+6G��ov+6u�~v+6pG�j�B*���v+6
}��v+6+p��v+6�����v+6�ۋ�]�+6�e[�+6�k�+6�e���+6���e�+63�c�+6?�,6�e,6�,,6�e�X,6���-,63��,,6?��H,6�&���H,6�������.I,6�8��I,6�e�I,6��I,6�e��I,6�����,6�e��,6��,6�e�7�,6����,6�e�,6�&�,6�e�R�,6����@-6�e�@-6��@-6�e��@-6����-6�e�-6��-6�e�"�-6���M�-6�eK�-6�[�-6�e���-6�����-6�&����-6���qz���-6�8�.6�e	.6�.6�e�D.6���M.6�eM.6�M.6�e�;M.6���KM.6;}�UM.6=}�]M.6=k��M.6!�u�l���M.6<˃��M.6<���Q�.6�eN�.6�^�.6�e���.6�e��.6���.6�e�!1/6�e1/6�.1/6�e��h/6�&���h/6���!
!��i/6�8���/6�e��/6�è/6�e��@06�e�@06��@06�e�Z�06�eW�06�g�06�e���06�&����06����"�"���06�8�e�16�ec�16�s�16�e��26�e�26��26�e��H26�e�H26��H26�e�E|26�eB|26�R|26�e���26�&���26���!$*$���26�8���26�e��26���26�e��46�&���46����%�%��46�8���56�&���56���A'J'���56�8�66�e66�#66�e�Y66�eW66�g66�e�."66�e+"66�;"66�e�+566�e)566�9566�e��R66�e�R66��S66�e��y66�e�y66��y66�e���66�e��66�
�66�e���66�e��66���66�e���66�e��66���66�e�v76�es76��76�e�g76�ed76�t76�e�r76�eo76�76�e��876�&���876����(�(��976�8���86�&����86���a*j*���86�8�O�96�eL�96�\�96�e��X:6�&���X:6����+�+��Y:6�8��P;6�e�P;6��P;6�e�=�;6�e;�;6�K�;6�e���;6�&����;6����-�-���;6�8��<6�e|�<6���<6�e��x=6�&���x=6���//��y=6�8���=6�e��=6���=6�e��>6�e�>6��>6�e��?6�&���?6����0�0��	?6�8���@6�&���@6���12:2���@6�8��(B6�&���(B6����3�3��)B6�8���C6�&���C6���Q5Z5���C6�8��HE6�&���HE6����6�6��IE6�8���F6�&����F6���q8z8���F6�8��hH6�&���hH6���:
:��iH6�8���I6�&����I6����;�;�� �I6�8��aJ6��55��aJ60c.1<6���aJ6u.���aJ6pc.��>6���aJ6u.��
bJ6pc.��:6	�bJ6u.
��&bJ60c. VQ;6Z�4bJ6u. 
��BbJ6(���i��-�PbJ6����:6�aJ6�a�K6�8�1�K6�&��_�K6���#=�,=s����L6�e��L6���L6�e��M6�&���M6����>�>��� M6�8�*&M6�e'&M6�7&M6�e�3(M6�e0(M6�@(M6�e�inM6�efnM6�vnM6�e��N6�e�N6��N6�e�N6�e�N6�N6�e�QN6�eNN6�^N6�e��\N6�e�\N6��\N6�e���N6�e��N6���N6�e���N6�&���N6���A@J@��!�N6�8�#�N6�e!�N6�1�N6�e��8P6�&���8P6����A�A��!9P6�8���Q6�&����Q6���aCjC��"�Q6�8��XS6�&���XS6�e�XS6���XS6����D)�D��2YS6�8��YS6Ke�:_S6u�8_S6�F_S6U���eS6u��eS6�fS6і�fS6��!S�fS6����gS6u��gS6��gS6�����gS6����gS6Üst
�hS6͜�����hS6՜�hS6ۜ�$hS6��/hS6��:hS6�
�FhS6���QhS6���\hS6��fhS6��ohS6��zhS6�d��hS6=�
��hS6)���hS6ٛ��hS6+��aiS6a3����S6�L����S6p5Y�iS6{���S6ρ�ЋS67��a���l�S6#FX�S6Z�֫S6a3��
�S6�L���S605[���S6q�p�S6ρ���S67��a���,�S6#F)�S6[���S6a3����S6�L����S605\�K�S6q�1�S6ρ�\�S67��a�����S6#F��S6\�_�S6a3����S6�L����S605]��S6n���S6ρ�#�S67��a�����S6#F��S6]�$T6a3��YT6�L��hT605^��T6l��T6ρ��T67��a����T6#F�T6^��:T6a3��#;T6�L��3;T605_��:T6q��;T6ρ��>T67��a���>?T6#F;?T6_��^T6a3���^T6�L���^T605`�n^T6p�S_T6ρ��bT67��a���cT6#FcT6`�xT6à���T6à�
�T6à�k�T6à�֞T6à�2�T6a3��}�T6�L����T6�5`��T6�������T60ρ�����X�T6�O�a�T6 �T�T6�FQ�T6`���T6�&����T6����F�F��&�T6�8��T6a3���T6�L��'�T6p5b���T6H�}�T6ρ���T67��a���v�T6#Fs�T6b��U6a3��U6�L��$U605c��U6q�zU6ρ	��U67��a���AU6#F>U6c��2U6a3���2U6�L���2U605d�_2U6q�E3U6ρ
�p6U67��a���7U6#F	7U6d�vVU6a3���VU6�L���VU605e�*VU6q�WU6ρ�;ZU67��a����ZU6#F�ZU6e�?zU6a3��tzU6�L���zU605f��yU6p��zU6ρ�~U67��a����~U6#F�~U6f��U6a3���U6�L��)�U605g���U6h�~�U6ρ
���U67��a���D�U6#FB�U6g�:�U6ߓ�B�U6���J�U6ϓ�S�U6+��`�U69��k�U6��v�U6�et�U6���U6Ke���U6a3���U6�L��'�U605h���U6`�D�U60ρ�������U6�O��U6 ���U6u���U6���U6і���U6��!S���U6�����U6��M�U6�U6n�V6!ڀ��U6F��U6h��xV6�&���xV6���HH��#yV6�8��V6u��V6	��V6���V6
�PO@ �[�V63�Y�V6*��X6�&���X6����I�I��#	X6�8��[Y6u��[Y6��[Y6U��˜Y6�&���Y6���1K:K��$�Y6�8���Y63���Y6���Y6}

���Y63���Y6���Y6�}

����Y63���Y6���Y6}

�0�Y6u�-�Y6*�;�Y6e��F�Y6�{��@ @@ �T�Y6����^�Y6:���a�aa�r�Y6�l��Y6%m���Y6�m���Y6�l���Y6�l���Y6�l���Y6�l���Y6�l���Y6�l���Y6�l��Y6'{��Y6���7�Y6��b�Y6E������������}�Y6����Y62��Y6���Y6˄��Y6���Y6�Ao��Y6���Y6k��Y6�#��Y6�#����Y6+��8�Y6WG2Df���L�Y6KH2Tv�X�Y65M�w�Y6�t�Y6���Y6�L����Y6a3����Y6�L����Y605m���Y6��`�Y63�]�Y6�m�Y6�����Y63���Y6�
�Y63�
�Y6�n�Y63�l�Y6���Y63���Y6,���Y63���Y6�F�Y63�D�Y6-���Y63���Y6��Y63���Y6�]�Y63�[�Y6	���Y63���Y6��Y63��Y6	�]�Y63�[�Y6���Y63���Y6	�
�Y63��Y6�g�Y63�d�Y6	�)�Z63�'�Z6�6�Z6}

���Z63���Z6���Z6�}

���Z63��Z6��Z6}

���Z6u���Z6���Z6і�q�Z6u�o�Z6�}�Z6і���Z6u���Z6)��Z6A����?�#�Z6��.�Z6<��������C�Z6�l@�Z6�Q�Z6}kO�Z6���Z6�!|�Z6���Z6����Z6�2�Z6��Z6i��Z6�3�Z6�#�H�Z6�iE�Z6<�]�Z6�#�f�Z6Y$�q�Z6�$�}�Z6%���Z6%���Z6����Z6���Z6_���Z6����Z6_���Z6����Z6_���Z6��=�Z6p�����S�Z6-lN�Z6�u�Z6#Fr�Z6
n
�8�Z6u�6�Z6 �D�Z61�U�Z6���@@@�e�Z67@�v�Z6�ۋ@@@�1=[6�i-=[6�h�C=[6m��=[6a3���=[6�mŒi��=[6�L
�
�	>[605p��=[6i�&>[60����?[6����?[6@y��a��@[6@y�@��A[6KI��A[6WG2Df����A[6KH2Tv��A[6aF��A[6
�M�Bz�j��A[6�N��A[6?�N�@�pL�2��B[6�O�B[6 @�(B[6�e%B[6�<B[6Ke��B[6F�B[6p��[6�e�[6��[6�e�9�[6I�����[6+���Q\6�&#��Q\6���Ar,Jr�Ar�R\6���cR\6�8�o�]6I���K�]6+��y�]6�&$���]6����s�s��s���]63����P0�����]6�8��q_6�&%��q_6���au&ju���q_6�8�za6�&&��a6����v�v���a6�8��?b6u��?b6!��?b6$��?b6�#��?b6(˃@@��?b6�#�	@b6(��@@�#@b6{&��0@b6��krb6u�irb6�wrb6U��z�b6�&'���b6����x�x��ڑb6�8��b63��b6��b6}

�?�b63�=�b6�L�b6�}

��g�b63�e�b6�t�b6}

���b6u���b6*���b6e����b6�{��@ @@ ���b6������b6:���a�aa�Ѫb6�l��b6�l��b6�l���b6�l��b6�l��b6�l�(�b6�l�6�b6�l�C�b6'{�`�b6���z�b6����b6����b6����b62�b6��b6˄�b6��b6�Ao�b6�4�b6k�?�b6�#�L�b6�#���V�b6+��u�b6WG2Df�����b6KH2Tv���b65M���b6���b6�Ŭb6����b6�L��<�b6a3����b6�L��1�b605x�,�b6����b63���b6���b6}

���b63���b6���b6�}

���b63��b6� �b6}

�Z�b6u�X�b6�g�b6і���b6u���b6���b6і��b6u��b6)�&�b6A����?�G�b6��Q�b6<��������f�b6�lc�b6�u�b6}kr�b6����b6�!��b6���b6���2�b6�2/�b6�?�b6i�<�b6�V�b6�#�b�b6�#�l�b6Y$�w�b6�$���b6%���b6%���b6����b6���b6_���b6����b6_���b6����b6_���b6���b6�i�b6<���b6p��^����b6-l��b6���b6#F��b6
z
�� c6u�� c6 �� c61�� c6���@@@�� c67@�� c6�ۋ@@@�_Rc6�i[Rc6�h�qRc6m��Rc6a3��Sc6�m�qi�(Sc6�L
�
�7Sc605|��Rc6i�TSc60����Tc6����Tc6@y��a��Uc6@y�@��Vc63��Vc6?��Vc6KI��Vc6WG2Df����Vc6KH2Tv�Wc6aF�Wc6
�M�Bz�j� Wc6�N�,Wc6?�N�@�pL�2��RWc6�O�[Wc6 @�gWc6�edWc6�{Wc6Ke�8Xc6F5Xc6|�z!d6�&(��!d6���zz�z�"d6���Z"d6�8�z�e6�&)���e6����{�{��{�ȱe63����P0�����e6�8�+�f63�)�f6?�U�f63�S�f6?�zAg6�&*��Ag6���1}:}���Ag6�8�z�h6�&+���h6����~�~����h6�8���j6@�;���j6�8�{�k6�&-���k6����� ���k6�8�{�m6�&.���m6���q�z���فm6�8�!n6I� ��}n6+0��n6ۇ�{o6�&/��o6����
����o6�8��o63��o6��o63��o6	��p63��p6�p63�p6	�{Xp63�yXp6��Yp63��Yp6	�{�p6�&0���p6���������١p6�8� �p63��p6�(�p63�%�p6	�K�p63�I�p6�D�p63�B�p6�Q�p6���m�p63�k�p6���p6u���p6���p6і�)�p6u�'�p6�5�p6і�@�p6��!S�R�p6���T�p63�R�p6�K�p63�I�p6,�@�p63�>�p6�Y�p6E����?����p6u��p6��p6і���p6��1��p6����p63��p6-��p63��p6)�
�p6u��p6��p6M��:�p63�8�p6�G�p6}

���p63���p6���p6�}

����[�p63�Y�p6�h�p6}

���p63���p6V���p6���?���p6����p6���p63���p61���p6����p6u���p6���p6і���p6��'d>���p6�����p63���p6�{1r6�&1��1r6���!�*����1r6�8��jr63��jr6?���s6�&2���s6�����9������s6�8�{Qu6�&3��Qu6���A�J����Qu6�8�$�u6i����u63��u6?�\�u63�Z�u6?�|�v6�&4���v6���ьڌ����v60P������v6�8�|qx6�&5��qx6���a�j����qx6�8�|z6�&6��z6���������z6�8�|�{6�&7���{6���������ޑ{6�8�|!}6�&8��!}6��������!}6�8�r~6ۇ��,~6c��'n~6ۇ�*z~6c��U�~6u�S�~6	�c�~6��o�~6
�PO@ �<�~6u�:�~6�I�~6і�T�~6��'dF�e�~6�����~6u���~6	���~6����~6
�PO@ �|�~6�&9���~6���������ޱ~6�8�63�6*�16u�.6�=6U���6u��6��6���,�6u�*�6!�8�6$�C�6�#�N�6(˃@@�]�6�#�i�6(��@@���6{����6����63���6?��63��6?�R3�63�P3�6?�|A�6�&:��A�6���1�:����A�6�8�
r�6�er�6�r�6�e��t�6�e�t�6��t�6�e�-v�6�e+v�6�;v�6�e�Ֆ�6G��㖀6u��6pG�j�Bz��
��6
}���6+p�"��6����5��6�ۋ����6������6U}�Κ�6=n@�%7����6�,����63-�ǜ�6=k�㜀6�u5���6<˃���6<�����6�e��6�,��6�e�N��6�eL��6�\��6�e���6�e���6���6�e����6�e���6����6�e�΀6�e΀6�$΀6�e�S��6�eP��6�`��6�e�|с6�&;��с6�����ʗ���с6�8�}a�6�&<��a�6���Q�Z����a�6�8�Մ6�eՄ6�#Մ6�e�qׄ6�enׄ6�~ׄ6�e�qۄ6�enۄ6�~ۄ6�e��6�e�6��6�e�}�6�&=���6���������6�8�}��6�&>����6���q�z���߁�6�8�}�6�&?���6����
�����6�8�}��6�&@����6���������ߡ�6�8�)��6�e'��6�7��6�e�3ĉ6�e1ĉ6�Aĉ6�e�}1�6�&A��1�6���!�*����1�6�8�}��6�&B����6������������6�8���6�e��6���6�e�}Q�6�&C��Q�6���A�J����Q�6�8�~�6�&D���6���ѥڥ����6�8�ِ6�e
ِ6�ِ6�e�~q�6�&E��q�6���a�j����q�6�8�~�6�&F���6����������6�8�~��6�&G����6�����������6�8�㡔6�eᡔ6��6�e�Z��6�eX��6�h��6�e�~!�6�&H��!�6��������!�6�8��/�6�e�/�6��/�6�e�~��6�&I����6���������౗6�8�~A�6�&J��A�6���1�:����A�6�8�~њ6�&K��њ6�����ʰ���њ6�8�a�6�&L��a�6���Q�Z����a�6�8��6�&M���6���������6�8���6�&N����6���q�z���ၟ6�8��6�&O���6����
�����6�8��e�6�e�e�6��e�6�e�,��6�&P�Z��6��2��Ǡ�������6�8�1�6�&Q��1�6���!�*�S���1�6�8���6�&R����6������������6�8�Q�6�&S��Q�6���A�J����Q�6�8���6�&T���6���Ѿھ����6�8��q�6�&U��q�6���a�j����q�6�8���6�&V���6�����������6�8����6�&W����6���������⑭6�8��4�6@�;��4�6�8����6�&Y����6������� �鱰6�8��A�6�&Z��A�6���1�+:����A�6�8�U1�6�eS1�6�c1�6�e��2�6�e�2�6��2�6�e��ѳ6�&[��ѳ6�����/�����ѳ6�8��a�6�&\��a�6���Q�Z����a�6�8���6�&]���6�����#��	����6�8����6�&^����6���q�z����へ6�8��0�6�+�\:�63�Z:�6/�k:�6�~ �{ʹ6�eyʹ6��ʹ6�e��ʹ6Ӻ���6�&_���6����
�����6�8���6Ӻ��F�6|�0Z�6I��� i�6+���z�63��z�6/��z�6�~��z�6�z����6�&`����6����� ����须6�8��U�6u��U�6�V�6U��҇�63�χ�6�އ�6}

�J��63�H��6�W��6�}

��w��63�u��6����6}

����6u����6*�ŋ�6e��ϋ�6�{��@ @@ �ދ�6����狼6:���a�aa����6�l���6%m���6k%7�%��6�m�2��6�l�@��6�l�N��6�l�]��6�l�k��6�l�z��6�l����6�l����6'{����6���ό�6�����6E��������������6��Q��62O��6�a��6˄]��6�t��6�Aoq��6����6k����6�#����6�#������6+��э�6WG2Df���卼6KH2Tv��65M���6�
��6�,��6��e��6�L��Ǝ�6a3��6��63�4��6�C��6������6�L��ᏼ605�����6�X��63�U��6�Z��63�X��6�j��63�h��6�r��63�p��6,�w��63�u��6�|��63�z��6-�5��63�3��6����63����6����63����6	����63����6����63����6	����63����6����63����6	����63����6�
��63���6	��
�63��
�6?�-�63�+�6?�2,�6u�/,�6�>,�6і�I,�6��!P�Z,�6���.�6u�.�6�&.�6����/.�6���9.�6Ü�E.�6͜�����Q.�6՜�[.�6ۜ�e.�6��p.�6��|.�6�
��.�6����.�6����.�6���.�6���.�6���.�6�d2��.�6=���.�6)���.�6ٛ��.�6+���/�6ρ�3�67��a����3�6#F�3�6���B�6à�p_�6à����6à�}��6a3�����6�L�����6�5����6����1��6ρ�Q��67��a������6�F���6���P�6a3���P�6�L���P�605��rP�6R�:Q�6ρ�dT�67��a����T�6#F�T�6���c�6à���6a3����6�L����6�5���6����S�6ρ���67��a����6�F�6���q�6a3��r�6�L��r�605���q�6R�sr�6ρ��u�67��a���$v�6#F!v�6�����6a3����6�L��&��605�����6R����6ρ����67��a���<��6#F9��6���=�6a3��.>�6�L��>>�605���=�6R��>�6ρ��A�67��a���GB�6#FDB�6���q�6à�S��6à����6à����6a3��D��6�L��U��6�5��6�������6ρ����67��a������6�F}��6��,_�6a3��`_�6�L��q_�605���^�6R��_�6ρ	��b�67��a���wc�6#Ftc�6��4��6a3��h��6�L��y��605����6R����6ρ
����67��a������6#F���6��=+�6a3��q+�6�L���+�605��+�6R��+�6ρ�/�67��a����/�6#F�/�6��=��6a3�����6�L�����6�5�`��6�������6ρ���67��a������6�F���6��IL�6a3��}L�6�L���L�605��%L�6I��L�6ρ
�P�67��a����P�6#F�P�6����6ߓ�	��6�����6ϓ���6+��'��69��3��6��>��6�e;��6�U��6Ke����6a3�����6�L��β�605��|��62��8�63��8�6��8�6}

��9�63��9�6�
:�6�}

��*;�63�(;�6�7;�6}

��<�6u��<�6��<�6і�>�6u�>�6�>�6і�[?�6u�X?�6)�i?�6A����?��?�6���?�6<���������?�6�l�?�6��?�6}k�?�6���?�6�!�?�6�-@�6���u@�6�2s@�6��@�6i�@�6��@�6�#��@�6�#��@�6Y$��@�6�$��@�6%��@�6%��@�6���@�6��@�6_��@�6��A�6_�A�6��A�6_�A�6���A�6�i�A�6<��A�6u��A�6 �B�61�B�6���@@@�-B�67@�>B�6�ۋ@@@��B�6p����B�6-l�B�6��B�6#F�B�6
�
�0��6�i-��6�h�C��6m�P��6a3��z��6�mQ�j����6�L
�
����6p5����6�ĭ�60ρ�����S��6���a��6@y��a�0��6@y�@�>��6KI�O��6WG2Df���e��6KH2Tv�q��6aF�|��6
�M�Bz�j����6�N����6?�N�@�pL�2�����6�O�Ʊ�6 @�ұ�6�eϱ�6���6Ke����6�����6���6�/�6����6F��6����6i������6�&�����6����(����+��6���q��6�8��Q�6�&���Q�6���AJ�A��Q�63����P0����R�6�8����6�&�����6����	�	�����6�8��q�6�&���q�6���aj���q�6�8���6�&����6���������6�8��?�6i������6�&�����6���������6�8�aK�6@�;�tK�6�8����6�&�����6����� ���6�8��A�6�&���A�6���1:���A�6�8�Pa�6i�����6i������6i������6i�����6i�����6i���a�6i���\��6i�����6�&��G��6��������{��6�8����6i������6i������6��������60c.ϫ�6����6u.
�����6(��G��-�
��6�����6���6�&��6�i�2��6G����<��6���F��6�����6�C������6�C������6cD���6���6���6�D�������6�D�������6�D���6�D�� �@ �v�6�D�P#�6E��U�sv�-+�6TE����3�6�+EL@ i���:�6?EL@ X@ ��:�66OE��i�a��B�6�sEDT���@ �@ ��J�6��E��@ �@ �@ �@ ��R�6�Ea�wZ�6�E�Sb�6�EH�.j�6�E.��6�
r�6e���y�6F��Á�6#F����6AF����6y�!����6���‰�6�w g��6�Ή�6�w�B�6�ډ�6�wЭ�6���6�wl��6���6�w<��6����6�������60c.ϫ�6���6u.
��-��6Eu�!��6Eu���6Eu���6Eu���6Eu���6Eu���6Eu�ޥ�6Eu�ө�6Eu�u��K"��Lu��L<�M�kp��L�M�j�'\�i$\<��\p��_���\-l�\��\"F�\

���i
�w9�1��l.��?�
�e<��~�a3�����m�9����L
�
�ϖ 5�q�?�a�3�_��m�]�x����]�ۘ]�����]�L�]�V����]����Ù]�͙���]�	��:�]�D��v�]	���	���]
���
��]����*�]�5��f�]
�q�
���]����ޛ]����]�%��V�]�a����]����Μ]�ٜ�
�]���F�]�Q����]������]�ɝ���]���6�]�A��r�]����]2�؞]d����] � ��Q�]Ȁ\����]Ȁ��] ��]!�&�]"�Y�]#���]$���$�ɠ]%<���]&���&�9�]'��m�](����])�ӡ]*��]+�9�],
�D�,�u�]-
���-���].��]/��/� �]0�+�0�\�]1���]2
���2�ˣ]3���]4�1�]5�<�5�m�]6�x�6���]7�ܤ]8��]9��9�K�]:�V�:���];���;�å]<�Υ<���]=�
�=�;�]>�F�>�w�]?���?���]@���@��]A���A�+�]B�6�B��3����u����U���3��<��3��7��3���|3�y'��!3��!��"3��"(��$u��$��%u��%��&3��&@��&Sd����'3��'4��(3��(B��('��)���)+��&)A=�����}u��}'��}a���3�߃�/�3�-�A�x�3�u��Ӈ3�Ї��}

�+�3�)��8�}

��3����}

��3�
�?�T�3�Q��ˑ3�ȑ�O�3�L���3�	���3�	�+�h�3�e��u����љ3�ϙ!�ۣ3�٣>���1	�B�3�?����3���	���3���L�3�I�	���3����ӱ3�б	�h�3�e����3���	�
�3��C�c�3�a�,���3���.�ø@u�?@'�6�3�4�?���u��� ���1�»���@@@�ӻ7@���ۋ@@@�-�ρ��3�����O�� @�+�
�e(���F����3���	���3����G�3�D�	���3�����3��	�j�3�h����3���	�~�3�|�=�����Ȁn�3�l�*���3������}

�+�3�)��7��}

�����3������}

���u������і��u����і���3�����������3����1�3�/����u���)���A����?�������<�����������l�����}k������!��\�������i��<����2�����i�������#����#���Y$���$��%��%�'���$��;�_�8���K�_�H���[�_�W�����a3��l�3�j�V�z����?�����P�3�M�1�]���g�3�e�����L����`5�����p�ف��4�-l.��X�"FU�

�'\�i#\�e�9\m��\a3���\�m�f��\�L
�
�] 5�}\l�$]0���?]���M]@y��a�^@y�@�_KI�&_WG2Df���<_KH2Tv�H_aF�S_
�M�Bz�j�b_�N�n_?�N�@�pL�2���_�O��_ @�>`j��<�:`__#j��`F�`�F�&���F���))�)�G���^G�8���a3����&��������*�*��*���3����P0����
��8����L����5
�Z*������0������O��� @��F��aBa3��f�&���f���1,:,���f�8��n�L���n�5
��	ك���Ao0ρ�����}o�O��o @��pF�p�a�	a3���	�&����	����-�-����	�8���	�L����	�5�zڃ���B�	0ρ�����~�	�O���	 @��
F�
�aba3����&�������Q/Z/��ކ�8����L�����5�

ڃ���B�0ρ�����~��O��� @�ΐFː�a�a3���
�&���
����0�0���
�8��
�L���
�5��ڃ���B
0���~
�O��
 @�� 
F� 
�a�a3�����&�������q2z2��ަ�8����L�����5�*ڃ���B�0ρ�����~��O��� @�ΰF˰�aa3���6�&���6���4
4���6�8��>�L���>�5��ڃ���B?0ρ�����~?�O��? @��@F�@��u��!��$�$��#�/�(˃@@�>��#�K�(��@@�d�{��q���h�u�e��s�U���43��4��4}

��53��5��5�}

���63��6��6}

�8u�8*�8e��(8�{��@ L@ �68����@85����i�!�V8�l�d8�l�s8�l��8�l��8�l��8�l��8�l��8�l��8'{��8����8��)9E������������D9��}92{9��9˄�9��9�Ao�9��9k��9�#��9�#����9+���9WG2Df���:KH2Tv�:5M�<:�::�M:���:�L���:a3���;�L���; 5 ��:�˴���״ c.���u.
��� c."	�
��u."
�(��iU��-��
��__ȴ��D����D c.���Du.
���D c."	�
�Eu."
ĀE(��j���-�E
��__�D�������� c.����u.
���� c."	�
��u."
�(��ju��-� �
��__����d����d c.���du.
���d c."	�
�eu."
Āe(��j��-� e
��__�d�������� c.����u.
���� c."	�
��u."
�(��k���-�!�
��__���̈́���ل c.���u.
���� c."	�
��u."
�(��k%��-�!�
��__ʄ������ c.���u.
��� c."	�
�u."
Ā(��l���-�!
��__��Τ���ڤ c.���u.
���� c."	�
��u."
�(��lE��-�"�
��__ˤ��4 ����4  c.���4 u.
���4  c."	�
�5 u."
Ā5 (��$���-�"5 
���@�4 ��m!3��m!=��m!�����!�����! c.����!u.
���! c."	�
��!u."
�!(��.���-�+�!
���@��!��p2���p2 c."	�
�p2u."
Ā+p2(��K��-�8p2
���$#�o2�`4���p4 c."	�
�~4u."
�4(��e���-��4
���$#]4�`�5���p�5 c."	�
�~�5u."
��5(��e���-���5
���$#]�5�`=7���p=7 c."	�
�~=7u."
�=7(��e��-��=7
���$#]=7�`�8���q�8 c."	�
�~�8u."
��8(��f���-���8
���$#^�8��Mu��M��Mі��M��!P��M���rMu�pM�~M�����M����MÜ��M͜������M՜��Mۜ��M���M���M���M����M����M��M��	M��M�d2�-M=��8M)��DMٛ�QM+���Mρ�M7��a����M"F�M!��&Mà�q3Mà��=Mà��NMà��fMà�C�Mà���Mà�­Mà�C�Ma3����M�L����M�5Cb�M������Mߓ���M�����Mϓ���M+����M9���M���M�e�M�9�MKe

  • Hi,

    I will connect you with an expert. 

  • Hi,

    Are other devices in the field able to connect to router TP-Link Deco M5 (EU variant) ?

    Saurabh

  • We tested with multiple of our devices at the same location (i.e. same physical router) and all had the same issue. We had admin access to the router at the time and tried different configurations but very little could be changed as it is a locked down router aimed at the consumer market. We tried enabling and disabling 2.4GHz/5GHz networks, guest network, fast roaming and beamforming - all with the same result.

    We have not tested with a different TP-Link Deco M5 (i.e. other physical router, but same make and model) as we don't have access to that right now.

    Our devices are consumer products so we have very little insight into what network equipment they are connected to unless they contact us with an issue like the above. What we do know is that we have many devices that are connected over some wifi network and it is working fine.

  • HI, 

    This seems to be WiFi mesh router , but I am assuming you are connecting the DUT in infrastructure Station/Client mode.

    "What we do know is that we have many devices that are connected over some wifi network and it is working fine."

    Non-WiLink8 devices are able to connect to the exact same router ?

    I will check within the team if we have this router in our test lab

    Saurabh

  • Hi,

    Yes, we are connecting the DUT in station mode like a regular client.

    And yes, other devices (smartphones, laptops) are able to connect to the exact same router.

  • Hi,

    We tested this AP in our test lab and we able to successfully connect to it. Log snippet below :

    @am335x-evm:/usr/share/wl18xx# ./sta_connect-ex.sh Deco_base WPA-PSK 12345678
    netid=2
    =========================
    OK
    OK
    OK
    [255004.897062] wlan0: deauthenticating from 7c:ec:79:c8:02:f7 by local choice (Reason: 3=DEAUTH_LEAVING)
    wlan0: CTRL-EVENT-DISCONNECTED bssid=7c:ec:79:c8:02:f7 reason=3 locally_generated=1
    OK
    root@am335x-evm:/usr/share/wl18xx# wlan0: CTRL-EVENT-REGDOM-CHANGE init=CORE type=WORLD
    wlan0: CTRL-EVENT-REGDOM-CHANGE init=USER type=COUNTRY alpha2=US
    wlan0: SME: Trying to authenticate with b0:4e:26:d6:cb:a7 (SSID=[255011.283208] wlan0: authenticate with b0:4e:26:d6:cb:a7
    'Deco_base' freq=5180 MHz)
    [255011.297064] wlan0: send auth to b0:4e:26:d6:cb:a7 (try 1/3)
    [255011.542832] wlan0: authenticated
    wlan0: Trying to associate with b0:4e:26:d6:cb:a7 (SSID='Deco_ba[255011.552228] wlan0: associate with b0:4e:26:d6:cb:a7 (try 1/3)
    se' freq=5180 MHz)
    [255011.670592] wlan0: associate with b0:4e:26:d6:cb:a7 (try 2/3)
    [255011.698399] wlan0: RX AssocResp from b0:4e:26:d6:cb:a7 (capab=0x1411 status=0 aid=1)
    [255011.730384] wlan0: associated
    wlan0: Associated with b0:4e:26:d6:cb:a7
    wlan0: CTRL-EVENT-SUBNET-STATUS-UPDATE status=0
    wlan0: CTRL-EVENT-REGDOM-CHANGE init=COUNTRY_IE type=COUNTRY alpha2=DE
    [255012.769007] cryptd: max_cpu_qlen set to 1000
    wlan0: WPA: Key negotiation completed with b0:4e:26:d6:cb:a7 [PTK=CCMP GTK=TKIP]
    wlan0: CTRL-EVENT-CONNECTED - Connection to b0:4e:26:d6:cb:a7 completed [id=2 id_str=]
    [255012.830924] wlcore: Association completed.

    Best

    Saurabh

  • Thank you for checking this. Unfortunately it seems you have connected to a 5GHz frequency (freq=5180 MHz). Our wifi chip only supports 2.4GHz so there's a difference in setups on both ends.

    We're going to purchase a router of the same make and model for our own lab and retest the setup on that one. Will get back to you with the results.

    Can you share the software versions used (wpa_supplicant, kernel etc.)? And also the shell script?

  • Hi , 

    We actually tested both bands.

    root@am335x-evm:/usr/share/wl18xx# wlan0: CTRL-EVENT-REGDOM-CHANGE init=CORE type=WORLD
    wlan0: CTRL-EVENT-REGDOM-CHANGE init=USER type=COUNTRY alpha2=US
    wlan0: SME: Trying to authenticate with b0:4e:26:d6:cb:a6 (SSID=[255058.244758] wlan0: authenticate with b0:4e:26:d6:cb:a6
    'Deco_base' freq=2427 MHz)
    [255058.261537] wlan0: send auth to b0:4e:26:d6:cb:a6 (try 1/3)
    [255058.442855] wlan0: authenticated
    wlan0: Trying to associate with b0:4e:26:d6:cb:a6 (SSID='Deco_ba[255058.451836] wlan0: associate with b0:4e:26:d6:cb:a6 (try 1/3)
    se' freq=2427 MHz)
    [255058.570674] wlan0: associate with b0:4e:26:d6:cb:a6 (try 2/3)
    [255058.589242] wlan0: RX AssocResp from b0:4e:26:d6:cb:a6 (capab=0x1431 status=0 aid=1)
    [255058.620340] wlan0: associated
    wlan0: Associated with b0:4e:26:d6:cb:a6
    wlan0: CTRL-EVENT-SUBNET-STATUS-UPDATE status=0
    wlan0: CTRL-EVENT-REGDOM-CHANGE init=COUNTRY_IE type=COUNTRY alpha2=DE
    wlan0: WPA: Key negotiation completed with b0:4e:26:d6:cb:a6 [PTK=CCMP GTK=TKIP]
    wlan0: CTRL-EVENT-CONNECTED - Connection to b0:4e:26:d6:cb:a6 completed [id=3 id_str=]
    [255059.700636] wlcore: Association completed.

    I will try to get requested details.  This being thanksgiving week , there might be some delay in the response. 

    Saurabh