This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235MODS: Download abruptly aborts

Part Number: CC3235MODS


We have an issue with our product that it can't finish downloading a file from our http server.

Details
Processor: CC3235MOD
Wifi:  SimpleLink Wi-Fi Internet-on-a chip
File size: ~3.2MB
Percentage of file successfully downloaded before it abruptly stops:  non-deterministic in multiple runs; sometimes between 18%-20%
AT command used in our source code:  HttpReadResBody, with 512 byte size
Analysis
We've confirmed through Wireshark that the http server hosting our file is not the cause of the problem.  Please see the last line in the below Wireshark screenshot.  This shows the absence of TexasIns_8b:9b:51 response.  This coincides exactly to where the download stops prematurely.
Questions/Request
Can you provide an AT command with a specific example, in C, of how we can determine what is causing our download to halt abruptly?  Otherwise, what do you recommend?