This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3130: Radio test on CC3130, interface from RX processor.

Part Number: CC3130

Hi

For productiontest of CC3130, we need to use some of the Radio TX/RX test commands.

So for enabling the radiotesting via SPI channel (RX65 -> CC3130), I would need to integrate the files radiotool.c + h file into my already integrated TI SDK on our RX65 processor, or how should I understand it ?

All other "normal" communication should of cource be disabled when making Radio TX/RX tests.

Do we need to flash a special bin version for having the radio tx/rx features available ?

Best Regards

Jørgen Busch

  • Hi Jørgen,

    You should add RF testing code into your own RX65 firmware. As inspiration you can use radiotool.c code. But do not forgot upload latest ServicePack into sFlash.

    Jan