Hello, i need your help.
My embedded system use the 3.10.44 kernel and is a powerpc. (We can not update our kernel....)
We currently only had our wlan chip in AP or STA mode. With the firmware Rev 6.3.10.0.133 - wl127x-fw-5-sr.bin. All ok..
Now we wanted to use both at the same time with the firmware Rev 6.5.7.0.42 - wl127x-fw-5-mr.bin. That works so far, but unfortunately there is a kernel error.
If wlan0 is not connected to any AP and a terminal device is still registered on wlan1.
Jan 13 07:49:10 xxx-203568021013 kern.info kernel: wlcore: firmware booted (Rev 6.5.7.0.42)
Jan 13 07:49:11 xxx-203568021013 kern.info kernel: wlcore: down
Jan 13 08:03:08 xxx-203568021013 kern.err kernel: wlcore: ERROR command complete timeout
Jan 13 08:03:08 xxx-203568021013 kern.err kernel: wlcore: ERROR INTERROGATE command failed
Jan 13 08:03:08 xxx-203568021013 kern.warn kernel: wlcore: WARNING acx roaming statistics failed: -110
Jan 13 08:03:08 xxx-203568021013 kern.info kernel: wlcore: Hardware recovery in progress. FW ver: Rev 6.5.7.0.42
Jan 13 08:03:08 xxx-203568021013 kern.info kernel: wlcore: pc: 0x89e4, hint_sts: 0x00000001 count: 1
Jan 13 08:03:08 xxx-203568021013 kern.info kernel: wlcore: down
Jan 13 08:03:08 xxx-203568021013 kern.info kernel: wlcore: down
Jan 13 08:03:10 xxx-203568021013 kern.info kernel: wlcore: firmware booted (Rev 6.5.7.0.42)
> If wlan0 is connected to an AP and wlan1 is connected to an end device, there are no kernel error messages
With newer firmware comes the same error...wl127x-fw-5-sr.bin / wl127x-fw-5-mr.bin Single: Rev 6.3.10.0.142 // Multi: Rev 6.5.7.0.50
git.kernel.org/.../linux-firmware.git
Can you help me? What does the error mean?.