May i know how to do complete system reboot without using watchdog.
use case is like : After OTA i need to reboot the system and also after AP mode configuration i want to reboot the system
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
May i know how to do complete system reboot without using watchdog.
use case is like : After OTA i need to reboot the system and also after AP mode configuration i want to reboot the system
See RebootMCU() in the ota_update example (in the SDK).
//****************************************************************************
//
//! Reboot the MCU by requesting hibernate for a short duration
//!
//! \return None
//
//****************************************************************************
static void RebootMCU()
{
//
// Configure hibernate RTC wakeup
//
PRCMHibernateWakeupSourceEnable(PRCM_HIB_SLOW_CLK_CTR);
//
// Delay loop
//
MAP_UtilsDelay(8000000);
//
// Set wake up time
//
PRCMHibernateIntervalSet(330);
//
// Request hibernate
//
PRCMHibernateEnter();
//
// Control should never reach here
//
while(1)
{
}
}