This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1807MOD: I need support in modifying frequency of operation, mode of operation in the wifi module using wlconf for FCC.

Part Number: WL1807MOD


Hi,

as part of FCC, we need provision to do following actions in wifi module - 1807 - wilink 8.8:

1) Ability to change between supported operating modes (a, b, g, n, ac, ax)

2) Ability to select the operating frequency channel

3) Ability to control the highest duty cycle greater than 98% for FCC/ISED

4) Ability to control all supported Data Rates/Modulation/Modes

5) Ability to control the output power (maximum power will be implemented in final product)

6) Ability to select the operating antenna, if MIMO is supported

7) Ability for the DUT to connect to an AP and run iperf to meet the minimum payload if DFS is supported..

1, 2 & 3 are more mandatory for now. any help would be much appreciated.

Thanks in advance.

BR,

Anantha R