This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3235MODASF: Automatic selection of 2.4GHz vs 5GHz during connection attempt

Part Number: CC3235MODASF


Hello,

My client has a question that I have not been able to find explicitly in the datasheets, though I think the answer is yes reading between the lines:   If we have a device (in station mode) with the CC3235, and we are trying to connect to a known SSID, but we do NOT know whether the SSID is on 2.4 GHz or 5 GHz network, will the CC3235 automatically search both 2.4Ghz and 5Ghz bands to be able to find this SSID automatically?

Thanks,

Katie