Other Parts Discussed in Thread: CC3130
We want to use the RadioToolGui for different test purposes, but do not want to use the CC31xxMUBOOST interface. From the documentation it seems that only 2 of the 4 VCP of the FT4232 are used, the 2 "middle" ports. So i think i could two com ports adjacent to each other selecting the higher number port as control and the port below would then generate the nHIB signal, this is not working. Is there any way to use the RadiotoolguiCLI without using the BOOST PCB?
B.R. Flemming