The system is connected for a while and at some point the RSSI has gone for -83 and there are lots beacon loss happened and could see the below in wpa_supplicant
May 23 21:23:37 wpa_supplicant[857]: wlan0: First radio work item in the queue - schedule start immediately
May 23 21:23:37 wpa_supplicant[857]: RTM_NEWLINK: ifi_index=3 ifname=wlan0 operstate=2 linkmode=1 ifi_family=0 ifi_flags=0x1002 ()
May 23 21:23:37 wpa_supplicant[857]: nl80211: Interface down (wlan0/wlan0)
May 23 21:23:37 wpa_supplicant[857]: wlan0: Event INTERFACE_DISABLED (26) received
May 23 21:23:37 wpa_supplicant[857]: wlan0: Interface was disabled
May 23 21:23:37 wpa_supplicant[857]: wlan0: State: SCANNING -> DISCONNECTED
May 23 21:23:37 wpa_supplicant[857]: nl80211: Set wlan0 operstate 0->0 (DORMANT)
May 23 21:23:37 wpa_supplicant[857]: netlink: Operstate: ifindex=3 linkmode=-1 (no change), operstate=5 (IF_OPER_DORMANT)
May 23 21:23:37 wpa_supplicant[857]: wlan0: Determining shared radio frequencies (max len 2)
After this the system was not able to connect to AP until the system was resetwpa_interface_disabled.txt
Attached the complete wpa_supplicant logs