On an active and stable connection, occasionally, the device displays this Disconnect event:
[GENERAL EVENT] - Fatal Error!
Status: -109 (SL_GENERAL_ERROR_CON_MGMT_STATUS_DISCONNECT_DURING_CONNECT)
Sender: 5
I have a device that successfully reconnects to the AP after this happens but sometimes this error is constant, and the device never reconnects.
I've noticed that this seems to happen every 30ish minutes before reconnecting.
Other devices on the same firmware are never able to initially connect because of the same error.
I've searched through the forums a bit but have not found a solution.
Our device is on the latest SDK version for the CC3100 and the RSSI from the device ranges from -17 to -30 (The device is right now to the router).
Our device is rated to work on the 2.4 GHz range only with 802.11 b/g/n. i've made sure the router is operating with those parameters only and disabled any roaming functionality and signal strength is set to high. This is the router I'm working with for reference: AX1800 Wi-Fi 6 Router. I've tried multiple APs/routers with similar issues.
I'm going to try and capture the NWP logs with a few of these disconnects. Will reply with the logs soon.
Anything else I can try?
Thank you