Part Number: CC3200MOD
Other Parts Discussed in Thread: CC3200,
1. How to setting or control the wifi dBm to lower than rquired value?
a. China had announced a new requirment (工业和信息化部关于加强和规范2400MHz、5100MHz和5800MHz频段无线电管理
有关事宜的通知) at 2021-10-13 which required the Transmitter Unwanted Emissions in the Spurious Domain should under should not exceed the required limit dBm as below

b. The result shows that the CC3200 module was exceed the limit value in the frezqency range 2487~2455

2. Which type is the spicification of the CC3200MOD module as below

For the further information please refer to the attached "工信部无〔2021〕129号《工业和信息化部关于加强和规范2400MHz、5100MHz和5800MHz频段无线电管理有关事宜的通知》"
Thanks for your support
|
Paul Chang|Manager LELTEK INC. Wireless Handheld Ultrasound Provider Email: paul.chang@leltek.com |
工信部无〔2021〕129号《工业和信息化部关于加强和规范2400MHz、5100MHz和5800MHz频段无线电管理有关事宜的通知》.pdf