Other Parts Discussed in Thread: CC3200, SYSCONFIG
Hello,
I am trying to port a working project that uses SPI and uDMA in Ping-Pong mode from a cc3200 to a cc3235sf. 
The example with the cc3235sf should use FreeRTOS. So far, there have been significant problems with porting. 
The microcontroller receives data via the SPI interface and should trigger an interrupt as soon as the buffer is full.
As I see it, this interrupt is never triggered. Is there an example where SPI is used with uDMA, CC3235SF and FreeRTOS? I configure the SPI driver via Sysconfig.
In the old example, the vector table is defined in a file "startup_ccs.c" file directly in the application folder, in the new example with FreeRTOS, this table appear to be defined in the file 
"startup_cc32xxCC32xx_css.c". Could the cause lie here? It would be nice if someone could bring light into the darkness for me.